3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Hi I'm having some problem with my 3d printer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 347 subscribers
  • Views 2651 views
  • Users 0 members are here
  • stl
  • problem_solving
  • help!
  • 3d print
Related

Hi I'm having some problem with my 3d printer

mads391i
mads391i over 9 years ago

Hi I've just bought a cheap Chinese 3d printer.

When I connect printer to my computer it comes to life (all lights are blinking and motors move on spot a bit) but when I try to print cura says detecting baud rate and nothing happens. I'm using windows 10 if that matters; also tried with my mac didn't help. It is a ctc dual-extruder 3d printer.

I've read that should make change something about Marlin but I don't know anything about it.

 

Specs on 3d printer if you need:

Electronics

· CTC Board single-piece motherboard

· 5 axis, 1/16 micro-stepping motor control

· 4x20 LCD character display and multi-direction control pad

· Universal Power Supply: 100-240V, 50/60Hz

Software: ReplicatorG

· Compatibility: Windows.

· Print from SD card or over USB

· Input file type: STL, gcode,x3g

  • Sign in to reply
  • Cancel

Top Replies

  • awardautomation
    awardautomation over 9 years ago +3 suggested
    Can you give more details about the "motherboard"? What markings are on the main microprocessor? If you are unsure, post a photo of it. If it uses an atmel chip, chances are good its arduino compatible…
  • fvan
    fvan over 9 years ago +2 suggested
    "Marlin" is the firmware used by some 3D printers. Typically, this is flashed on an Arduino compatible chip on the printer's control board. Could you be more detailed about: I've read that should make…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to awardautomation +2 suggested
    Also good to know where the printer was bought and what is the original brand. Most of the cheap Chinese sellers are resellers as gearbest. Enrico
Parents
  • awardautomation
    0 awardautomation over 9 years ago

    Enrico is 100% correct, most of the cheap Chinese sellers are not manufacturers, they are simply resellers.

    I buy a lot of things from Aliexpress (think chinese ebay) and they all sell exactly the same items, with the description copy and pasted from somewhere else.

    Its hard to know whats going on over there, but there is probably 1 manufacturer for every 1000 sellers.

    In any case the one part that works well with the Repetier firmware I mentioned is the RAMPS 1.4 shield for arduino mega.

    It was developed for reprap 3d printers and since its open source, you don't need to make it yourself, just buy it from china.

    Make sure you confirm with the seller if it comes with the actual stepper drivers. They are removable from the RAMPS board since people often burn them out.

    stepper motor driver for RAMPS

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • awardautomation
    0 awardautomation over 9 years ago

    Enrico is 100% correct, most of the cheap Chinese sellers are not manufacturers, they are simply resellers.

    I buy a lot of things from Aliexpress (think chinese ebay) and they all sell exactly the same items, with the description copy and pasted from somewhere else.

    Its hard to know whats going on over there, but there is probably 1 manufacturer for every 1000 sellers.

    In any case the one part that works well with the Repetier firmware I mentioned is the RAMPS 1.4 shield for arduino mega.

    It was developed for reprap 3d printers and since its open source, you don't need to make it yourself, just buy it from china.

    Make sure you confirm with the seller if it comes with the actual stepper drivers. They are removable from the RAMPS board since people often burn them out.

    stepper motor driver for RAMPS