3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum A True Rotary 3D Printer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 341 subscribers
  • Views 2345 views
  • Users 0 members are here
  • 3d_printing
  • 3d_printer
  • innovation
Related

A True Rotary 3D Printer?

n5kzw
n5kzw over 13 years ago

I was wondering if there would be any advantage to to a 3D printer that operated in a cylindrical coordinate space instead of a cartesian space?   Would it be feasible to come up with a very fine threaded rod that would attach to the center of the print table to permit rotary positioning and Z-axis advancement at the same time?

 

Thoughts?

Ed

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I believe what you are describing would fit the SCARA-style RepRap Morgan design ( http://reprap.org/wiki/RepRap_Morgan ), which has a cylindrical build volume bounded by the two motors that define the…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Ed. A true Cylindrical "3dPrinter" (additive manufacturing device) is definitely a do-able and robust device to build. The above reply doesn't do what you asked. Scara is a series robot with 2 revolute…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    There have been a number of rotary variations, including one system that pairs multiple extruders with the rotational base plate to allow higher feed rates and some interesting variations in material integration…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I believe what you are describing would fit the SCARA-style RepRap Morgan design (http://reprap.org/wiki/RepRap_Morgan), which has a cylindrical build volume bounded by the two motors that define the rotational position and the deflection from that rotational vector in order to provide (X,Y) coordinate values within the print volume. There are currently three basic lines of RepRap design development (delta, cartesian and polar), with variations in construction such as Z-axis variations (dropping build plate, raising extruder, or building upside-down from suspended build plate, etc). Delta RepRaps are like the common Rostock design, Cartesian models include the standard RepRaps like the Mendel and Prusa designs, while Polar variations include options like the recent Morgan design. All accomplish the same thing - they move the extruder between (X,Y,Z) coordinates to build one layer at a time. A few DLP liquid designs use voxels that are cured all at once, but otherwise extruders deposite material sequentially - whether through a heated nozzle, syringe, or through an extruder-screw enabled conduit. SLA printers work more like the DLP designs, curing a liquid polymer one layer at a time as the build plate settles to create each new layer, and really-fine resolution material comes from multi-photon systems that only cure material where two beams intersect within the liquid-filled 3D build space. Other deisgns are mostly granular binding using sprays of material or glue similar to ink-jet printers, or they rely on laminated cutouts of paper stacked atop one-another and glued together for the final design. Beyond that are the blown-powder or wire-feed systems that use lasers or electron beams to melt or sinter materials together at the point of the extruder.

     

    VR,

     

    Kalani Kirk Hausman

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I believe what you are describing would fit the SCARA-style RepRap Morgan design (http://reprap.org/wiki/RepRap_Morgan), which has a cylindrical build volume bounded by the two motors that define the rotational position and the deflection from that rotational vector in order to provide (X,Y) coordinate values within the print volume. There are currently three basic lines of RepRap design development (delta, cartesian and polar), with variations in construction such as Z-axis variations (dropping build plate, raising extruder, or building upside-down from suspended build plate, etc). Delta RepRaps are like the common Rostock design, Cartesian models include the standard RepRaps like the Mendel and Prusa designs, while Polar variations include options like the recent Morgan design. All accomplish the same thing - they move the extruder between (X,Y,Z) coordinates to build one layer at a time. A few DLP liquid designs use voxels that are cured all at once, but otherwise extruders deposite material sequentially - whether through a heated nozzle, syringe, or through an extruder-screw enabled conduit. SLA printers work more like the DLP designs, curing a liquid polymer one layer at a time as the build plate settles to create each new layer, and really-fine resolution material comes from multi-photon systems that only cure material where two beams intersect within the liquid-filled 3D build space. Other deisgns are mostly granular binding using sprays of material or glue similar to ink-jet printers, or they rely on laminated cutouts of paper stacked atop one-another and glued together for the final design. Beyond that are the blown-powder or wire-feed systems that use lasers or electron beams to melt or sinter materials together at the point of the extruder.

     

    VR,

     

    Kalani Kirk Hausman