3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Printrbot simple isn't so simple!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 341 subscribers
  • Views 865 views
  • Users 0 members are here
  • firmware
  • simple
  • printrbot
Related

Printrbot simple isn't so simple!

e14 Contributor
e14 Contributor over 12 years ago

I have put together a Printrbot simple kitset for my school and I can't get it to work.

My main problem is that when it connects to the Repetier software it sees all of the axis measurements incorrectly.

x moves about 85mm, y moves about 18mm and z moves about 150mm but says it is moving 10mm.

I tried updating the firmware as it made the same errors when using Pronterface.

But to no avail! It still does the same thing.

Any ideas would be appreciated!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I've built the Printrbot LC v1, Printrbot Plus v1, and the Printrbot Jr v1, all with great results.


    However, I don't think I understand your problem. What says it's moving 10mm? Are you clicking the arrows in the software to move it in 10mm increments and it's moving these enormous amounts?

     

    Give me some more detail and maybe I can help out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The program (Either Repetier or Pronterface) isn't collecting the correct lengths of the axis from the Printrbot simple. I have set it's dimensions as 100mmx100mmx100mm in Repetier but it sees them as the wrong length for instance the z axis it sees as 10mm, but that actually moves the printer over 100mm and grinds as the motor slips as shown in this photo.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The program (Either Repetier or Pronterface) isn't collecting the correct lengths of the axis from the Printrbot simple. I have set it's dimensions as 100mmx100mmx100mm in Repetier but it sees them as the wrong length for instance the z axis it sees as 10mm, but that actually moves the printer over 100mm and grinds as the motor slips as shown in this photo.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    From what you've said, there's only one logical explanation. You tell the printer to move 10mm, and it ends up moving significantly more than that. My best guess is it's sending the wrong number of steps (for the stepper motor) per 1mm. So if it's 120 steps for 1mm, yours is thinking some other number entirely.

     

    This is from the getting started guide on printing the wrong size, which would also equate to motors moving the wrong amount. Yours just happens to be an extreme case. This is what it says:

     

    Print not correct size (G-Code)

    Verify values for X,Y,Z by typing command M501.

    Values should be X119 Y119 Z2020 E100.

    If  for some reason values are not this, change with G-code command M92 X119.

    Save settings on firmware with M500 command.

    Type M501 to verify change has been made.

     

    But.... that section from the getting started guide is a little brief and won't help if your printer needs different values than the default. I'd recommend this calibration guide, http://zheng3.com/2013/06/02/calibrating-the-printrbot-simple/

     

    I hope that helps! It really, really sounds like your problem is that it has the wrong step values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you very much that was correct and the guide was awesome!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer