3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum What 3d printer should build?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 341 subscribers
  • Views 1025 views
  • Users 0 members are here
Related

What 3d printer should build?

e14 Contributor
e14 Contributor over 12 years ago

     Hi everyone.  So after more than a year of contemplation, I'm finally going to dive into 3d printers head first.  I've read and watched some online builds, and the one thing that bothers me is the resolution of the fdm prints.  I'm hoping to create some smooth finished, as well as mechanical pieces.  On the other hand, the little research I've done on dlp printers tells me that while the resolution is great, the strength and size don't meet my needs.

 

 

      So here's my questions.  Cartesian or Delta?  As far as fdm goes which one of these two would give me the best resolution?  Also, in their respective categories which design would you use, keeping in mind the aesthetics of the prints is very important?  While we're on the subject, what determines the quality of the prints?  Is it hardware or software?  If it is hardware, can I build something close to the level of these high end printers?  If it is determined by software than which would you use, free or not?  Or does it all come down to calibration, in which case the loose nut behind the wheel becomes the weak point?

 

     I'm hoping to spend $500-$1000.  The print dimensions I'm hoping for are 200mm x 200mm x 800mm(I think this is a reasonable size).  Sorry for the lengthy post.  It's just that when you're new at something all one seems to have are questions.

 

    BTW, if you want to reply with a parts list of your dream build, please do so it well help me learn.  Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • hawkeyethehacker
    0 hawkeyethehacker over 12 years ago

    Also, if somebody has given an answer you are happy with, please mark them as a correct answer and not assumed. Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hawkeyethehacker
    0 hawkeyethehacker over 12 years ago

    Also, if somebody has given an answer you are happy with, please mark them as a correct answer and not assumed. Thanks image