3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Selecting the appropriate printer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 341 subscribers
  • Views 639 views
  • Users 0 members are here
  • printer
  • 3d
  • selection
Related

Selecting the appropriate printer

e14 Contributor
e14 Contributor over 11 years ago

I want to buy a 3D printer to be used to print architectural and engineering models.

I am quite keen on the Cube Pro Trio. Does anyone have a review on this printer

and is it the correct printer for my application. Thxz Trevern

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Trevor, Well the Cube Pro Trio is a shiny model but the cubify plastic is cartridge based with smart chips (think inkjet printers where they still have ink but refuse to print). Whilst it is possible…
Parents
  • Nate1616
    0 Nate1616 over 11 years ago

    Trevor,

    Martyn has some very good points about dual extruders and support material.

     

    Coming from the AEC industry and having used 3d Printers for showcasing designs I must say that FDM/FFF printers just don't do them justice.  What I have found is that clients (Architectural specifically) want to see the materials applied to the print.  Well current FDM/FFF printers aren't capable.  There are technologies that I hope will bridge this such as http://www.spectrom3d.com/.  The current printers that achieve full color printing are things such as http://mcortechnologies.com/ which is a laminate type of printing process and also http://www.3dsystems.com/ which is a binder jetting process.  Out of the 2 technologies laminate produces far more durable objects.  Now these are professional grade printers so cost far more than lets say a Cube Pro.  I have also found that printing full interiors such as furniture is very complicated on FDM/FFF printers.   If its more for internal collaboration and color isn't necessary then we use an SLA printer.  Very high resolution.  The two technologies I mentioned above can also be used.

     

    The last option you could look into is farming the printing out to some one like http://www.shapeways.com/.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Nate1616
    0 Nate1616 over 11 years ago

    Trevor,

    Martyn has some very good points about dual extruders and support material.

     

    Coming from the AEC industry and having used 3d Printers for showcasing designs I must say that FDM/FFF printers just don't do them justice.  What I have found is that clients (Architectural specifically) want to see the materials applied to the print.  Well current FDM/FFF printers aren't capable.  There are technologies that I hope will bridge this such as http://www.spectrom3d.com/.  The current printers that achieve full color printing are things such as http://mcortechnologies.com/ which is a laminate type of printing process and also http://www.3dsystems.com/ which is a binder jetting process.  Out of the 2 technologies laminate produces far more durable objects.  Now these are professional grade printers so cost far more than lets say a Cube Pro.  I have also found that printing full interiors such as furniture is very complicated on FDM/FFF printers.   If its more for internal collaboration and color isn't necessary then we use an SLA printer.  Very high resolution.  The two technologies I mentioned above can also be used.

     

    The last option you could look into is farming the printing out to some one like http://www.shapeways.com/.

     

    Nate