3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Which is better ABS or PLA filament?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 343 subscribers
  • Views 1557 views
  • Users 0 members are here
  • 3d_printing
Related

Which is better ABS or PLA filament?

bkoehlercq
bkoehlercq over 11 years ago

Hello,

 

I am very much a beginner, and am just learning more about 3D printing. I do 3D modeling as a hobby, and I have a pretty basic question. I would like to save up for my first 3D printer and would like to know which is better PLA or ABS filament?

 

Also would like some suggestions on a good starter printer.

 

Thank you in advance

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    I will just add the Clem's response. Another good thing about ABS is you can give it an acetone bath and make the print look as though it was cast using molds. ABS needs to be used on any part that will…
  • clem57
    clem57 over 11 years ago +2 suggested
    Simplifying the myriad of factors that influence the use of one material over the other, broad strokes draw this comparison. ABS - Its strength, flexibility, machinability, and higher temperature resistance…
Parents
  • Nate1616
    0 Nate1616 over 11 years ago

    I will just add the Clem's response.  Another good thing about ABS is you can give it an acetone bath and make the print look as though it was cast using molds.  ABS needs to be used on any part that will be around any sort of heat.  Using PLA even around your cars heat on will cause it to deform.  PLA will need to be printed with a fan blowing across the part as its very good at retaining heat.  If you don't want a fan another thing that helps is to not have the print solid, add a like a honeycomb pattern to allow the material to print.  I have found that even with this a fan help drastically with the quality of the print.  I have had issue with Bowden extruders and PLA as PLA is a softer material and would compress in the tube but can be fixed with slower speeds and larger retractions.  As far as which one will give you better quality(PLA or ABS) i would say with the right machine settings they will be the same.

    To answer your second part, what printer you will get is dependent on what you are going to be doing with the printer.  If you need large print volume then your selection will get narrowed down.  What style of printer do you want(Cartesian, Delta, Polar).  Are you looking to get very high resolution prints.  If your answer is yes then you would look at getting a Stereolithagraphy based printer not FFF/FDM.  The downside is small print volumes.  The last thing is do you want to build the printer yourself or do you want one that is ready to go the minute(well not fully true) you receive it.

     

    Nate

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Nate1616
    0 Nate1616 over 11 years ago

    I will just add the Clem's response.  Another good thing about ABS is you can give it an acetone bath and make the print look as though it was cast using molds.  ABS needs to be used on any part that will be around any sort of heat.  Using PLA even around your cars heat on will cause it to deform.  PLA will need to be printed with a fan blowing across the part as its very good at retaining heat.  If you don't want a fan another thing that helps is to not have the print solid, add a like a honeycomb pattern to allow the material to print.  I have found that even with this a fan help drastically with the quality of the print.  I have had issue with Bowden extruders and PLA as PLA is a softer material and would compress in the tube but can be fixed with slower speeds and larger retractions.  As far as which one will give you better quality(PLA or ABS) i would say with the right machine settings they will be the same.

    To answer your second part, what printer you will get is dependent on what you are going to be doing with the printer.  If you need large print volume then your selection will get narrowed down.  What style of printer do you want(Cartesian, Delta, Polar).  Are you looking to get very high resolution prints.  If your answer is yes then you would look at getting a Stereolithagraphy based printer not FFF/FDM.  The downside is small print volumes.  The last thing is do you want to build the printer yourself or do you want one that is ready to go the minute(well not fully true) you receive it.

     

    Nate

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • bkoehlercq
    0 bkoehlercq over 11 years ago in reply to Nate1616

    Hey thanks Nate. I appreciate your input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deepankarmaithani
    0 deepankarmaithani over 11 years ago in reply to Nate1616

    acetone bath is something everyone should try,specially those having low end printer.