3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum 3D Printer drivers/motors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 341 subscribers
  • Views 2103 views
  • Users 0 members are here
Related

3D Printer drivers/motors

e14 Contributor
e14 Contributor over 11 years ago

Hi guys,

 

I recently started researching into making my own 3D printer (which I might do or I might not) but does the stepper motor which feeds the filament into the hot head need it's own A4988 driver? I'm planning to control it using the Arduino Mega and the RAMPS 1.4 board if that helps and is there any thing else I need to use/know before I decide to go ahead on this project?

 

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • Nate1616
    0 Nate1616 over 11 years ago

    Kristaps-

    Yes, you will need a stepper driver for the extruder.  The typical setup is a driver for each axis(x,y,z) and one for the extruder.  The z driver will drive 2 motors in the typical Cartesian style printer.  The Mega 2560/RAMPS 1.4 is a great setup.  One thing you might want to look at is the newer electronics that are using faster processors.  This is going to be the year in 3d printing that will make 8bit controllers a dying technology.  The smoothie board is a nice 32bit board.  I'm also starting to look at the BeagleBone Black and CRAMPS board but haven't had much time with it yet.  They are currently working on a updated version that is suppose to have support for the Edison.  If you have any more questions don't hesitate to ask.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Nate1616

    Do you have to have 2 Z stepper motors or can you use one and link the other rod using a pully? Also, unfortunately, because this is going to be a budget build I can't really use any 32-bit boards which is a shame but I'll probably be looking into that in the future. Do you have any recommendations for a temp sensor which can go above 160C and don't require and external board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 11 years ago in reply to e14 Contributor

    Kristaps-

    No you don't have to have 2 motors for the z-axis but caution you that having a heavy carriage will cause the motors to skip/miss steps.  What you might want to look at is converting the standard Wade's extruder (direct drive) to the Bowden.  This will lighten up the carriage as the bowden extruder moved the motor off the carriage.

    As far as the temp sensor goes the typical thermistors used on extruders will allow you to go above 160C.  For example this is a common thermistor. http://media.digikey.com/pdf/Data%20Sheets/Honeywell%20Sensing%20&%20Control%20PDFs/135-104LAG-J01.pdf

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 11 years ago in reply to e14 Contributor

    Here is the standard hookup of the thermistor(temp measure).  No extra board is needed.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Nate1616

    I see, but wouldn't having a Bowden style extruder cause some timing issues or is the speed also controlled by the RAMPS board? Thanks for the thermistor! I'll try and find one that I could use in my build.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Nate1616

    I was planning to have it go through an Ardunio so I could keep an eye on it and so when it reaches a certain temp, it shuts the supply and throws up some warning or light on the case. Edit - I was also planning to use PLA for my machine because I can't be bothered with ABS shrinking and deforming due to the wrong temp though I see how it's connected.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Nate1616

    I was planning to have it go through an Ardunio so I could keep an eye on it and so when it reaches a certain temp, it shuts the supply and throws up some warning or light on the case. Edit - I was also planning to use PLA for my machine because I can't be bothered with ABS shrinking and deforming due to the wrong temp though I see how it's connected.