3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum What gets in the way of your 3D Printing project?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 342 subscribers
  • Views 5521 views
  • Users 0 members are here
  • projects
  • 3D Printing
  • 3d modelling
  • introduction
Related

What gets in the way of your 3D Printing project?

cstanton
cstanton over 4 years ago

All aboard the discussion train...

3D printers have came along way since the 'make your own RepRap with another 3D printer' at home, thanks to the expiry of patents and we also have ones that are now on conveyor belts.

Still, getting into 3D printing has its hurdles, we try to address some of these, but problems can still get in the way, such as finding that you need to replace the hotend of your 3D printer, and it instead sheers off in the heat block, and you have to find creatives ways to free it (talking from personal experience). There's also the manner of, how do you create the item which you're going to 3D print? What factors do you have to consider? Can you even get a hold of a metal 3D printer, or would resin be okay? and is the resin itself okay?

While I have access to a filament 3D printer at home, I do consider maybe acquiring a resin printer, but know for sure that any further 3D printing means I should really have a filtered enclosure because of fumes. That's partly what gets in the way of my creation these days, since I use OpenSCAD, I also don't fight with the licenses introduced from recent Autodesk changes, or the nuances of Blender...

So many options, perhaps that's also what gets in the way? Or maybe it's setup costs (I'm looking at you Ultimaker).

We're looking at expanding our content, and what we ask from 3D Printer manufacturers to goven our campaigns and content on the Community, and I'm interested in what you need help with, so reply and let us know, regardless of knowledge level or what you've been doing!

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 4 years ago +4
    At the moment, I've got two printers and although bed levelling manually is a bit finicky, once dialled in, things seem to go fine for a while. That is, until a thermistor wire breaks and we get a thermal…
  • hlipka
    hlipka over 4 years ago +3
    Not much these days. Owning a 3d printer since 7 years now. The first one was one which needed constant attention and tuning, and I spend more time improving it than with it printing. When I finally decided…
  • javagoza
    javagoza over 4 years ago +3
    I've been trying to get into the world of 3D printing for a while. I have read a lot and I have understood the limitations and advantages of the different types of filaments. I tried several CAD programs…
Parents
  • ralphjy
    ralphjy over 4 years ago

    There are a couple of problems that I consistently have with my 3D filament printer.  The first is caused by laziness.  I tend to leave my filament loaded between prints and on occasion due to moisture absorption (it rains in Oregon!), I'll have brittle filament that breaks.  And as Murphy would have it, it always breaks between my filament sensor and the extruder motor - so if I'm not paying attention I'll lose the print (horrifying if you're a few hours in).  Normally, if I'm around - I'll hear the filament break and can reload it on the fly...

    The other problem that I have is the dimensional accuracy of the print.  Due to the nature of 3D printing, printed dimensions will always be a little off from what is designed.  This is due to a combination of idiosynchrasies of the printer mechanisms, filament type, filament consistency, and the specific shape that is being printed.  I think experience brings you some "Kentucky windage", but if I need a precision fit I will always need to print multiple times to get the dimensional compensation correct (or use a file or filler).

    A problem I occasionally have is changing settings when I change filament types (sometimes even different spools of the same type).  I recently really messed up my hotbed when using a PLA+ filament - I still haven't figured that out yet - I just stopped using it for now.  Not sure if it is the temperature setting or something wrong with the material itself.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 4 years ago

    There are a couple of problems that I consistently have with my 3D filament printer.  The first is caused by laziness.  I tend to leave my filament loaded between prints and on occasion due to moisture absorption (it rains in Oregon!), I'll have brittle filament that breaks.  And as Murphy would have it, it always breaks between my filament sensor and the extruder motor - so if I'm not paying attention I'll lose the print (horrifying if you're a few hours in).  Normally, if I'm around - I'll hear the filament break and can reload it on the fly...

    The other problem that I have is the dimensional accuracy of the print.  Due to the nature of 3D printing, printed dimensions will always be a little off from what is designed.  This is due to a combination of idiosynchrasies of the printer mechanisms, filament type, filament consistency, and the specific shape that is being printed.  I think experience brings you some "Kentucky windage", but if I need a precision fit I will always need to print multiple times to get the dimensional compensation correct (or use a file or filler).

    A problem I occasionally have is changing settings when I change filament types (sometimes even different spools of the same type).  I recently really messed up my hotbed when using a PLA+ filament - I still haven't figured that out yet - I just stopped using it for now.  Not sure if it is the temperature setting or something wrong with the material itself.