3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Ender 3 Pro continual issues after initial successful prints - Updated
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 336 subscribers
  • Views 16848 views
  • Users 0 members are here
  • 3D Printing
  • Ender 3D Pro
Related

Ender 3 Pro continual issues after initial successful prints - Updated

opalko
opalko over 3 years ago

Hi folks, I have an Ender 3 Pro that I bought about a month ago. Stock machine. I have successfully printed using PLA and PETG filament initially.  I am using stock settings for PLA and PETG in Cura on a Linux machine for slicing.

The last thing I printed was a case, in PLA, for a transistor tester, one of those cheapee ones that work well. The outside of the case printed fine but the screw holders on the inside were a loose nest of filament that had no cohesion. They would just snap off with the touch of the finger. It would never hold screws.  So I tried printing the lower half again. This time the bottom layer did not even go down well. Tried again. This time even worse!

Ok after consulting different forums, I was first told my extrusion temp was too low - stock Cura setting is 200. I bumped it 210. Nope. Then I was told to clean the extruder nozzle, which I did. Nope. Then I was told to check the z step. So I went through the process of calculating that and adjusted it. No difference.

At this point I started over. I

- leveled bed again (still didn't work)

- cleaned nozzle again (still didn't work)

- tried different extraction settings (on/off, speed etc) (still didn't work)

Today I went back to the default settings and tried printing it one more time (and then a second and third attempt..). Now the skirt won't even lay down properly. Any guidance for what is going on or where to start (again) with this? I keep the PLA and PETG in the foil pouches they came in with dessicant but I don't have a dryer or use the oven before printing.

Here is a link to the photo album of first good prints and then the degradation over time to the last picture which is from today of the bottom of the tester case I am trying to print again.

https://photos.app.goo.gl/PmBKJQojMPebxnpJ8

Thanks

Robert Opalko

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 3 years ago +4
    Hi Robert, I look forward to learning what is causing this.
  • milosrasic98
    milosrasic98 over 3 years ago +4
    Hi! I had a similar issue where the printer just started under extruding, I've tried cleaning the nozzle, bumping up the temperature, switching the nozzle, but nothing helped. As I was trying to fix it…
  • ntewinkel
    ntewinkel over 3 years ago +3
    I had the same issues. For me it was the extruder arm that got a crack in it that you can only see after you take it off. Buying a metal extruder fixed all the issues. i think I’m using the correct name…
Parents
  • opalko
    opalko over 3 years ago

    So I have worked on this a bit more this week with no success.

    As I mentioned in a post above I:

    • re-leveled bed
    • checked extruder arm for cracks (did not see any):

    image

    image

    • check PTFE tubing (not mangled & no clogs)
    • tried test prints at different temps and print speeds (bad to worse)

    First I tried printing the bottom of the tester case (this one) again at 50% speed.  Initially it started printing beautifully with the bottom layer looking really good. Then as it got to the screw holders and the last bit of the top of the lower case half, the print quality went downhill. This was the result:

    image

    Then I rechecked bed, clogs,... and started with the 4-column retraction / test print. (This one) and it was a squidgy mess to start. So I tried it at a lower temp (fail), then a lower temp & slower speed (Better! but weird stringing), so then I tried the same temp at 50% speed (big time fail):

    image

    I think I am going to order an all metal extruder arm set and Capricorn tubing & different nozzle but does anyone think this is the problem? Is it possible the filament (PLA) is collecting too much moisture and causing these things? I store the filament in a foil pouch with desiccant when not in use, so it would have had to really absorb moisture fast to go from printing the bottom of the case pretty darn well to failing by the end.  I'm not quite at the wit's end the other fellow on this forum was with this printer but,.... suggestions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to opalko

    I don’t think the filament is at fault. I’ve left mine on the printer for weeks and it still prints fine.

    I also don’t think the extruder is the problem, as my prints looked stringy at all heat settings.

    Maybe a new nozzle?

    I’m definitely not an expert, so please do your own extra research, and hopefully others can comment, but my next step would be replacing the hot end assembly. It’s only about $17 CAD for the whole set that includes the nozzle, heater, wires and the tubing. Amazon link: https://a.co/d/f2T1nZy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to ntewinkel

    One other thing to try might be to print one of the samples that came with the printer, like the cat. Just in case you suspect the software might be doing something funny.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    Good idea, thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    Good idea, thanks!