3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Ender 3 Pro continual issues after initial successful prints - Updated
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 336 subscribers
  • Views 16886 views
  • Users 0 members are here
  • 3D Printing
  • Ender 3D Pro
Related

Ender 3 Pro continual issues after initial successful prints - Updated

opalko
opalko over 3 years ago

Hi folks, I have an Ender 3 Pro that I bought about a month ago. Stock machine. I have successfully printed using PLA and PETG filament initially.  I am using stock settings for PLA and PETG in Cura on a Linux machine for slicing.

The last thing I printed was a case, in PLA, for a transistor tester, one of those cheapee ones that work well. The outside of the case printed fine but the screw holders on the inside were a loose nest of filament that had no cohesion. They would just snap off with the touch of the finger. It would never hold screws.  So I tried printing the lower half again. This time the bottom layer did not even go down well. Tried again. This time even worse!

Ok after consulting different forums, I was first told my extrusion temp was too low - stock Cura setting is 200. I bumped it 210. Nope. Then I was told to clean the extruder nozzle, which I did. Nope. Then I was told to check the z step. So I went through the process of calculating that and adjusted it. No difference.

At this point I started over. I

- leveled bed again (still didn't work)

- cleaned nozzle again (still didn't work)

- tried different extraction settings (on/off, speed etc) (still didn't work)

Today I went back to the default settings and tried printing it one more time (and then a second and third attempt..). Now the skirt won't even lay down properly. Any guidance for what is going on or where to start (again) with this? I keep the PLA and PETG in the foil pouches they came in with dessicant but I don't have a dryer or use the oven before printing.

Here is a link to the photo album of first good prints and then the degradation over time to the last picture which is from today of the bottom of the tester case I am trying to print again.

https://photos.app.goo.gl/PmBKJQojMPebxnpJ8

Thanks

Robert Opalko

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 3 years ago +4
    Hi Robert, I look forward to learning what is causing this.
  • milosrasic98
    milosrasic98 over 3 years ago +4
    Hi! I had a similar issue where the printer just started under extruding, I've tried cleaning the nozzle, bumping up the temperature, switching the nozzle, but nothing helped. As I was trying to fix it…
  • ntewinkel
    ntewinkel over 3 years ago +3
    I had the same issues. For me it was the extruder arm that got a crack in it that you can only see after you take it off. Buying a metal extruder fixed all the issues. i think I’m using the correct name…
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    Well, just a bit into it but so far, so good. This is wild. I think if this prints correctly I will try to "compile" my own .gcode for Benchy and then print it and see what happens. Also, I'll compare the 2 .gcode files: yours and mine.  Not sure what else to do at this point. I don't have another machine that doesn't run Linux to run Cura on. I'll have to check if there are other Ubuntu ready slicing programs.

    Or, I could just get you to create all my .gcode file haha. Thank you for sending the .gcode file.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to opalko

    Also, there is still some "clunking" but not nearly as much as on other prints lately. Do you know if you used "standard", "dynamic", or "super" quality settings?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to opalko
    opalko said:
    Or, I could just get you to create all my .gcode file haha.

    Laughing I just found a new retirement gig! Wink 

    If it works, and if your own doesn’t, then I can try exporting that profile (for the black filament), maybe yours has a wonky setting somewhere.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to opalko

    Dang, I didn’t make note of that, but 95% sure it was 0.2 standard.

    mine did not clunk at all

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    I reloaded Cura and wiped all the profile settings I had (I think) so it will be interesting to see what the differences are.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to opalko
    opalko said:
    Do you know if you used "standard", "dynamic", or "super" quality settings?

    I just checked Cura: Standard 0.2mm, 0.4mm nozzle. No supports, no build plate adhesion.

    Cura 5.3.1

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    Well this is very interesting. I'm out words to describe what I'm thinking; flummoxed is all I can come up with. Mine printed without the issues I saw in previous prints.  But there are some significant differences.

    Here are some photos to compare. Yours on left, mine on right.  Yours printed at 215, mine at 200. I used the same filament for both since it's all I have. lol

    image

    Mine has 2 lines running across the bottom of the boat, whereas yours has 1?

    image

    Not much difference here on the bottom (that I can tell). I think mine is not as readable in this picture but it may be how I have boat positioned.

    image

    This one has the biggest difference. Whatever the square box in the back of the boat is supposed to be, yours extends all the way down uniformly to the deck while mine sort of juts inwards.  No idea why, the model shows it sort of tapering inwards but not a sharp change like mine...?

    image

    I guess I could try printing again at 215 but this doesn't explain why all the other non-cat, non-boat prints have failed lately! Can't be a clogged nozzle. I did nothing at all between the first and second print like cleaning the bed, the nozzle, none of that. I don't know if comparing the .gcode files is worth the time now. Sooo strange.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to opalko

    Correction: under better lighting I can see that mine doesn't jut inwards there, it's missing any layer in there! It's also in the same plane as that top line that runs around the outside of the boaThinking 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to opalko

    Mine didn’t have those lines. It looks like your printer is having extrusion issues where it skips the layers and ends up with the lines.

    I’m assuming your filament has a temperature rating listed? But at 215 that should cover most PLA. And it appears to work well for most of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • opalko
    opalko over 3 years ago in reply to ntewinkel

    "[Recommend Settings】We recommend printing the PLA filament at nozzle temperature of 200-230°C, bed temperature of 50-65°C, and printing speed of 50-100mm/s."

    is what mine says..sort of a wide range..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>