3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum A nice to know, if you are 3D printing.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 338 subscribers
  • Views 3099 views
  • Users 0 members are here
  • 3d modeling
  • 3D Printing
Related

A nice to know, if you are 3D printing.

colporteur
colporteur over 1 year ago

What is your 3D printing tip, trick or trap?

A friend of mine purchased a BIBO 3D printer three years ago. It stayed in the box until recently. The printer is now on my office floor as I learn to 3D print. A FREE 3D PRINTER YES!

Like all technology paths, with experience life becomes easier and without the experience, the response “I wish I had known that!” is common. I recently discovered glue sticks make a difference and the right glue stick even more.

I’m looking for tips, tricks, and traps E14 members have learned on their 3D printing journey. Maybe you have a tool that is indispensable for rooting out those support structures. I’ve cut my thumb once trying to clear a support structure and want to avoid that in the future. Do you have something, I would like to know about it?

I’m using Ultimaker Cura as slicer software and have started down the path of learning FreeCAD. I have created a few models in the CAD software and successfully printed them to solve problems I used to do in wood and metal. This has motivated me to continue.

If your suggestion is to throw the free 3D printer I have in the garbage because: 1) the manufacture has gone out of business: 2) newer printers do much more 3D heavy lifting than the dinosaur I have, don’t bother. I’m looking to tap into community experience without having to invest in cut thumb failures to learn it.

  • Sign in to reply
  • Cancel

Top Replies

  • milosrasic98
    milosrasic98 over 1 year ago +3
    Hope you enjoy 3D printing, it's an amazing hobby and an even better tool paired with electronics! Few tips: Make sure the printer is in a really good ventilated area, and be careful with the filaments…
  • obones
    obones over 1 year ago +1
    I have been down this path no that long ago and I must says that I prefer OrcaSlicer, it feels more intuitive to me. And do not forget to activate mouse ears to avoid corner lifting. But the first thing…
  • obones
    obones over 1 year ago in reply to obones +1
    Another thing that came back to me is to make sure your filaments are dry and stay dry. A food dryer is good for this, along with "sous vide" bags that do not leak with time.
Parents
  • vmate
    vmate over 1 year ago

    There's a billion little things to figure out, most are slicer settings, that will make a huge difference. Here are a few less known, but super useful tricks:

    - For functional parts, you can increase line width slightly(which is normally equal to your nozzle diameter). For example, with a 0.4mm nozzle, it would be set to 0.4mm by default, but by slightly increasing it(by about 10-20%), layers will be "squished" together harder, and layer adhesion will greatly increase. This comes at the cost of overhangs becoming very ugly though.

    - There are similar tradeoffs for temperature and cooling, both following this pattern of lower temperatures and more cooling = better looking, hotter and less cooling = stronger but worse looking.

    - The "alternate extra wall" option will make the walls and infill bind together much better, but can sometimes introduce weird artifacts in the outer walls

    - Increasing wall line count over increasing infill density will result in quicker prints while having the same strength

    - The best "all-around" infill is "Cubic Subdivision". "Gyroid" is technically better, but it is a lot slower to print.

    - "Z Hop When Retracted" can prevent the nozzle knocking off parts when filament curls up and gets in the way of the nozzle, but slows down prints.

    - To reduce stringing, especially with filaments like PETG, tune retraction speed and distance, and use Cura's  "Combing Mode" feature

    - There's about a dozen super useful settings for just supports, go through them so you're aware of their existence. Here are a few important but rarely mentioned ones: "Support X/Y Distance", "Support Interface Density", "Support Horizontal Expansion"

    - Enable "Remove Empty First Layers" to avoid accidents with models not touching the buildplate, and not noticing.

    - Check out tree supports. Most of the time they are not applicable or work a lot worse than "regular" supports, but every once in a while, it's great to have it.




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 1 year ago in reply to vmate

    Are the options you list supported by all 3D printers?

    The UltiMaker Cura software I am using doesn't align option names to many of the options you suggest. An example would be layer width, I'm thinking that is resolution in this software. I discovered an option for temperatures but it was under a menu called Materials>Printing Temperature or Build Plate Temperature.

    I'm thinking of moving to Octoprint software on a Raspberry Pi before investing much more. This will save me having to physically visit the printer to load files and print via the 2 inch screen. I'm thinking it might offer some naming consistency since BIBO printer is not made anymore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate over 1 year ago in reply to colporteur

    Yes, these are the exact names from Cura(with the exception of layer width, that should've been line width, sorry). I assume you're using the simplified menu.

    image

    Click the "Show Custom" button, and it will show the proper settings.
    Once there, the "three bar" menu icon in the top right will reveal the "Manage Setting Visibility" button. which will bring up a window where you can select what options you want to see exactly, that list will have everything I mentioned.

    image

    image

    Definitely do not turn on everything, there are way too many settings here you'll never need to use. Over time, you'll figure out what you need to adjust, but be aware that there's a lot of things that can be tweaked, and look over this list every once in a while to make sure you know the capabilities of your slicer.

    These are all the settings I've enabled over the years, currently configured to print functional PETG parts:
    image

    The vast majority of options will be supported on all 3D printers, there's only a few that require firmware support (like acceleration and jerk control, but no need to worry about that - they are only used to speed up prints, while maintaining quality)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vmate
    vmate over 1 year ago in reply to colporteur

    Yes, these are the exact names from Cura(with the exception of layer width, that should've been line width, sorry). I assume you're using the simplified menu.

    image

    Click the "Show Custom" button, and it will show the proper settings.
    Once there, the "three bar" menu icon in the top right will reveal the "Manage Setting Visibility" button. which will bring up a window where you can select what options you want to see exactly, that list will have everything I mentioned.

    image

    image

    Definitely do not turn on everything, there are way too many settings here you'll never need to use. Over time, you'll figure out what you need to adjust, but be aware that there's a lot of things that can be tweaked, and look over this list every once in a while to make sure you know the capabilities of your slicer.

    These are all the settings I've enabled over the years, currently configured to print functional PETG parts:
    image

    The vast majority of options will be supported on all 3D printers, there's only a few that require firmware support (like acceleration and jerk control, but no need to worry about that - they are only used to speed up prints, while maintaining quality)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 1 year ago in reply to vmate

    A question on settings. I assume settings are print material dependent? 4 rolls of PLA plastic came with the printer. I've have been working black and just figured out how to bring the second extruder online. I'm also assuming the settings are printer dependent. Some printers having better performance than others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate over 1 year ago in reply to colporteur

    Generally, there's relatively little difference between different rolls of filament that are of the same plastic types. Some people prefer to tune their profiles for each filament spool they have, but I haven't done that, as the improvement is not worth the time and wasted filament in my opinion.

    For different plastic types, there will be some differences, mainly temperatures, retraction, cooling, print speed. However, you should be able to make a profile that works quite well for pretty much everything(with the exception of nozzle and bed temperature, those will need to be adjusted for each type of material).

    Almost all machine-dependent settings will be because of the extruder motor/gearing/filament path. If you have dual extruders, they should be identical, so no need to individually adjust settings for each extruder.

    One thing you should verify is your e-steps. This value tells your printer how much it has to turn the extruder motor to extrude a specific amount of material. Here's a guide that explains it well: https://all3dp.com/2/extruder-calibration-calibrate-e-steps/
    I am not familiar with your printer, but measuring and calculating things should be the same as in the guide, but setting the newly calculated e-steps value might differ, you'll have to do some research.