3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum What is the 3D printing community/group looking for?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 343 subscribers
  • Views 5332 views
  • Users 0 members are here
Related

What is the 3D printing community/group looking for?

Nate1616
Nate1616 over 10 years ago

I just wanted to get the communities opinion on what would be of useful content to have.  With the 3D Printing 101 courses being put on hold because of unfortunate events i would be willing to put something together.  Now this could be anything related to printing.  From how-to, maybe new product reviews, training courses...  Let me hear your thoughts.

 

Nate

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to Nate1616 +5
    I think the lack of activity in the 3D printing area is down to two factors: Relatively few people have a 3D printer (or access to one). There are a few good dedicated 3D printing community web-spaces…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to gadget.iom +4
    Paul, I agree with you. What has blocked me until now was just what was the case to write, or what was just useless approach. I read and follow a lot of different 3D printing communities and what is my…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Perhaps something dealing with common problems in 3D printing Warping when using ABS Layers not sticking Stringing thin tall prints coming away from the bed etc
Parents
  • Nate1616
    Nate1616 over 10 years ago

    Thanks you all for the feedback.  It seams like the majority of you said that having some sort of modeling tutorials would be beneficial.  What tools specifically as there is endless amount to choose from?  Your average user would probably use something like Autodesk 123D, OpenSCAD, TinkerCAD (Autodesk Owned also).  Now you get into more complex software such as Autodesk Inventor, Blender, Sketchup, Revit, 3ds Max, Onshape (my favorite non Autodesk product).  Let me know what i should focus on as I'm pretty fluent in most listed except Blender. 

     

    Nate

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to Nate1616

    I tend to use Nemetschek Vectorworks Designer for 3D modelling. I think that the general modelling in 3D aspect is not too difficult and there probably are plenty of vendor tutorials on using the specific application however it is more the considerations you then have to apply to the model for it to become a successful 3D print.

     

    I've been working on a project design recently which will be externally printed through 3DHubs, so I don't know what machine it is going to end up on or the associated quirks. I've therefore created the 3D design so that it doesn't require any support structures and to keep tolerances fairly flexible, which will mean additional work after printing. However, recently I've seen some talk of using support structures which can be dissolved in soap solution, so presumably this is done with a two filament machine and potentially makes designs less restrictive.

     

    Guidelines for tolerances for fasteners would be quite useful. This project I've just done pilot holes which will need to be drilled and countersunk after printing, but perhaps it is possible to avoid that extra work. Perhaps accuracy is now good enough to use something like threaded inserts straight after printing.

     

    An overview of various tried and tested construction techniques might be useful. I suspect a lot of this may follow traditional woodworking joins but once again we need to know how machine/material tolerances are going to affect this. My recent project was done in two halves which will be butt jointed together allowing the use of a gasket as a spacer if necessary, however I did initially think about a lap joint for a neater finish and easier assembly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 10 years ago in reply to Nate1616

    I tend to use Nemetschek Vectorworks Designer for 3D modelling. I think that the general modelling in 3D aspect is not too difficult and there probably are plenty of vendor tutorials on using the specific application however it is more the considerations you then have to apply to the model for it to become a successful 3D print.

     

    I've been working on a project design recently which will be externally printed through 3DHubs, so I don't know what machine it is going to end up on or the associated quirks. I've therefore created the 3D design so that it doesn't require any support structures and to keep tolerances fairly flexible, which will mean additional work after printing. However, recently I've seen some talk of using support structures which can be dissolved in soap solution, so presumably this is done with a two filament machine and potentially makes designs less restrictive.

     

    Guidelines for tolerances for fasteners would be quite useful. This project I've just done pilot holes which will need to be drilled and countersunk after printing, but perhaps it is possible to avoid that extra work. Perhaps accuracy is now good enough to use something like threaded inserts straight after printing.

     

    An overview of various tried and tested construction techniques might be useful. I suspect a lot of this may follow traditional woodworking joins but once again we need to know how machine/material tolerances are going to affect this. My recent project was done in two halves which will be butt jointed together allowing the use of a gasket as a spacer if necessary, however I did initially think about a lap joint for a neater finish and easier assembly.