3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum What is the 3D printing community/group looking for?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 343 subscribers
  • Views 5311 views
  • Users 0 members are here
Related

What is the 3D printing community/group looking for?

Nate1616
Nate1616 over 10 years ago

I just wanted to get the communities opinion on what would be of useful content to have.  With the 3D Printing 101 courses being put on hold because of unfortunate events i would be willing to put something together.  Now this could be anything related to printing.  From how-to, maybe new product reviews, training courses...  Let me hear your thoughts.

 

Nate

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to Nate1616 +5
    I think the lack of activity in the 3D printing area is down to two factors: Relatively few people have a 3D printer (or access to one). There are a few good dedicated 3D printing community web-spaces…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to gadget.iom +4
    Paul, I agree with you. What has blocked me until now was just what was the case to write, or what was just useless approach. I read and follow a lot of different 3D printing communities and what is my…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Perhaps something dealing with common problems in 3D printing Warping when using ABS Layers not sticking Stringing thin tall prints coming away from the bed etc
Parents
  • Nate1616
    Nate1616 over 10 years ago

    Thanks for all the ideas!  Can someone from E14 put their input on what direction they would like to go or see?

     

    Nate

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to Nate1616

    3D printers cost about as much as a high end computer, so more people could afford them than actually purchase, because why?

    They are not as useful as a computer?

    They are too complicated to use - nobody who can afford one learned how in school?

    They don't produce things people want at a price they want to pay?

    They don''t produce items with high enough quality?

    I don't know - but now that I have one, I think it is a pretty high priority to have one.

     

    Your initiative could address some of these barriers or issues.

    For example, video instruction on how to design with a low cost CADD package would allow more people to to feel the design side is something they can handle.

    Maybe an explanation of how to use free models from the internet to print and where to get them.

    Maybe just some stories of how useful they can be would get people more interested.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to dougw

    Hi Doug,

     

    I think you hit the nail on the head, they are not perceived to have high quality, and to be honest most people have not seen the output from a 3D printer in real life.

    Until I did, I was extremely sceptical that it could be useful. Now that I have physically seen some output, I can see uses for it because it does reduce the barrier to make complex shaped objects. I still think they are overpriced though. It still feels primitive that many need spools of plastic and what still looks like a crude assembly of stepper motors or expensive fluids. When I was at school no-one had a paper printer (maybe a dot-matrix one!) and people used local stores or the library for their paper printing/copying needs, or a photo store for their photographs. It would be nice to see affordable 3D print or build services in local locations so people could pay to 'print' locally. I know there are online services but it defeats the 'green-ness' of 3D printing that you'd need to transport and ship items across the country or world, rather than produce locally.

     

    I don't see that a 3D print solution has to use the same technology to handle all materials, it could process materials separately and combine them with adhesives for instance), even if some parts are done manually. Intelligent software could auto-select a sheet material (e.g. wood) if large parts of the design needed a flat surface for instance. Or offer lower prices on certain material if that was in stock.

    In all likelihood basically some sort of automated 3D print solution that maybe too large and expensive for individuals but affordable enough for local firms to run.

    Today if I want a flat object (e.g. a front panel) there are firms that will offer that, and have their own requirements for how they want the design file. If I want a laser cut piece then I have to go somewhere else. And if I want metalwork folded etc then I have to go to another firm. It would be nice to be able to farm out parts of your design automatically to the nearest firms/individuals with the capabilities to build it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago in reply to dougw

    Hi Doug,

     

    I think you hit the nail on the head, they are not perceived to have high quality, and to be honest most people have not seen the output from a 3D printer in real life.

    Until I did, I was extremely sceptical that it could be useful. Now that I have physically seen some output, I can see uses for it because it does reduce the barrier to make complex shaped objects. I still think they are overpriced though. It still feels primitive that many need spools of plastic and what still looks like a crude assembly of stepper motors or expensive fluids. When I was at school no-one had a paper printer (maybe a dot-matrix one!) and people used local stores or the library for their paper printing/copying needs, or a photo store for their photographs. It would be nice to see affordable 3D print or build services in local locations so people could pay to 'print' locally. I know there are online services but it defeats the 'green-ness' of 3D printing that you'd need to transport and ship items across the country or world, rather than produce locally.

     

    I don't see that a 3D print solution has to use the same technology to handle all materials, it could process materials separately and combine them with adhesives for instance), even if some parts are done manually. Intelligent software could auto-select a sheet material (e.g. wood) if large parts of the design needed a flat surface for instance. Or offer lower prices on certain material if that was in stock.

    In all likelihood basically some sort of automated 3D print solution that maybe too large and expensive for individuals but affordable enough for local firms to run.

    Today if I want a flat object (e.g. a front panel) there are firms that will offer that, and have their own requirements for how they want the design file. If I want a laser cut piece then I have to go somewhere else. And if I want metalwork folded etc then I have to go to another firm. It would be nice to be able to farm out parts of your design automatically to the nearest firms/individuals with the capabilities to build it.

    • Cancel
    • Vote Up +3 Vote Down