3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum ReFILL-ament for 3D Printers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 345 subscribers
  • Views 5764 views
  • Users 0 members are here
  • amazon web services
  • frontpage
  • 3d_printing
  • 3d_printer
Related

ReFILL-ament for 3D Printers

abhijitnathwani
abhijitnathwani over 9 years ago

Hello everyone,

 

I have been working on a project that all of the 3D printer enthusiasts would definitely like! We often face trouble forgetting to place the order once our filament is coming to an end. Well, no more!

 

The Concept

ReFILL-ament is special Amazon DRS enabled device, that helps you calculate the usage of the filament for 3D printers, and re-orders itself when the filament is about to run out.

imageThe Basic Idea

 

All the 3D printers print the object using the filament, melting it and shaping it up as per the required specification. The filament is like the ink refill of our pen. Without refill ink, we cannot write and without the filament, we cannot print 3D objects.

So what happens, when we have thought of an idea! Prepared a 3D model for the same after many iterations, and we are eager to print it visualize our imagination. Until you realize that you don't have enough filament to print the object! That actually kills the imagination and the enthusiasm in us. So to avoid that embarrassing moment, ReFILL-ament takes care of your usage, and orders on your behalf, so that you never run out of filament and the new one arrives before the old runs out!

The basic idea is to create a completely standalone device that orders the filament on the preferences chosen earlier while configuring. The device would be packed in 3D printed enclosure so that it is easy to maintain it. Being USB-powered, there will be less of hassles!

ReFILL-ament reads the RFID card attached to the filament to identify which filament is currently under use. It also as an IR Array on the reverse. So, the design on the RFID card is made such a way that it cuts 3 IR in sequence. A combination of RFID information and a complete IR sequence helps the device to count the number of turns, and eventually estimate the remaining filament on the reel.

 

ReFILL-ament with my 3D-Printer

 

 

image

 

 

ReFILL-ament Setup with 3D-Printer

Following video shows the setup of ReFILL-ament with your 3D-Printer and register your ReFILL-ament device with Amazon DRS by the product registration web page.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

ReFILL-ament in Action

Following video shows how ReFILL-ament tracks usage of maximum three filament reel and place order on Amazon on your behalf when the quantity of any of three filaments is less than 30% using filament reel preference (ABS/PLA and Color) for each filament reel selected during ReFILL-ament Product registration process with Amazon DRS.

(NOTE: In this video 1 unwound is considered 1% usage just for demo purpose, in real use based on length/number of wounds of filament this percentage use can be set to actual)

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What is unique in ReFILL-ament?

  • Stand Alone device works with any 3D-Printer without even touch 3D-Printer.
  • Track usage of 3 filament spool and can be used to track more spools with little modification in the code.
  • USB powered device with Support of most of Amazon DRS API by ESP8266.
  • A meaningful status display on OLED Display.
  • if Internet connectivity not available then also tracks filament usage.
  • The Same project can be used for track any kind of spool usage and reorder the same. So it's not only applicable to 3D-Printer.
  • Low cost and easy Hardware design with easily available components makes this project really DIY so someone can easily replicate (Low-cost ESP8266 SoC, Low-cost sensors)
  • All current information (i.e. Filament UsageTokens, AP Credential, Slot Status) stored in EEPROM of ESP8266 every time it changes. So on every power cycleRefillament retains the latest information.
  • All Amazon DRS APIs implemented for ESP8266 SoC, Just Authorization Code generation done at Product Registration Webpage. So it will be easy for makers to implement the similar project without much knowledge of scripting...
  • Hardware Schematic, ESP8266 Firmware, and Product Registration web page source code all released in open source domain under CC-BY-SA license. So anyone can use this work or contribute.
  • Main philosophy used in this project is "Keep it As Simple As Possible" and "Put First Thing First" at the same time also considered end user aesthetics and ergonomics.

 

imageimage

imageimage

For more documentation visit here: https://www.hackster.io/abhijit-nathwani/refill-ament-for-3d-printers-261881

 

I would love to hear views from the community on the same.

 

Regards,

Abhijit Nathwani

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago +4
    The 3D printer dynamic filament monitor. Blog post at http://balearicdynamics.com/?p=604&preview=true Soon the project on Element14. Enrico
  • balearicdynamics
    balearicdynamics over 9 years ago +3
    ... and here is how it works. Videos will coming soon with the project on Element14 Filament monitor for Arduino – Balearic Dynamics Enrico
  • ravi_butani
    ravi_butani over 9 years ago in reply to balearicdynamics +2
    Hii Abhijit... Here my limited knowledge of math resulted in following solution for measure precise % filament usage..
Parents
  • sourgin
    sourgin over 9 years ago

    Hi, I'm new here and this is my first post read, as this also is my first reply.

     

    First of all if you have a new value for a trigger to chagne the configuration of the filament, so it records manually the first time when it's empty and use that as a base for the calculus? It will be, by a rute 66 lenght shorter to write, and easy for the user.

    Something like, ir1 read, ir2 noread, ir3 read will trigger "Store new rte count" so you now know how many revolutions where needed till the filament was consumed.

     

    In addition other way to do it, is the ye old way, a database that stores the data and users can contribute to it, So you have software updates :3 Evewyone loves a software update. And you have a file wich stores a keyword for the filament and it's rte (revolutions to end) values.

     

    So lets imagine that u have to program the arduino first, so you look at the database and select wich filaments are you going to use "I don't have a 3dprinter... for now :#" so I imagine that people don't switch filaments that fast "As per brand/model"

     

    So you can have something like this on the arduino code.

    filamentBase.c

     

    #define brand-type-weight rte;

    #define code number

     

    By this method, you can also made a change on the industry making the filamenters write down how many revolutions to the end of the filament where stored on a bobin. That would made them easy to control. And for the factory is easy to record, as they already have that value.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • abhijitnathwani
    abhijitnathwani over 9 years ago in reply to sourgin

    Hello sourgin,

     

    Thank you for your suggestions. These could be definitely looked upon.  I liked the idea where we could integrate the count in bobbin itself. Software updates also sound cool!

     

    Abhijit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • abhijitnathwani
    abhijitnathwani over 9 years ago in reply to sourgin

    Hello sourgin,

     

    Thank you for your suggestions. These could be definitely looked upon.  I liked the idea where we could integrate the count in bobbin itself. Software updates also sound cool!

     

    Abhijit