3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum 3D Printing: About the extruder choice
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 342 subscribers
  • Views 1440 views
  • Users 0 members are here
  • 3d printer
  • filament spool
  • abs
  • pla
  • issue
  • 3D Printing
  • dual-extruder
  • warning
  • filament
Related

3D Printing: About the extruder choice

balearicdynamics
balearicdynamics over 9 years ago

I write this short note, an abstract from the - in-print next October - issue of The Shed Magazine. I should admit that I had never though to this important detail without spending a lot of time in chat with rachaelp trying to understand and solve the problems of her first "dual extruder" 3D printer. Sometime sharing our own issues maybe one of the best forms of cooperation and knowledge sharing.

 

A dual-filament extruder maybe a trap, so please be careful! Dual filament does not mean that the extruder can pull one or the other filament depending on the design, instead it means that two filament spools are involved at the same time. If you try to use a dual filament extruder (that has a single nozzle) with a single lament feed, it will not work. Use a dual filament extruder only at times you choose to play with mixing colours together or if you plan to consume a lot of material.

 

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to balearicdynamics +1
    My response was based on this " If you try to use a dual filament extruder (that has a single nozzle) with a single lament feed, it will not work " I am pretty sure that if you only load up one filament…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Robert Peter Oakes +1
    You understood what is possible with my classical English mistakes Dual filament extruder is two wires together in a single extruder. What you mention instead is four-in-one. Yes your extruder will mix…
  • rachaelp
    rachaelp over 9 years ago in reply to Robert Peter Oakes +1
    As balearicdynamics says, I had a 2-in 1-out dual extrusion printer very briefly. The problem with these in my experience is that if you are only wanting to print in one colour you end up with a major…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Actually they do work and now there is already a 4 filament, one nozzle printer, the Prusa I3 MKII Multi Material

    Original Prusa i3 MK2 Multi Material upgrade kit

    I have seen this reviewed already and while it seems wasteful of filament due to a purge tower being used, it does work well

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    For those interested, you can download the models and print your own parts to create your own version. Prusa is fully open source.

    Enjoy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Robert Peter Oakes

    Sure Prusa is fully open source. Never told different.

     

    What you mention is a multi material extruder. As a matter of fact a double (or 4 units) extruder that is not a "dual" one. The first 3D printer versions of multi material was including two extruders (as many models has now). This generates a problems in reducing the effective printing area and recently there is this kind of extruders supporting multiple feeds (of different materials too) that includes in a single extruder group multiple supports. This is the first kind of alternative solution to multiple extruders and seems nice just because is saving 3D volume for printing.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to balearicdynamics

    My response was based on this "If you try to use a dual filament extruder (that has a single nozzle) with a single lament feed, it will not work"

    I am pretty sure that if you only load up one filament and try to print even though this one can handle 4, it will still work, maybe I just dont understand your comment ?

    Regards

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Robert Peter Oakes

    You understood what is possible with my classical English mistakes image

     

    Dual filament extruder is two wires together in a single extruder. What you mention instead is four-in-one. Yes your extruder will mix different materials and works independently; as a matter of fact - if I am not wrong - from the printing software you can select Extruder 1, 2, 3, 4 depending on what you are printing. In the case of dual extruder I mention, you just see ONE extruder in the printing software and it needs two filament feeds. The only advantage is that you can print randomly mixing two colours. Better than me this crap solution can be explained by rachaelp that owned one of them for some time.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Robert Peter Oakes

    You understood what is possible with my classical English mistakes image

     

    Dual filament extruder is two wires together in a single extruder. What you mention instead is four-in-one. Yes your extruder will mix different materials and works independently; as a matter of fact - if I am not wrong - from the printing software you can select Extruder 1, 2, 3, 4 depending on what you are printing. In the case of dual extruder I mention, you just see ONE extruder in the printing software and it needs two filament feeds. The only advantage is that you can print randomly mixing two colours. Better than me this crap solution can be explained by rachaelp that owned one of them for some time.

     

    Enrico