555 Timers
  • Technologies
  • More
555 Timers
Forum How to slow the charging and discharging of a 555 timer without changing the frequency.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 53 subscribers
  • Views 6434 views
  • Users 0 members are here
  • 63stratman-1
Related

How to slow the charging and discharging of a 555 timer without changing the frequency.

63stratman
63stratman over 5 years ago

Imagine driving at night and seeing a radio tower in the distance. At the top, a red light appears to brighten and dim instead of just blinking on and off. How can this effect be accomplished with a 555 timer? I assume the charging and discharging times must be increased, but I don't want to change the on/off frequency of around 1hz.

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 5 years ago +10 verified
    So, quickly hacking together something derived from the sort of things suggested by John and Doug, would this do what you want? Needs a large electrolytic value to get the timing, though, and not really…
  • fmilburn
    fmilburn over 5 years ago +7 suggested
    It sounds like you want to create something like a 1 second sine wave. A search on the internet for "555 timer sine wave" will turn up a number of hits. Edit: it requires a filter and won't be a perfect…
  • jw0752
    jw0752 over 5 years ago +6 suggested
    Hi Roger, Try putting a 1000 uF capacitor across the load on the output of the 555. You should also add an in series resistor to the output. Keep in mind if the light that you are trying to fade in and…
Parents
  • shabaz
    0 shabaz over 5 years ago

    Lots of ways to do this : ) but if you wish to stick with using 555's for this, yet another approach is to place a 4017 on the output, and it will generate 10 outputs, pulsed in sequence (you'll have to increase the 555 frequency from 1 Hz to 10 Hz, but the final output frequency from the overall circuit will still be 1 Hz). Then, by arranging 10 resistors as the top parts of a potential divider, and an eleventh resistor as the bottom part of a potential divider, you've got very near to a sinewave. (Use Excel to calculate the resistor values). A final output resistor and capacitor filter will perfect it. You'll need an op amp or similar as John mentions, to drive the LED, there won't be sufficient current from the filtered output to drive the LED directly. You could also consider PWM, that's a bit more advanced.

    Some handy parts for 555 experiments:

    ICM7555 (sometimes better than NE555)

    CD4017 or CD74HC4017 - counter with 10 outputs

    LM2901 - comparator

    MCP601 - op amp

    BC547 - NPN transistor

    BC557 - PNP transistor

    BSS138 - N-channel MOSFET

    BSS84 - P-channel MOSFET

    (Both of the MOSFETs are surface-mount but large enough to attach wire strands if desired, or solder onto a proto board adapter. Too hard trying to work around not using surface-mount, since it's the current reality that most parts are now surface mount).

     

    With parts from the above list, and resistors and capacitors, you should be able to come up with several different ways to implement your design.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago

    Lots of ways to do this : ) but if you wish to stick with using 555's for this, yet another approach is to place a 4017 on the output, and it will generate 10 outputs, pulsed in sequence (you'll have to increase the 555 frequency from 1 Hz to 10 Hz, but the final output frequency from the overall circuit will still be 1 Hz). Then, by arranging 10 resistors as the top parts of a potential divider, and an eleventh resistor as the bottom part of a potential divider, you've got very near to a sinewave. (Use Excel to calculate the resistor values). A final output resistor and capacitor filter will perfect it. You'll need an op amp or similar as John mentions, to drive the LED, there won't be sufficient current from the filtered output to drive the LED directly. You could also consider PWM, that's a bit more advanced.

    Some handy parts for 555 experiments:

    ICM7555 (sometimes better than NE555)

    CD4017 or CD74HC4017 - counter with 10 outputs

    LM2901 - comparator

    MCP601 - op amp

    BC547 - NPN transistor

    BC557 - PNP transistor

    BSS138 - N-channel MOSFET

    BSS84 - P-channel MOSFET

    (Both of the MOSFETs are surface-mount but large enough to attach wire strands if desired, or solder onto a proto board adapter. Too hard trying to work around not using surface-mount, since it's the current reality that most parts are now surface mount).

     

    With parts from the above list, and resistors and capacitors, you should be able to come up with several different ways to implement your design.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer