555 Timers
  • Technologies
  • More
555 Timers
Forum Bounce Servo with 555 timer
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 52 subscribers
  • Views 5975 views
  • Users 0 members are here
Related

Bounce Servo with 555 timer

Eric
Eric over 4 years ago

I want to toggle a servo with the push(and release) of a button.  I then want the servo to return to original position after x seconds.  I think I'm close by enlisting a 555 timer.  I have it successfully powering an LED for 1 second. (hold your applause)

Is this at least possible with this same circuit?  This is just a hobby project and I was trying to avoid grabbing an Arduino and coding something.

When I tried to connect my servo to pin 3, positive, and negative....it moved slightly once out of 10 attempts.  The LED is dimmer and shorter lived while the servo is attached.  

I should check back in here at least once a day until I get this working (and will report so) or smash the thing with a bat.

-EP

Some details...may be garbage.  THANKS IN ADVANCE!

Power = old 9v battery (8v)
Resistors = 10k
Cap = 100uf

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 4 years ago +4 verified
    Does this do what you wanted (sorry the video is a bit blurry)? community.element14.com/.../7411.MVI_5F00_3478.MOV Here's the circuit and the build on a breadboard the start position is controlled…
  • scottiebabe
    scottiebabe over 4 years ago in reply to jc2048 +3
    Neat little circuit. I wonder if I can upload .asc files on the new website. In the holiday spirit I put JC2048's deign into LTSpice for one to experiment with too. community.element14.com/.../1641.JC2048Servo…
  • dougw
    dougw over 4 years ago +2
    As @ scottiebabe points out it is a bit tricky but possible to do with 555 timers. You could make the middle waveform with a 556 (dual 555) - one 555 would generate a continuous square wave with 20 ms…
Parents
  • jc2048
    +1 jc2048 over 4 years ago

    Does this do what you wanted (sorry the video is a bit blurry)?

    Video processing failed.
    You don't have permission to edit metadata of this video.

    Here's the circuit and the build on a breadboard

    image

    image


    the start position is controlled by the 1k resistor under the 1N4148, the end position by the 470n capacitor
    controlled by the MOSFET (I actually used two 470n in parallel, so the circuit value's wrong), and the delay time
    after the switch is released is set by the 150k and the 10u.

    These are the output waveforms going to the servo, in case you're interested. First is the rest position, the second
    the position when the switch is pressed.

    image

    image

    Anyway, it will give you something to play with if you're interested in experimenting with a 555.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jc2048
    +1 jc2048 over 4 years ago

    Does this do what you wanted (sorry the video is a bit blurry)?

    Video processing failed.
    You don't have permission to edit metadata of this video.

    Here's the circuit and the build on a breadboard

    image

    image


    the start position is controlled by the 1k resistor under the 1N4148, the end position by the 470n capacitor
    controlled by the MOSFET (I actually used two 470n in parallel, so the circuit value's wrong), and the delay time
    after the switch is released is set by the 150k and the 10u.

    These are the output waveforms going to the servo, in case you're interested. First is the rest position, the second
    the position when the switch is pressed.

    image

    image

    Anyway, it will give you something to play with if you're interested in experimenting with a 555.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • scottiebabe
    0 scottiebabe over 4 years ago in reply to jc2048

    Neat little circuit. I wonder if I can upload .asc files on the new website. In the holiday spirit I put JC2048's deign into LTSpice for one to experiment with too.

    Fullscreen 1641.JC2048Servo.asc.txt Download
    Version 4
    SHEET 1 880 792
    WIRE -320 -32 -544 -32
    WIRE 0 -32 -320 -32
    WIRE 192 -32 0 -32
    WIRE 368 -32 192 -32
    WIRE -320 0 -320 -32
    WIRE -320 96 -320 80
    WIRE -224 96 -320 96
    WIRE -192 96 -224 96
    WIRE 80 96 48 96
    WIRE 368 96 368 -32
    WIRE 368 96 304 96
    WIRE -320 128 -320 96
    WIRE -192 128 -192 96
    WIRE 80 160 -96 160
    WIRE 448 160 304 160
    WIRE -768 176 -768 144
    WIRE -320 224 -320 192
    WIRE -192 224 -192 192
    WIRE 80 224 -32 224
    WIRE 448 224 304 224
    WIRE 0 288 0 -32
    WIRE 80 288 0 288
    WIRE 352 288 304 288
    WIRE -544 336 -544 -32
    WIRE -320 336 -320 304
    WIRE -240 336 -320 336
    WIRE -192 336 -192 304
    WIRE -192 336 -240 336
    WIRE -96 336 -96 160
    WIRE -96 336 -192 336
    WIRE -592 352 -720 352
    WIRE 352 352 352 288
    WIRE -320 384 -320 336
    WIRE -192 384 -192 336
    WIRE 48 416 48 96
    WIRE -720 432 -720 352
    WIRE 352 448 352 416
    WIRE -544 480 -544 416
    WIRE -192 512 -192 448
    WIRE -320 528 -320 448
    WIRE -32 528 -32 224
    WIRE 464 528 -32 528
    WIRE -720 544 -720 512
    WIRE -544 608 -544 560
    WIRE -448 608 -544 608
    WIRE -368 608 -448 608
    WIRE -544 640 -544 608
    WIRE -448 640 -448 608
    WIRE -320 672 -320 624
    WIRE -544 752 -544 720
    WIRE -448 752 -448 704
    FLAG 48 416 0
    FLAG 352 448 0
    FLAG 192 -32 VCC
    FLAG 448 160 DISCHARGE
    IOPIN 448 160 Out
    FLAG -192 512 0
    FLAG -320 672 0
    FLAG -240 336 CAP
    FLAG 448 224 CAP
    IOPIN 448 224 BiDir
    FLAG 464 528 OUT
    IOPIN 464 528 Out
    FLAG -544 752 0
    FLAG -448 752 0
    FLAG -592 400 0
    FLAG -768 176 0
    FLAG -720 544 0
    FLAG -768 64 VCC
    FLAG -224 96 DISCHARGE
    SYMBOL Misc\\NE555 192 192 R0
    SYMATTR InstName U1
    SYMBOL cap 336 352 R0
    SYMATTR InstName C1
    SYMATTR Value 100n
    SYMBOL res -336 -16 R0
    SYMATTR InstName R1
    SYMATTR Value 1.2k
    SYMBOL res -336 208 R0
    SYMATTR InstName R2
    SYMATTR Value 1k
    SYMBOL res -208 208 R0
    SYMATTR InstName R3
    SYMATTR Value 10k
    SYMBOL diode -304 128 M0
    SYMATTR InstName D1
    SYMATTR Value 1N4148
    SYMBOL diode -176 192 R180
    WINDOW 0 24 64 Left 2
    WINDOW 3 24 0 Left 2
    SYMATTR InstName D2
    SYMATTR Value 1N4148
    SYMBOL cap -208 384 R0
    SYMATTR InstName C2
    SYMATTR Value 470n
    SYMBOL cap -336 384 R0
    SYMATTR InstName C3
    SYMATTR Value 470n
    SYMBOL nmos -368 528 R0
    SYMATTR InstName M1
    SYMATTR Value AO6408
    SYMBOL cap -464 640 R0
    SYMATTR InstName C4
    SYMATTR Value 10�
    SYMBOL res -560 624 R0
    SYMATTR InstName R4
    SYMATTR Value 150k
    SYMBOL res -560 464 R0
    SYMATTR InstName R5
    SYMATTR Value 1k
    SYMBOL sw -544 432 M180
    SYMATTR InstName S1
    SYMATTR Value SX
    SYMBOL voltage -720 416 M0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V1
    SYMATTR Value PULSE(0 1 2 0 0 100m 1 1)
    SYMBOL voltage -768 48 R0
    WINDOW 123 0 0 Left 0
    WINDOW 39 0 0 Left 0
    SYMATTR InstName V2
    SYMATTR Value 6
    TEXT -72 728 Left 2 !.model SX SW(Ron=.1 Roff=1G Vt=0.5 Vh=1m)
    TEXT -930 776 Left 2 !.tran 10
    TEXT -392 -104 Left 4 ;JC2048 E14 Servo Design
    

    No luck with .asc, I had to add a .txt extension.

    image

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 4 years ago in reply to scottiebabe

    Thanks. An even easier way to experiment with it.

    It's interesting that there are all these spice models for 555 timers. Tina-TI has several in the part libraries that it comes with.

    Whilst I'm thinking about it, if anyone wants to actually build it, I used a BS170 for the MOSFET [a 2N7000 would also be fine]. I also had a 10uF electrolytic across the supply rails at the breadboard end - the servo is noisy (electrically), but it worked ok with a 6V supply. That was a small 'micro' servo. It might not be so happy with a larger one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Eric
    0 Eric over 4 years ago in reply to jc2048

    So, full disclosure, I inherited several pounds of components and am just getting my feet wet.  I think I saw some of those orange\black (diode?) pieces.  And I think another video labeled that  black 'D' shape a transistor.(EDIT: that is the mosfet. I had only seen them as rectangles)  I'll have to search for any mosfets.  I don't have a fancy power supply(yet) that I can dial in the voltage...so I'm just playing on a worn out 9v.  I think some math still works as I saw the 555 timer works with fractions of the power (1/3, 2/3).  THANKS for understanding my request!  Seems like this is an answer, but I want to attempt it first.  My personal attempt didn't go great, but I feel this is a working solution and have marked it as such. Thanks for all the quick replies and interest!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 4 years ago in reply to Eric

    A worn out 9V battery won't work too well with a servo. You'd do better with 4 fresh AA batteries for a fairly robust 6V. A low cost way to get the battery holder might be to look for an old consumer device and use the battery compartment (an old wrecked toy or radio, or something like that).

    Almost any small n-channel MOSFET would work here. I used the BS170 because I had some, but mentioned the 2N7000 because they're more common and people are more likely to have them. For the connections, look in the datasheet. Beware, though: the connections vary, so you do need to look them up - don't assume they're all the same. Here are the pinouts for the BS170 and 2N7000 and you can see that they're different.

    image

    image


    The circuit isn't very precise and the timing will vary as the supply voltage changes. I haven't helped by putting in the diodes to separate the charge and discharge path to get a short pulse time. For the diodes, 1N914 are common too and you may have some of those.

    You can extend the delay time by increasing either the 150k or the 10u next to it. If you go too far though, the return of the servo at the end will get more and more sluggish.

    One small problem with a servo is that it has a motor and can produce lots of electrical noise. That might affect the timing circuit. If you have any doubts, run the servo on a different supply (with the grounds still connected together) and see if that cures it. If it does, you'll need to clean up the supply to the timing circuit.