555 Timers
  • Technologies
  • More
555 Timers
Forum 555 timer bistable
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 49 subscribers
  • Views 2861 views
  • Users 0 members are here
Related

555 timer bistable

Psin545
Psin545 over 3 years ago

imageI have a question regarding some behaviour of a 555 timer circuit in bistable mode. I attached a photo I found off the internet that is the one I’m using, the output goes to a 440 ohm resistor and then to a red LED also I’m using 10k pull up resistors. I noticed when I push the trigger pin switch and the light comes on, that sometimes when my hand is hovering over the circuit the LED goes out. I got curious and made sure not to bang into anything or touch anything and I would slowly bring my hand near the circuit, and almost half or more of the time the LED would turn off. Being more curious now I took the breadboard set up like a “bridge” (basically I have two small bins and I had the breadboard laying across so each end of the breadboard is resting on those bins and there’s nothing touching the bottom of the breadboard) I noticed that if I put my hand under the breadboard (without touching it at all!) the LED light on the output pin goes out. Getting more curious I held the breadboard by the sides so there was minimal contact and the light would work perfectly fine until I ran my hand close to (but still not touching) the breadboard. I tried this on different surfaces such as plastic bins, slabs of wood, the floor (lol) and on a glass table. It did it the least amount of times when laying on the plastic bin. I’m not using a anti static wrist strap but I’m curious if this is an environment issue or like a workstation issue? Or a simple fix with a anti static strap? It was kind of neat to play around with it like that but now I wonder about the last 2 years and all the heart ache from circuits not working properly even though I was CERTAIN I had built them exactly as per the diagrams. Also I tried 5 different 555 chips and 5 different breadboards with the same results. Any ideas or suggestions? 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +6
    Hi, Not everything on the Internet is reliable. If you look at the datasheet of the chip , on page 10, you'll see the proper circuit. The clue (in case you're wondering how come I knew to check the…
  • dougw
    dougw over 3 years ago +6
    It looks like you have discovered a way to make a kind of proximity sensor. Maybe if you connect an otherwise unconnected wire to pin 6 it will be even more sensitive.
  • Psin545
    Psin545 over 3 years ago in reply to shabaz +2
    Thanks it’s funny cause after I posted this I went to lay down for a bit and as I was laying there I said to myself “you left pins floating” haha. I should of known better. I’ll check those links out though…
Parents
  • bidrohini
    bidrohini over 3 years ago

    Take a look at the Datasheet of 555 first. For further studies, you can see 

    Operational Amplifiers and Linear Integrated Circuits by  Robert F. Coughlin & Frederick F. Driscoll

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bidrohini
    bidrohini over 3 years ago

    Take a look at the Datasheet of 555 first. For further studies, you can see 

    Operational Amplifiers and Linear Integrated Circuits by  Robert F. Coughlin & Frederick F. Driscoll