Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog Deep-Sea Mining for Rare Earth Metals Could Help Solve the Climate Crisis
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 1 Oct 2021 6:37 PM Date Created
  • Views 2896 views
  • Likes 0 likes
  • Comments 3 comments
  • mining
  • environment
  • future
  • rare earth
  • cabeatwell
  • innovation
Related
Recommended

Deep-Sea Mining for Rare Earth Metals Could Help Solve the Climate Crisis

Catwell
Catwell
1 Oct 2021

image

The seabed is loaded with trillions of polymetallic nodules, an amalgamation of cobalt, nickel, manganese and other rare earth metals that could help with the climate crisis. (Image credit: The Metals Company)

 

Three miles below the Pacific Ocean lies trillions of tiny black nuggets that could provide a solution to the climate crisis and bolster green energy but could dramatically impact the environment. Those nuggets are polymetallic nodules composed of cobalt, nickel, manganese and other rare earth metals formed via a biochemical process where shark teeth and fish bones become encased by minerals. The natural process is done throughout millions of years and eventually settles on the ocean floor.

 

Australia-based The Metals Company state those nuggets are essentially “a battery in a rock” and an easy way to help solve climate change. The company recently announced that it derived an alloy of high-grade battery metals from its initial smelting campaign, which relies on rotary kiln technology to produce the metals. The process is derived from conventional nickel flowsheets that separate the base metals encased in the nodules into two concentrated streams. The first produces an alloy comprised of critical metals crucial for EV batteries and wiring, including nickel, cobalt, and copper. The other stream is composed of manganese silicate that can be further processed to manganese alloy, a critical component in steel production.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Metals Company states there are enough polymetallic nodules to produce 4.8-billion electric vehicles, or instead the batteries that power them. They could also be used to produce energy-dense batteries for grid energy storage, allowing green energy a long-term storage solution. Mining those nuggets would be as simple as vacuuming golf balls off of a putting green.

 

Some biologists feel harvesting those polymetallic nodules could have an environmental impact that is yet unknown and may produce a cascading effect that worsens the current trajectory of climate change. The extraction process is minimally invasive to the environmental area they are being harvested from, but the world’s oceans are contiguous with currents navigating the globe. So, while there may be minimal impact at one site, another could have catastrophic damage if the polymetallic nodule variable is removed. It’s still too early to tell what those consequences, if any, might be without further study, but if there is negligible impact, we may see a solution that combats climate change in the near future.

 

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 5 years ago

    Big claim unsubstantiated in the provided video.

     

    I agree that we could potentially find large amounts of harvestable metals on the ocean floor, but it would take a significant expenditure in fossil fuels to make the harvesting equipment, transport it to a work site and then collect and return the metals for processing.

     

    Yes, you can potentially make large numbers of batteries with the metals, but at what cost?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Big claim unsubstantiated in the provided video.

     

    I agree that we could potentially find large amounts of harvestable metals on the ocean floor, but it would take a significant expenditure in fossil fuels to make the harvesting equipment, transport it to a work site and then collect and return the metals for processing.

     

    Yes, you can potentially make large numbers of batteries with the metals, but at what cost?