Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog Lenovo And Qualcomm Introduce A Laptop That Has An ARM But No Leg
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ipv1
  • Date Created: 30 May 2019 3:48 AM Date Created
  • Views 938 views
  • Likes 6 likes
  • Comments 2 comments
  • inovation
  • computex
  • laptop
  • arm
  • news
Related
Recommended

Lenovo And Qualcomm Introduce A Laptop That Has An ARM But No Leg

ipv1
ipv1
30 May 2019

When the Raspberry Pi was introduced in the classroom as a viable desktop replacement, many were skeptical to the processing power and software ecosystem that came with the single board computer. Then came the Pitop and things have never been the same. Enter Computex 2019 on 26th May in Taipei, where the future of technology is showcased and one of the unexpected demos was Qualcomm Snapdragon 8cx and it's partnership with Lenovo. Codenamed Project Limitless, a 2-in-1 laptop was on display that is powered by Snapdragon SOC and runs Windows 10 no less. It looks like the Yoga convertible that has induced mixed feelings in the users.

 

image

 

So this was bound to happen right? The kicker is the benchmarks using PCmark10, according to which the 8cx actually beats an 8th Generation i5 while running MS Office applications. The Snapdragon was running these apps in emulation so the numbers are even more impressive. When it comes to battery life, well it is just not fair competition and we hope that we can get our hands on one soon. The demo unit had the X55 5G modem as part of the always connected theme and we cannot help but wonder what this means for the future of portable computers this holiday season.

 

 

As far as the app development is concerned, the cross platform framework Electron will be supporting ARM on Windows later this year. Electron is the same technology that powers Visual Studio Code as well as desktop clients for the like of Slack and Discord. On the gaming end, Unity is being recompiled for ARM and the results are promising.

 

So the question is, will you be looking at ARM portables to replace your laptop or will you wait till more manufacturers come up with similar offerings.

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 7 years ago +2
    Aren't many Chromebooks using an ARM processor? The Snapdragon 8c is interesting and the Adreno 680 GPU is impressive supporting OpenGL-ES 3.2 and Direct3D 12 for Windows. It has been interesting to see…
  • clem57
    clem57 over 7 years ago +1
    I am impressed to say the least. Here are the specs: Latest DirectX 12 API Advanced Camera and Video capabilities: Cinema core with VP9 & H.265 decoder and 2nd Gen HDR Playback; High efficiency video encoder…
  • clem57
    clem57 over 7 years ago

    I am impressed to say the least. Here are the specs:

     

     

    • Latest DirectX 12 API

       

    • Advanced Camera and Video capabilities: Cinema core with VP9 & H.265 decoder and 2nd Gen HDR Playback; High efficiency video encoder

    • Dual 4K external displays

    • Connected Standby / Instant On

    • Multi-gigabit speeds for virtually seamless cloud connectivity/computing: up to 2Gbps LTE

    • Location Aware for app accuracy

    • Wi-Fi: MU-MIMO, Multi-gigabit Wi-Fi, Dual-band simultaneous (DBS), Integrated baseband

    • 4th Generation Qualcomm AI Engine

    • Enhanced voice assistant experiences for Alexa and Cortana with Qualcomm Aqstic technology

    • Supports all versions Windows 10 (Enterprise, Pro, Home)

    • Improved crypto-security

    • Remote management and location awareness for enterprise efficiency

    • Advanced location features:
      • Low Power Geofencing and Tracking
      • Sensor-assisted Navigation
      • Pedestrian Navigation
    • Sensors: Qualcomm All-Ways AwareTm technology

    • Charging: QualcommRegistered Quick ChargeTm 4+ technology

     

    Specifications

    5G

    5G Chipset: QualcommRegistered SnapdragonTm X55 Modem

    5G Technology: 5G NR

    5G Spectrum: mmWave, sub-6 GHz, 5G/4G spectrum sharing

    5G Modes: FDD, TDD, SA (standalone), NSA (non-standalone)

    5G mmWave specs: 800 MHz bandwidth, 8 carriers, 2x2 MIMO

    5G sub-6 GHz specs: 200 MHz bandwidth, 4x4 MIMO

    5G Peak Download Speed: 7 Gbps

    5G Peak Upload Speed: 3 Gbps

    5G RF: 100 MHz envelope tracking, Adaptive antenna tuning

     

     

    CPU

    CPU Cores: QualcommRegistered KryoTm 495 CPU, Octa-core CPU

    CPU Architecture: 64-bit

     

     

    Process

    Process Technology: 7 nm

     

     

    DSP

    DSP Technology: QualcommRegistered HexagonTm 690 Processor, Qualcomm All-Ways AwareTm technology

     

     

    Cellular Modem

    Modem Name: QualcommRegistered SnapdragonTm X24 LTE modem

     

     

    LTE Category

    Downlink LTE Category: LTE Category 20

     

     

    LTE Downlink Features

    Downlink LTE Streams: Maximum 20 spatial streams

    Downlink Carrier Aggregation: 7x20 MHz carrier aggregation

    Downlink LTE MIMO: Up to 4x4 MIMO on five carriers, Full-Dimension MIMO (FD-MIMO)

    Downlink QAM: Up to 256-QAM

     

     

    LTE Uplink Features

    Uplink Technology: QualcommRegistered SnapdragonTm Upload+, Uplink Data Compression (UDC)

    Uplink Carrier Aggregation: 3x20 MHz carrier aggregation

    Uplink LTE Streams: Up to 2x 106Mbps LTE streams

    Uplink QAM: Up to 256-QAM

     

     

    LTE Speed

    LTE Peak Download Speed: 2 Gbps

    LTE Peak Upload Speed: 316 Mbps

     

     

    Cellular Technology

    Cellular Technology: WCDMA (DB-DC-HSDPA, DC-HSUPA), TD-SCDMA, CDMA 1x, EV-DO, GSM/EDGE

    LTE Technology: LTE FDD, LTE TDD including CBRS support, LAA, LTE Broadcast

     

     

    Wi-Fi

    Wi-Fi Standards: 802.11ad, 802.11ac Wave 2, 802.11a/b/g, 802.11n

    Wi-Fi Spectral Bands: 2.4 GHz, 5 GHz, 60 GHz

    MIMO Configuration: 2x2 (2-stream)

     

     

    Bluetooth

    Bluetooth Version: Bluetooth 5.0

     

     

    NFC

    Near Field Communications: Supported

     

     

    Location

    Satellite Systems Support: Beidou, Galileo, GLONASS, GPS, QZSS, SBAS

    Location Support: QualcommRegistered Location

    Global Emergency Services Support: Assisted GPS, OTDOA (LTE-based positioning)

     

     

    RF

    RFFE: QualcommRegistered RF Front-End (RFFE) solution, High-power transmit (HPUE), QualcommRegistered Adaptive Antenna Tuning

     

     

    USB

    USB Version: USB 3.1

     

     

    Camera

    Image Signal Processor: Qualcomm SpectraTm 390 image signal processor, Dual 14-bit ISPs

    Dual Camera: Up to 16 MP

    Single Camera: Up to 32 MP

    Video Capture (30 FPS): 4K HDR video capture, 4K Ultra HD video capture

    Slow Motion Video Capture: 720p @ 480 FPS

     

     

    Video

    Video Playback: Up 4K HDR @ 120fps

    Codec Support: H.265 (HEVC), H.264 (AVC), VP9

    Video Software: Rec. 2020 color gamut video capture, Up to 10-bits per color video capture

     

     

    Display

    Max On-Device Display: 4K Ultra HD

    Max External Display: Two 4K Displays

     

     

    General Audio

    Audio Technology: Qualcomm TrueWirelessTm Technology, QualcommRegistered Broadcast Audio technology, Qualcomm AqsticTm audio technology, QualcommRegistered aptXTm audio technology

    QualcommRegistered aptXTm audio playback support: QualcommRegistered aptXTm, QualcommRegistered aptXTm HD

     

     

    Audio Playback

    Channel output: Surround Sound

    Speaker protection: Speaker protection

     

     

    GPU

    GPU Name: QualcommRegistered AdrenoTm 680 GPU

    API Support: DX12

     

     

    Memory

    Memory speed: 2133MHz

    Memory Type: LPDDR4x, 8 channels

     

     

    Storage

    SSD: NVME SSD

    UFS: UFS 3.0

     

     

    *Requires network connection and compatible network.

    ** Battery life varies significantly with settings, usage, and other factors

    Qualcomm Snapdragon, Qualcomm Adreno, Qualcomm Aqstic, Qualcomm Kryo, Qualcomm AI Engine, Qualcomm All-Ways Aware, Qualcomm Quick Charge, Qualcomm Hexagon, Qualcomm Snapdragon Upload+, Qualcomm Spectra, Qualcomm RF Front End, Qualcomm Adaptive Antenna Tuning, Qualcomm Location, Qualcomm Spectra, Qualcomm TrueWireless, Qualcomm Broadcast Audio and Qualcomm aptX are products of Qualcomm Technologies, Inc. and/or its subsidiaries.

     

    From: https://www.qualcomm.com/products/snapdragon-8cx-compute-platform

    My summary:

     

    QualcommRegistered KryoTm 495 CPU, Octa-core CPU.

         A 7nm process tech chip with incredible 7-watt TDP allowing multiple days on 1 battery charge.

         The new Adreno 680(GPU), which doubles the memory interface from 64 bits to 128 bits.

     

    Read more at https://hothardware.com/news/snapdragon-8cx-acpc-windows-10-on-arm-kryo-495#aEQ4VmiAsRZwt00E.99

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago

    Aren't many Chromebooks using an ARM processor?

     

    The Snapdragon 8c is interesting and the Adreno 680 GPU is impressive supporting OpenGL-ES 3.2 and Direct3D 12 for Windows.  It has been interesting to see the evolution of the ARM processor where even HP took a shot, or Moonshot, at creating an ARM based server. I think it is just a matter of time when these start taking a bigger chunk out of the Intel hold on the CPU market.  I do believe they have an ARM fab somewhere I suppose just to be ready. 

     

    At a lower end, I've had my eye on a Pinebook Pro which sports a Rockchip RK3399 SOC with Mali T860 MP4 GPU at a $199 US price range.