Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog The Senate Approves Bill S. 1885 for Autonomous Vehicle Safety Exemptions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 6 Oct 2017 4:25 PM Date Created
  • Views 1136 views
  • Likes 2 likes
  • Comments 4 comments
  • cabatwell
  • hmi
  • law
  • rules
  • artificial intelligence
  • senate
  • government
  • usa
  • ai
  • safety
Related
Recommended

The Senate Approves Bill S. 1885 for Autonomous Vehicle Safety Exemptions

Catwell
Catwell
6 Oct 2017

image

Nissan Autonomous Drive. (Image credit Norbert Aepli via Wiki Commons)

 

I asked, is Artificial Intelligence really a threat? Well...

 

The Senate Committee on Commerce, Science, and Transportation voted to pass Bill S. 1885- The American Vision for Safer Transportation through Advancement of Revolutionary Technologies (AV START) Act, which was introduced by Senator John Thune (R-SD) and is supposed to advance efforts to improve roadway safety through the development of autonomous vehicles.

 

What the bill does in a general overview is to allow automobile manufacturers pursue safety exemptions for autonomous vehicles based on production volume, while allowing individual states the ability to regulate registration, licensing, safety and insurance for said vehicles. This allows the Senate to establish what they call ‘a balance between federal and state laws affecting self-driving vehicles.’

 

What’s more, the bill offers several amendments with one that includes legislation to reform the TSA (Transportation Security Administration) to establish a ‘National Suicide Prevention’ hotline presumably to help prevent employees (or anyone else) of the agency from committing suicide in said AVs. Regardless, those safety exemptions are based on production volume, which is capped for each manufacturer at 15,000 the first year, 80,000 over the next three and no cap in the fourth. The bill also exempts self-driving semi tractor-trailers due to various labor unions aversions about the safety and job security regarding truckers, which are vehemently opposed to the technology altogether.

 

Companies such as GM, Ford and Alphabet Inc. have been lobbying for some time for the landmark legislation as a way to increase revenue from auto sales even though safety groups urged for more safeguards, which this bill puts into states hands regarding those regulations mentioned earlier. While some fear the bill could stymie AV development (especially in trucks) and isn’t yet sophisticated enough to relinquish control, others see this as the first stone laid in the foundation of AV rules and regulations designed at advancing the technology.

 

At least that’s what Senator Thune and other members think stating, “Today’s vote underscores the bipartisan desire to move ahead with self-driving vehicle technology.” He goes on to add, “Sen. Peters and the members of the Commerce Committee deserve credit for working together to move this bill forward toward Senate floor consideration and collaboration with our colleagues in the House of Representatives. The safety and economic benefits of self-driving vehicles are too critical to delay.”

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Being disabled, I actually like the idea of a self driving vehicle. Self driving trucks are a mixed bag, especially the big semi's. Whenever you have 100,000 pounds of payload running at highway speeds…
  • Catwell
    Catwell over 8 years ago in reply to ntewinkel +2
    Combine self-driving with "death-proof" cars, and I'm sold. C
  • ntewinkel
    ntewinkel over 8 years ago in reply to DAB +1
    I totally agree with all you've said, DAB. I've recently done a few road trips that took about 3 hours of driving, and it would have been great to just sit back and let the car do the driving! I might…
Parents
  • DAB
    DAB over 8 years ago

    Being disabled, I actually like the idea of a self driving vehicle.

     

    Self driving trucks are a mixed bag, especially the big semi's.  Whenever you have 100,000 pounds of payload running at highway speeds, you have a large potential pile driver into traffic.

     

    As with anything, time will tell if the technology is ready for adoption.

     

    I personally would not want to face the teamsters union when they realize that jobs will be lost.  I can imagine that there will be sabotage issues if that is the case.

     

    I can envision that autonomous vehicles could make traffic safer as they can be programmed to actually follow traffic laws.

     

    The biggest problem will be bad drivers interacting with the vehicles by erratic movements, which could confuse the AI program into an unfortunate vehicle correction cycle.

     

    As the old Chinese curse says "May you live in interesting times!"

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to DAB

    I totally agree with all you've said, DAB.

     

    I've recently done a few road trips that took about 3 hours of driving, and it would have been great to just sit back and let the car do the driving!

    I might even feel safer on the winding mountain roads to the other side of the island.

     

    I find it really sad that a labour union should have the power to stop great technology, just for fear of losing jobs. I have a feeling that a self driving truck would be much safer than an over-tired truck driver near the end of a shift.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 8 years ago in reply to DAB

    I totally agree with all you've said, DAB.

     

    I've recently done a few road trips that took about 3 hours of driving, and it would have been great to just sit back and let the car do the driving!

    I might even feel safer on the winding mountain roads to the other side of the island.

     

    I find it really sad that a labour union should have the power to stop great technology, just for fear of losing jobs. I have a feeling that a self driving truck would be much safer than an over-tired truck driver near the end of a shift.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 8 years ago in reply to ntewinkel

    Combine self-driving with "death-proof" cars, and I'm sold.

     

    C

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to Catwell

    >"death-proof" cars

    Isn't that kinda like how it's impossible to make things "fool-proof" because fools are so ingenious?