Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog The US Is Pushing for More Coal Power but Are the Returns Worth the Investment?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 Mar 2018 5:35 PM Date Created
  • Views 1373 views
  • Likes 4 likes
  • Comments 3 comments
  • business of engineering
  • government
  • fossil fuels
  • cabeatwell
  • grid
  • coal
  • power
  • energy
  • business
Related
Recommended

The US Is Pushing for More Coal Power but Are the Returns Worth the Investment?

Catwell
Catwell
7 Mar 2018

image

(Image credit: Greg Goebel via Wikipedia)

 

In the US, there is new investment into the declining coal industry as America’s leading power producer, which is now dominated by natural gas, accounting for 34% of the country’s electricity. To put that into perspective, as of 2016 coal produces 30% of US power followed by nuclear at 20%, renewables (solar, wind, hydro, etc.) at 15% and petroleum at 1%, according to the US Energy Information Administration (EIA).

 

There are several reasons why coal-fired power plants are in decline, with the foremost being pollution- burning coal is responsible for 42% of mercury emissions in the US, with the fleet producing 45,676 pounds in 2014 alone according to the EPA. It also creates 3.1-million tons of sulfur dioxide (acid rain), 1.5-million tons of nitrogen oxides (lung irritants) and 197,286 tons of particulate matter or soot. It is also responsible for producing other harmful substances such as lead, arsenic and carbon monoxide, making it bad for both the environment and humans.

 

Another detrimental impact resulting from burning coal is the release of greenhouse gases- primarily carbon dioxide and methane, which contributes profoundly to the issue of global warming. Out of all the dangers of using coal to generate power, global warming is the most harmful, long-term and irreversible. The effects of global warming results in severe consequences to the planet- rising temperatures and rising sea levels will help drive intense storms and drought along with the extinction of many species of animals as their natural habitats become inhabitable. According to a 2015 study from the Carnegie Institute for Science, the emissions from burning a lump of coal affects the climate 100,000-times greater than the heat it produces, and the heat that’s trapped by those emissions can be felt within several months of it being burned.

 

image

East-Central China covered in a layer of smog in November of 2004; produced by vehicle pollution, coal-fired power plants and home heating. (Image credit: NASA)

 

Pre-2016, the EPA enacted the Clean Air Act and Clean Water Act to limit the amount of emissions coal plants could release into the environment based upon their wattage output or efficiency, which the national average ranges to be around 32 to 42% for coal while natural gas hovers between 32 to 38% and nuclear at 38%. Those percentages are low when compared to hydro-electric, which ranges from a staggering 85 to 90%, according to data from Bright Hub Engineering. That being said, most coal plants are required to install filters to limit the amount pollutants that enter the environment or suffer penalties and fines, which are outlined in both Acts mentioned earlier.

 

It’s widely known that the Trump administration believe global warming to be a trend rather than a humanmade occurrence, which resulted in the US pulling out of the Paris Climate Accords early last year. Combined with references of removing ‘climate change’ and ‘global warming’ from governmental agencies, and the appointment of Scott Pruitt (climate change skeptic) to head the EPA, those environmental protection Acts (including the Stream Protection Act) are in danger of being repealed to favor coal production and processing. In fact, there are 60 environmental rules that are or in the process of being repealed in the efforts to promote the increased use of fossil fuels, based on research findings from the Columbia Law School and Harvard Law School.

 

image

The US has roughly 3.9-trillion short tons of coal reserves, enough to last for 283 years. (Image credit: CSIRO via Wikipedia)

 

Environmental impact point’s aside; it becomes clear why the US is looking to power its grid with coal. It is estimated the US sits on approximately 3.9-trillion short tons (2,000 pounds) of coal, enough to last 283 years. EIA projections show coal becoming cheaper over natural gas in the near future based on current trends, with the most current data showing natural gas averaged $21.30 per MWh (Miliwatt hour) with coal ranging between $21 and $23 per MWh and is set to fall.

 

Even though those prices are expected to drop, a large number of coal plants in the US have or supposed to be retired from the fleet, some of which have already been reconfigured for natural gas or have closed outright. An estimated 25,000 to 60,000 megawatts generated from coal plants are expected to be retired from service, and the numbers continue to grow as more utilities favor natural gas and renewable energy sources.

 

image

Retired coal units based on private, merchant and regulated entities from 2007 to 2016. (Image credit: Kleinman Center for Energy Policy)

 

Coal-fired power plants have been on a steady decline over the last decade due in part to the Obama administration’s strict EPA regulations. Utilities found it to be more cost effective to convert their plants from coal in favor of natural gas due to those rules and more continue to shutter their doors. To put the numbers of closed plants into perspective- from 2007 to 2016, 531 coal plants (representing 55.6GW) were retired, nearly one every 15 days according to the Kleinman Center for Energy Policy.

 

If we use the Kleinman report as a model and apply it to the question of whether or not the US should increase investments into coal-based power plants, the utilities have given us the answer with a resounding no. Even China (the world’s largest consumer of coal) is switching over to renewables at an increased rate, vowing to spend $360-billion over the next two years on renewable power sources as an effort to improve the country’s air quality, which caused 366,000 premature deaths in 2013 alone, according to a report from US and Chinese scientists. With all of the studies, reports, and projections, with the utilities already heavily invested in renewable energy sources, the returns will never be worth the investment when it comes to coal-produced power.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 8 years ago +2
    This topic is so ripe with politics that even it's existence as an issue is the arena of the ill informed. Despite reported coal supplies, there is no such thing as "clean" coal. I read two weeks ago that…
  • DAB
    DAB over 8 years ago +1
    There are so many other uses for coal, that just burning it is a terrible waste. I understand many countries still use coal because it is what they have, but the effects on the population are devastating…
  • three-phase
    three-phase over 8 years ago in reply to DAB +1
    I believe Germany is using coal as its bridging technology to its low carbon energy production policy since the phasing out of nuclear following on from the Fukushima incident. I fully agree with your…
  • three-phase
    three-phase over 8 years ago in reply to DAB

    I believe Germany is using coal as its bridging technology to its low carbon energy production policy since the phasing out of nuclear following on from the Fukushima incident.

     

    I fully agree with your comments regarding spent nuclear full rods. There are molten salt reactors that can make use of the spent rods from the existing nuclear plants. I don't believe they yet have a design sanctioned by any nuclear authority.

     

    Waste Annihilating Molten Salt Reactor

     

    I would suspect that future Grids will move more towards hybrid systems, including renewable technologies such as solar, wind and tidal mixed with storage facilities in the form of batteries and heat pumps alongside gas, coal and nuclear that will slowly be phased out as Grids change from a centrally powered large generation systems to a more interconnected smaller embedded systems.

     

    The main problem is that technologies are only developed if there are commercial benefits and not for the power stability or renewable energy aspect hence the requirement for government based subsidies.

     

    Kind regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago

    There are so many other uses for coal, that just burning it is a terrible waste.

     

    I understand many countries still use coal because it is what they have, but the effects on the population are devastating. See China and India as prime examples.

     

    I was surprised to see that Germany still uses a lot of coal, but they have very few options.

     

    Is there a solution, it depends upon what people are willing to pay. Face it, coal is relatively inexpensive to mine and use. Other fuels are more expensive on an increasing scale.

     

    There is no easy answer. Solar and wind can help, but both are inconsistent.

     

    We could use nuclear fuel, but we need to greatly improve its efficiency so we stop wasting 99% of the energy, which is why we have so much nuclear "waste!"

     

    There are ways to recycle the nuclear fuel rods, which are a really stupid way to run a reactor, we just need to stop thinking of it as waste and realize that it is a resource.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 8 years ago

    This topic is so ripe with politics that even it's existence as an issue is the arena of the ill informed.

     

    Despite reported coal supplies, there is no such thing as "clean" coal. I read two weeks ago that coal miners are surging with black lung disease because the type of coal being mined is from thinner veins and is bordered by silica which these dudes are breathing. Not that clean, I guess.

     

    There are enough natural gas reserves that do not dirty up the environment and cause respiratory problems.

     

    But the most important thing for people who are in technology is that it pulls attention from the huge wins and development that is on going in alternative energy sources. Ask the average guy on the train how much energy is supplied today by solar and wind and you'll likely get a hmm and I dunno or may be 1%.  The facts are:

     

    The U.S. set a new renewable energy milestone in March, in data released Wednesday. For the first time, wind and solar accounted for 10 percent of all electricity generation, with wind comprising 8 percent and solar coming in at 2 percent. The report was published by the U.S. Energy Information Administration (EIA), which collects and disseminates environmental data that is used to inform policymakers.