Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog Three ways modern engineering could help save the world
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 22 Nov 2016 6:31 PM Date Created
  • Views 1151 views
  • Likes 0 likes
  • Comments 4 comments
  • sustainable engineering
  • sustainability
  • solar airplane
  • solar energy
Related
Recommended

Three ways modern engineering could help save the world

jlucas
jlucas
22 Nov 2016

Engineering has a complicated relationship with the environment. By-products of manufacturing such as carbon fuel emissions and deforestation may have made an unfortunate contribution to many of the problems our planet is currently facing, but it's also engineers and innovators who are making some of the most significant strides towards addressing those problems.

 

Here are three important ways in which engineers are leading the way in terms of making our planet healthier and more sustainable for all.

 

Providing Access to Clean Water for All

 

image

 

Around 750 million people - almost 2.5 times the population of the United States of America - currently lack access to clean, drinkable water. A growing population and declining water supplies threaten to intensify this problem, presenting a potential global crisis in the coming decades. However, engineers aren't giving up hope.

 

One example of a persistent and creative advocate for clean water access in the engineering space is Dean Kamen. Along with his team of engineers, Kamen created the Slingshot, a water purification device that uses a Sterling engine to convert nearly any contaminated water into suitable drinking water. An important feature of the device is its ability to use a wide variety of items as a fuel source, including widely available resources such as manure. Although much more needs to be done to overcome water scarcity, low-cost and low-maintenance devices such as the Slingshot provide engineers with a model of success to improve and expand upon in the future.

 

Pioneering Affordable Solar Energy

image

 

In the same way that availability of clean water is diminishing, a depleted supply of fossil fuels has forced engineers to seek alternative sources of energy. As the cleanest and most abundant renewable energy source available, solar energy has the potential to solve our energy crisis once and for all, if it can be harnessed in an efficient and cost-effective manner.

 

Commercial solar cells convert sunlight into electricity with an efficiency of only 10 to 20 percent which, when factoring in the cost of manufacturing solar cells, can actually raise the price of electricity. Before solar energy cells ever become a common sight in households everywhere, questions surrounding cost and effectiveness must be addressed. But significant progress is being made, and with the help of the engineers working tirelessly on new, more efficient ways to harness it, solar still has a major role to play in the future of our relationship with the modern world.

 

Developing Zero-emission Aircraft

 

image

 

Aviation currently accounts for 11% of carbon emissions from transportation, and 2% of all world emissions, and is growing rapidly, presenting a serious problem to an increasingly globally connected world. However, the next major chapter in humanity's relationship with air travel may not be too far off in the distance. Between March 2015 and July 2016, the Solar Impulse - a long-range experimental solar-powered aircraft project, became the first aircraft to make it around the world without fuel. The journey took 17 legs and encountered several problems, but it proved what can be achieved when dedication and innovation meet. Perhaps in the future, all air travel will be powered by renewable energy, helping us all to travel around our planet without causing her unnecessary damage.

 

Can engineering really save the world? Tell us about your favourite environmentally-friendly innovations in the comments section below...

  • Sign in to reply
Parents
  • DAB
    DAB over 9 years ago

    First, creating clean water is pretty easy using a rudimentary solar still.

     

    I am aghast that every house does not use one.

     

    Planting trees on the roofs of all large buildings and using life grass or plants on the roofs of all houses would greatly clean the air naturally.

     

    We could easily use dirigibles for transportation if people did not need to go as fast as modern aircraft.

     

    Everything that you consider bad has solutions, but politicians are unwilling to do what makes sense because it takes too long to show progress.

     

    If you took the money being wasted on carbon capture initiatives, you could solve all of these problems in short order.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    First, creating clean water is pretty easy using a rudimentary solar still.

     

    I am aghast that every house does not use one.

     

    Planting trees on the roofs of all large buildings and using life grass or plants on the roofs of all houses would greatly clean the air naturally.

     

    We could easily use dirigibles for transportation if people did not need to go as fast as modern aircraft.

     

    Everything that you consider bad has solutions, but politicians are unwilling to do what makes sense because it takes too long to show progress.

     

    If you took the money being wasted on carbon capture initiatives, you could solve all of these problems in short order.

     

    DAB