Business of Engineering
  • Technologies
  • More
Business of Engineering
Forum If I Had a Hammer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 245 subscribers
  • Views 6410 views
  • Users 0 members are here
Related

If I Had a Hammer

jack.chaney56
jack.chaney56 over 9 years ago

I used this as a clever draw to get more readers.  The actual intent is to start a discussion and get input from people for software.  Most of the discussions I have seen on the site are about inventing hardware solutions to popular problems.  I guess I am getting overloaded with how many ways there are to turn on an LED.  A significant amount of computer work is actually in the realm of information technology,  Too often what is lacking are skilled individuals that bring an array of tools to the task. The expression "If the only tool you have is a hammer, all your problems look like nails" is a problem I deal with in my professional life. I am constantly faced with vendors who provide the one pony circus (a million ways to make a state machine).

 

Embedded programming is a discipline that requires the developer to be expert at OS scheduling, database management, hardware interfacing, design architecture, and structured objects, as well as proper coding style, and best solution language. It is a constant process of sharpening the tool set to get the best solution. I have taken to putting some tools into retirement as well. Archiving example code and hint/help files is done periodically so I don't have to keep my COBOL skills current, but, by archiving properly, it is possible with a bit of effort, to blow the dust off a few brain cells, and get back in step with my Fortran lines starting in column 7. (...how old is this guy?)

 

Getting back to where I started with this, I wanted to put a call out to all you embedded PROGRAMMERS for tips and techniques and tricks learned that can become the foundation for tool boxes.

 

Tips like:

  • Thinking like a computer
  • Faster graphics and ray tracing
  • Integer only formulas
  • Weight loss (or wait loss) compression
  • T...I...M...I...N...G...

 

Again, some of these are done with hardware these days, but not all solutions have bottomless bank accounts. Sometimes a one chip 8-bit piece of hardware needs to run an 8 cylinder diesel fueling operation.

  • Sign in to reply
  • Cancel

Top Replies

  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to ntewinkel +4
    ntewinkel , Precisely what I was referring to. Fixed point for calculations saves tons and tons of calculation overhead and saves boatloads of memory. Time for my first contribution to the tools. Fixed…
  • DAB
    DAB over 9 years ago +3
    Hi Jack, I can sympathize. Using high level programming languages hide a lot of detail you need to learn when going into embedded programming. Luckily I learned assembly language programming on an old…
  • rsc
    rsc over 9 years ago +3
    The most important tip I can think of is to document what you do, both hardware and software. When you get to the point you're writing code in several languages on several compilers for different projects…
Parents
  • rsc
    rsc over 9 years ago

    The most important tip I can think of is to document what you do, both hardware and software.

    When you get to the point you're writing code in several languages on several compilers for different projects,

    it's easy to forget what formula you used for s subroutine, or what version of the program is in the machine today.

    Always have a header in every file noting the last edit date, a change log, input and output variables, and any

    derived formulas or assumptions about initial conditions.  I'm working on a project that uses NFC chips to track

    software and hardware versions/changes.

    Scott

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to rsc

    Can I have a "yay" for rsc (Scott)!!!  If I had a nickel for every time I have had to review what I have done over the course of the project.., So often the thing that kills greatness is the paperwork, or lack of it. The old saying is "if you have an hour to cut down a tree, spend 45min sharpening the saw".  Preparation and design should happen before any hardware or software gets implemented.  All the decisions about having something done in hardware, or in software should be determined with both groups represented in the room as well. Also, make sure you have the expertise to work with the tools you want to implement. I was on a project that decided to use FPGA components for a bundle of the routing circuits, but ran into a bit of a block when it was discovered the one person that knew how to design the FPGA firmware had exited a month before integration testing.

     

    Big time thank you,

    Jack

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to rsc

    Can I have a "yay" for rsc (Scott)!!!  If I had a nickel for every time I have had to review what I have done over the course of the project.., So often the thing that kills greatness is the paperwork, or lack of it. The old saying is "if you have an hour to cut down a tree, spend 45min sharpening the saw".  Preparation and design should happen before any hardware or software gets implemented.  All the decisions about having something done in hardware, or in software should be determined with both groups represented in the room as well. Also, make sure you have the expertise to work with the tools you want to implement. I was on a project that decided to use FPGA components for a bundle of the routing circuits, but ran into a bit of a block when it was discovered the one person that knew how to design the FPGA firmware had exited a month before integration testing.

     

    Big time thank you,

    Jack