Business of Engineering
  • Technologies
  • More
Business of Engineering
Forum If I Had a Hammer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 245 subscribers
  • Views 6391 views
  • Users 0 members are here
Related

If I Had a Hammer

jack.chaney56
jack.chaney56 over 9 years ago

I used this as a clever draw to get more readers.  The actual intent is to start a discussion and get input from people for software.  Most of the discussions I have seen on the site are about inventing hardware solutions to popular problems.  I guess I am getting overloaded with how many ways there are to turn on an LED.  A significant amount of computer work is actually in the realm of information technology,  Too often what is lacking are skilled individuals that bring an array of tools to the task. The expression "If the only tool you have is a hammer, all your problems look like nails" is a problem I deal with in my professional life. I am constantly faced with vendors who provide the one pony circus (a million ways to make a state machine).

 

Embedded programming is a discipline that requires the developer to be expert at OS scheduling, database management, hardware interfacing, design architecture, and structured objects, as well as proper coding style, and best solution language. It is a constant process of sharpening the tool set to get the best solution. I have taken to putting some tools into retirement as well. Archiving example code and hint/help files is done periodically so I don't have to keep my COBOL skills current, but, by archiving properly, it is possible with a bit of effort, to blow the dust off a few brain cells, and get back in step with my Fortran lines starting in column 7. (...how old is this guy?)

 

Getting back to where I started with this, I wanted to put a call out to all you embedded PROGRAMMERS for tips and techniques and tricks learned that can become the foundation for tool boxes.

 

Tips like:

  • Thinking like a computer
  • Faster graphics and ray tracing
  • Integer only formulas
  • Weight loss (or wait loss) compression
  • T...I...M...I...N...G...

 

Again, some of these are done with hardware these days, but not all solutions have bottomless bank accounts. Sometimes a one chip 8-bit piece of hardware needs to run an 8 cylinder diesel fueling operation.

  • Sign in to reply
  • Cancel

Top Replies

  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to ntewinkel +4
    ntewinkel , Precisely what I was referring to. Fixed point for calculations saves tons and tons of calculation overhead and saves boatloads of memory. Time for my first contribution to the tools. Fixed…
  • DAB
    DAB over 9 years ago +3
    Hi Jack, I can sympathize. Using high level programming languages hide a lot of detail you need to learn when going into embedded programming. Luckily I learned assembly language programming on an old…
  • rsc
    rsc over 9 years ago +3
    The most important tip I can think of is to document what you do, both hardware and software. When you get to the point you're writing code in several languages on several compilers for different projects…
Parents
  • jack.chaney56
    jack.chaney56 over 9 years ago

    Needed to say something about tables versus formulas. For real time systems, tables always win.

    • Given a non-linear curve where Y=f(x) and x is a measured value, the value at any point can be calculated using the function f(x)
    • For simple linear equations accuracy is high and calculation can be performed simply with a single multiply and add
    • For complex equations, accuracy becomes an issue, and the calculation can become difficult and time consuming.

    image

    • For short ranges, a linear interpolation can be used for a close approximation, but this becomes highly inaccurate outside a specified range

    image

    • Using fundamental calculus, if the range of delta X is distributed evenly, the linear interpolation between any two points more closely approximates any curve
    • If greater accuracy is required the number of sections can be increased

      image

    • By producing a table of these values, the equation becomes simple for any value Xn where Xn is between Xa and Xb
    • The equation becomes:


       ƒ (X)=Ya+(((Yb−Ya)·(Xb−Xn))(Xb−Xa) )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to jack.chaney56

    ...lost one of the diagrams

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Instructorman
    Instructorman over 9 years ago in reply to jack.chaney56

    I once had to calculate humidex in an 8-bit PIC microcontroller using the following formula - without using floating point:

    image

     

    Yup, that got turned into a look up table faster than you can say "Holy Excel spreadsheet, Batman!"

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 9 years ago in reply to Instructorman

    One simple, but effective advice could be "learn to use spreadsheets and make graphs from them".

    I used Excel in practically all sensor applications, before implementing the formula to a microcontroller, just to check that the raw output values make sense to what is measured.

     

    • Recently I created a simple altimeter (hobbyist project) using an absolute pressure sensor. The barometric formula looks pretty hard to be calculated by a microcontroller:

    image

    or

    image

     

    However, using Excel, I found out that for a +/- 1000 m of altitude deviation is the pressure change ca. 11 Pa per 1 meter.

    One integer subtraction and an integer division is much simpler, even after considering the computation error.

     

    • Excel is also powerful to draw various graphs, calculate missing values and provide functions' approximations. This is especially useful when working with sensors that need to be calibrated (or were factory calibrated).

    The following graph shows an example of a function providing relative humidity value from  HTS221HTS221 sensor's raw output(using two calibration values It also shows that the sensors I have on my table are linear but the slope is a bit different And last but not least that the higher is the sensors output value the lower is the relative humidity(Please excuse the missing labels it was just a quick graph to demonstrate the point X axis shows relative humidity in rH Y axis shows an 16-bit signed output from the sensor

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 9 years ago in reply to koudelad

    More information on how you did this would be great. Sounds like a greatly useful skill to have but not something a lot of us do have.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to kas.lewis

    Hi kas.lewis

    The process is part of a table lookup routine that I have in my toolbox. The process treats all tables as an NxM array, where N is the width and M is the height. The linkage to the data is done using a getter function so the data store can be abstracted.

    The function passes X as a parameter of f(x). Because N is the width of the table, there are N elements in the array of equal spacing the max value for X is defined during design. For most cases in my work, I use the ratio element (described earlier) 1024. The delta (spacing between elements) can now be determined as dX = 1024/N.

    The operation now needs two components, Xi which is the index into the table, and Xo witch is the offset from the index. The two values are obtained with the two operators, integer divide, and integer mod (remainder after division).

    Xi = x / dX;

    Xo = x % dX

     

    The getter function is called Z0 = getCal(table, x, y) using parameters of a table accessor, and the x and y indexes the function returns the content of the element (data type is determined by design).

    The operation requires the indexed value and the next value in sequence or x(n) and x(n+1). However, if the table is N units the indexes only go from 0 to N-1, but if the divide operation returns N-1, N, which is the next element, is beyond the end of the array. To account for this, a linear extension is performed:

    Z0 = getCal(table, Xi, y),

    Z1 = Z0 + Z0 - getCal(table, (Xi - 1), y)

    but for most cases it is simply Xi and (Xi + 1)

     

    Last, the interpolation is done as described before, this time with the defined variables  Z0+(((Z1−Z0)·Xo)dX )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to Instructorman

    Hi Instructorman

    I like the discussion of the baro sensor being used for altitude. The equations are good, and show step one of the process of developing an application. My intent of this forum was to provide tools and techniques to share with others in problem solving. So if you could, because you mentioned running into some hitches while working with standard packages like Excel, it would be extremely helpful if you would discuss what you did to overcome the issue in developing the embedded solution.

    I can understand how a complex operation with  ex  and complex powers can become involved, especially with smaller processors that don't have floating point hardware. I have to perform pH conversion in many of the functions for our system, so I understand the headaches of dealing with log and anti-log operations.

    So if you would be so kind as to expound on the tricks that got you to a final solution, that would prove helpful to the group.

     

    Thank you,

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 9 years ago in reply to kas.lewis

    EDIT: My reply was quite long, so I decided to create a separate blog post from it: Using spreadsheets (Excel) for simple computations and approximations

    I think there will be a huge amount of information over time in this thread, so it will be more readable for newcomers.

     

    David

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Instructorman
    Instructorman over 9 years ago in reply to jack.chaney56

      

    Thanks jack.chaney56 for the coaxing. image

     

    The work mentioned in my post was done for a client that owns the IP, so any discussion will be devoid of details, but I can describe the process I went through in general terms

     

    Actually, after reading rsc's post on the importance of documentation, which I completely agree with, and your follow up, I realized I would be relying on the quality of my own documentation to remember how I solved the tricky bits of getting an ex equation into an 8 bit PIC.  I worked on this problem back in 2010, so I remember that I did it, and that spread sheets and lookup tables were involved, but the details are not readily accessible in my working memory.  This is a great case study to illustrate why good documentation is so important.

     

    I have found the project files and started to reacquaint myself with the details.  Looks like we will soon find out if my documentation from 7 years ago was of sufficient quality to allow me to resurrect the methods and share them here.

    I hope to post again in a few days with an explanation of how I solved the problem.

     

    Mark A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 9 years ago in reply to jack.chaney56

    No big science happened there, I basically put all the constants, variables and the equation itself to a speadsheet and let the Excel calculate 10 000 values of an air pressure from 0 m to 10 000 m with a step of 1 m.

    Then I calculated the pressure difference between each of the 1 meter zone and estimated the error. The trend line could also be added (as described in my previous comment) with some approximation. For implementation into a microcontroller, sometimes a simplified equation works, sometimes a lookup table.

     

    I was only interested in destinations easily reachable by a tourist (ca. 0 - 2500 m) in that case image

     

    I wanted to emphasize that counting thousands of values to see the function behavior is just a matter of seconds for today's computers. And visualizing the data is often priceless.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • koudelad
    koudelad over 9 years ago in reply to jack.chaney56

    No big science happened there, I basically put all the constants, variables and the equation itself to a speadsheet and let the Excel calculate 10 000 values of an air pressure from 0 m to 10 000 m with a step of 1 m.

    Then I calculated the pressure difference between each of the 1 meter zone and estimated the error. The trend line could also be added (as described in my previous comment) with some approximation. For implementation into a microcontroller, sometimes a simplified equation works, sometimes a lookup table.

     

    I was only interested in destinations easily reachable by a tourist (ca. 0 - 2500 m) in that case image

     

    I wanted to emphasize that counting thousands of values to see the function behavior is just a matter of seconds for today's computers. And visualizing the data is often priceless.