Business of Engineering
  • Technologies
  • More
Business of Engineering
Quiz PC Builder's Quiz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 17 Oct 2022 2:38 PM Date Created
  • Last Updated Last Updated: 6 Jun 2024 4:26 PM
  • Views 252103 views
  • Likes 17 likes
  • Comments 244 comments
Related
Recommended

PC Builder's Quiz

The only way to get the exact PC you want is to build it yourself! Test your knowledge with our quiz on building your own PC.

profile image

Quiz | Business of Engineering | Resource | Test & Tools

PC Builder's Quiz
PC Builder's Quiz Score 100% on our PC Builder's Quiz and leave your feedback as a comment to earn this badge...

To earn the PC Builder Badge, score 100% on the quiz and leave your feedback on the quiz as a comment.

  • personal computer
  • PC builder
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 4 years ago +4
    Owners of fanless PC's may disagree with question 14.
  • swalberg
    swalberg over 4 years ago in reply to beacon_dave +3
    Yep, seen many computers with a single fan (or none), and the way the question is worded makes it sounds like it's an absolute.
  • dougw
    dougw over 4 years ago +1
    It is fun to breeze through an easy quiz once in a while.
Parents
  • 830filos
    830filos over 4 years ago

    I have been overclocking since I began building PC's...1998 with my Pentium II 333 Mhz overclocked to 430Mhz...So fans are very important and must have a good flow outwards...if you are pushing a lot of air, that air naturally replaces the empty space inside. Cases with holes on all sides is very hard to create natural flow as air flow is interrupted. Back then, there was no water cooling and the air coming in the case had to be cooler or else everything would overheat. So experiment was the only way to find the correct approach. I made a cone that would carry from under the case cold air directly to the fan on the CPU...that kept my PC working very well. And from the rear bottom and front bottom two more fans pulling air in and 2 fans on the top pushing out. My CPU was faster than the next 3 CPU's that intel manufactured. Today, if you have a water cooled case, meaning gpu,cpu on water blocks, there is not much heat in the case as it used to be because it is carried through the radiators. At the moment my PC running on a 3900X OC all core 4.3GHz 1.295V with water cooling, temperatures do not exceed 70⁰C when rendering. All my fans are pushing out except on in the back pulling in...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 830filos
    830filos over 4 years ago

    I have been overclocking since I began building PC's...1998 with my Pentium II 333 Mhz overclocked to 430Mhz...So fans are very important and must have a good flow outwards...if you are pushing a lot of air, that air naturally replaces the empty space inside. Cases with holes on all sides is very hard to create natural flow as air flow is interrupted. Back then, there was no water cooling and the air coming in the case had to be cooler or else everything would overheat. So experiment was the only way to find the correct approach. I made a cone that would carry from under the case cold air directly to the fan on the CPU...that kept my PC working very well. And from the rear bottom and front bottom two more fans pulling air in and 2 fans on the top pushing out. My CPU was faster than the next 3 CPU's that intel manufactured. Today, if you have a water cooled case, meaning gpu,cpu on water blocks, there is not much heat in the case as it used to be because it is carried through the radiators. At the moment my PC running on a 3900X OC all core 4.3GHz 1.295V with water cooling, temperatures do not exceed 70⁰C when rendering. All my fans are pushing out except on in the back pulling in...