Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Powering a Rane SM82 Rack Mixer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 69 subscribers
  • Views 4046 views
  • Users 0 members are here
Related

Powering a Rane SM82 Rack Mixer

Andy Betts
Andy Betts over 6 years ago

I've just bought an SM82 from the US, and got it for good money ($50 inc shipping) Obviously the PSU it came with is for 110v power so i've gathered together all the bits to make my own 230v PSU. they do sell reproduction PSU's on EBay but they go for around £50 and I can make one for around £20. i do have quite a bit of experience with soldering and electronics, but NOT with PSU's, never made one. But it's one of those things i want to have a go at to tick off the bucket list of things to do.

 

A guy previously made one and posted his build on another site (I've also posted on that site to try and gain more information) his build is here https://www.thegearpage.net/board/index.php?threads/diy-rane-rs1-power-supply-for-sm26-and-sm82.1838728/

 

he built his with no thermistors in series, which i don't want to do, I want to play safe.

 

I've purchased a transformer from Rapid Electronics (Vigortronix VTX-120-5412-209 PCB Transformer 230V 12VA 9V+9V) which should do the trick, but my question is around the thermistors. The PCT Thermistors are there to prevent inrush current into the transformer so i'm a little loath to build this without thermistors in place.

 

The schematic for the original PSU is not available, however there is a schematic for a Rap 10. The Rap 10 is the same as the single PSU, just multiplied 10 times, so please ignore the other 9 outputs on the schematic.... Here is the schematic https://www.ranecommercial.com/legacy/pdf/old/rap10sch.pdf

 

As the thermistor is variable resistance how do i know what one to buy?? Is there a way of calculating the zero power resistance? Rapid have the following on their site

 

https://www.rapidonline.com/Catalogue/Search?Query=thermistors&Tier=PTC

 

Any ideas??

  • Sign in to reply
  • Cancel

Top Replies

  • Andy Betts
    Andy Betts over 6 years ago in reply to shabaz +2
    Found one.... and cheap too https://www.rapidonline.com/bulgin-pf0001-63-mains-socket-panel-mount-fused-flange-250v-ac-10a-6-3mm-51-4352
  • Andy Betts
    Andy Betts over 6 years ago +2
    Found an answer elsewhere.... easy really and makes perfect sense My transformer is as below... I need to run secondary's in series which will give me a center tap... so i need to do this... join terminals…
  • Andy Betts
    Andy Betts over 6 years ago in reply to shabaz +2
    No problem Shabaz... We're all otherwise busy at this time....
Parents
  • Andy Betts
    Andy Betts over 6 years ago

    UPDATE:

     

    I've purchased a transformer, 230v primary with a dual 9v secondary.. You can read about it here.... Hopefully it'll be OK for my use. The data sheet is attached, mine is the 12va one

     

    This is slightly different from the one used by the guy above, as this one has 2 0v pins where his only had 1. Question.... As mine has 2 0v pins am I Ok to just utilize 1 of them, i assume yes. My 230v input will use the 2 outer pins on the primary side, but when you look at the schematic of the PSU on the secondary side it has 2 9v and 1 centre tap so I don't really need to use the extra 0v pin.

     

    image

     

     

    This is seen more clearly on the other guys build where you have the 3 sets of 2 wires....

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andy Betts
    Andy Betts over 6 years ago

    UPDATE:

     

    I've purchased a transformer, 230v primary with a dual 9v secondary.. You can read about it here.... Hopefully it'll be OK for my use. The data sheet is attached, mine is the 12va one

     

    This is slightly different from the one used by the guy above, as this one has 2 0v pins where his only had 1. Question.... As mine has 2 0v pins am I Ok to just utilize 1 of them, i assume yes. My 230v input will use the 2 outer pins on the primary side, but when you look at the schematic of the PSU on the secondary side it has 2 9v and 1 centre tap so I don't really need to use the extra 0v pin.

     

    image

     

     

    This is seen more clearly on the other guys build where you have the 3 sets of 2 wires....