Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum HELP!!!.... Blown Electric Mistress pedal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 72 subscribers
  • Views 10106 views
  • Users 0 members are here
Related

HELP!!!.... Blown Electric Mistress pedal

Andy Betts
Andy Betts over 6 years ago

I have made a huge school boy error... i was looking at running my original Electric Mistress pedal for a recording I'm doing and needed to run it off an external power supply. I had a 18v supply to hand which I just needed to connect up to a DC plug so that I could power the pedal. In my haste, I accidentally connected the negative and voltage wires the wrong way round...... connected the pedal, switched on the power and I immediately heard a small pop and the smell of burning. I have blown an original 1977 Electro Harmonix Electric Mistress effects pedal worth around $500!!! however, i'm sure it's not dead yet, and it can be brought back to life... Hence this post.

 

For your reference I have attached the schematic.

 

can anyone advise the best place to start troubleshooting, I'm assuming anything on the ground side of things could have been the first thing to blow, and I'm thinking a transistor.... bearing in mind the 18v supply was connected to the ground, and the ground was connected to the voltage in. Anything can be replaced, the only issue is if the culprit ends up being the SAD1024 chip that's it... the pedal is a gonner. However I very much doubt the voltage got that far in the circuit to be honest (hopefully)

Attachments:
imageMistress_v2_schematic.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4
    Hi Andy, I wanted to understand the voltage regulator a little better so I built one on the bread board. My original intention was to also hook it up backwards to see how it failed. I have decided not…
  • Andy Betts
    Andy Betts over 6 years ago in reply to Andy Betts +4
    repaired... Transistor was around the wrong way
  • DAB
    DAB over 6 years ago +3
    Bad luck is a pain. I looked over your schematic and you will probably need to replace all electrolytic capacitors as they do not tolerate being hooked up wrong. If you smelled or saw smoke, you probably…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Andy,

     

    The failure of the BC309 indicates that it had a very high current flowing through it. This is not a good sign for the rest of your circuit. Our best hope is that the 33 uF electrolytic cap shorted out and took the brunt of the current. Plan to replace the 33 uF cap if you can not check it. I know that the current was Emitter Collector on the BC309 as the 100K resistor on the base would have limited the base current and not allowed the transistor to heat enough to explode. This says that there was a short further down the line. Either the C12 33 uF cap or one of the other components. Especially vulnerable would have been the LM339, 4013, SAD1024, and the 4558 as they are hooked with no current limitation across the power rails. Once the BC309 exploded the current path was removed and any component not already damaged would probably be OK. If I get the time later I will build the power supply on a bread board and try to simulate your failure to see how the regulator powers the rails under reverse voltage conditions and just how long it takes for the BC309 to fail and open the circuit.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 6 years ago

    Hi Andy,

     

    The failure of the BC309 indicates that it had a very high current flowing through it. This is not a good sign for the rest of your circuit. Our best hope is that the 33 uF electrolytic cap shorted out and took the brunt of the current. Plan to replace the 33 uF cap if you can not check it. I know that the current was Emitter Collector on the BC309 as the 100K resistor on the base would have limited the base current and not allowed the transistor to heat enough to explode. This says that there was a short further down the line. Either the C12 33 uF cap or one of the other components. Especially vulnerable would have been the LM339, 4013, SAD1024, and the 4558 as they are hooked with no current limitation across the power rails. Once the BC309 exploded the current path was removed and any component not already damaged would probably be OK. If I get the time later I will build the power supply on a bread board and try to simulate your failure to see how the regulator powers the rails under reverse voltage conditions and just how long it takes for the BC309 to fail and open the circuit.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 6 years ago in reply to jw0752

    I just noticed that C9 100 uF on the reverse side of the circuit board would also have seen a reverse polarity directly and could also have suffered the same trauma as the C12 33 uF cap.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andy Betts
    Andy Betts over 6 years ago in reply to jw0752

    Hi John, that's not good news if the SAD1024 could be fried... I hope it isn't.

     

    I'll start in a methodical way, i'll sort all the voltage regulator section out first, test then if there's no life i'll move on to the other electrolytic caps and start replacing those that are exposed directly to ground as they likely would have got the full 18v on the ground rail. It won't hurt to replace a lot of them anyway as they're all at least 43 years old and are possibly suffering leakage anyway.