Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum HELP!!!.... Blown Electric Mistress pedal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 72 subscribers
  • Views 9956 views
  • Users 0 members are here
Related

HELP!!!.... Blown Electric Mistress pedal

Andy Betts
Andy Betts over 6 years ago

I have made a huge school boy error... i was looking at running my original Electric Mistress pedal for a recording I'm doing and needed to run it off an external power supply. I had a 18v supply to hand which I just needed to connect up to a DC plug so that I could power the pedal. In my haste, I accidentally connected the negative and voltage wires the wrong way round...... connected the pedal, switched on the power and I immediately heard a small pop and the smell of burning. I have blown an original 1977 Electro Harmonix Electric Mistress effects pedal worth around $500!!! however, i'm sure it's not dead yet, and it can be brought back to life... Hence this post.

 

For your reference I have attached the schematic.

 

can anyone advise the best place to start troubleshooting, I'm assuming anything on the ground side of things could have been the first thing to blow, and I'm thinking a transistor.... bearing in mind the 18v supply was connected to the ground, and the ground was connected to the voltage in. Anything can be replaced, the only issue is if the culprit ends up being the SAD1024 chip that's it... the pedal is a gonner. However I very much doubt the voltage got that far in the circuit to be honest (hopefully)

Attachments:
imageMistress_v2_schematic.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4
    Hi Andy, I wanted to understand the voltage regulator a little better so I built one on the bread board. My original intention was to also hook it up backwards to see how it failed. I have decided not…
  • Andy Betts
    Andy Betts over 6 years ago in reply to Andy Betts +4
    repaired... Transistor was around the wrong way
  • DAB
    DAB over 6 years ago +3
    Bad luck is a pain. I looked over your schematic and you will probably need to replace all electrolytic capacitors as they do not tolerate being hooked up wrong. If you smelled or saw smoke, you probably…
Parents
  • Andy Betts
    Andy Betts over 6 years ago

    UPDATE: I've replaced the blown transistor, and plugged it all in and tested. When I switch the effect on I get the usual volume drop as you normally get with these pedals but no effect at all..... I have signal through the circuit though obviously so I'm now concerned that the SAD1024 might be dead.

     

    So far I have replaced:

     

    IC LM741

    C9 - 100uf

    C10 - 10uf

    C11 - 10uf

    c12 - 33uf

    BC309 (this was replaced with a BC212L as per the original transistor)

     

    Any ideas?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andy Betts
    Andy Betts over 6 years ago

    UPDATE: I've replaced the blown transistor, and plugged it all in and tested. When I switch the effect on I get the usual volume drop as you normally get with these pedals but no effect at all..... I have signal through the circuit though obviously so I'm now concerned that the SAD1024 might be dead.

     

    So far I have replaced:

     

    IC LM741

    C9 - 100uf

    C10 - 10uf

    C11 - 10uf

    c12 - 33uf

    BC309 (this was replaced with a BC212L as per the original transistor)

     

    Any ideas?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Andy Betts

    As a first check: what is the voltage on CC212L' s collector (V+) ?

     

    2nd check: do you have small external PC desk speakers with built in amplifier?

    In that case you can use it as a signal tracer:

    connect ground of the speaker input to circuit ground (typilcal, on the cinch connection of these speakers, it's the biggest part of the tip close to the plastic housing.

    Then put the cinch tip to pin 1 of IC1 and check if you hear guitar signal. If yes, circuit before the delay is good.

    Then repeat at C5/R13 connection. You should hear the delayed signal...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andy Betts
    Andy Betts over 6 years ago in reply to Jan Cumps

    I'm actually in the middle of measuring the voltages on all the IC's and the transistors... I'll report back here when I have them