Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Can I have multiple powersources Powering one device if I use diodes?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 73 subscribers
  • Views 7187 views
  • Users 0 members are here
  • voltage
  • power
Related

Can I have multiple powersources Powering one device if I use diodes?

Sean_Miller
Sean_Miller over 5 years ago

I have a lithium ion battery powered device that I would like to allow plugging in a wall wart to power it as well.

 

If I put a diode on the lithium ion battery, would this prevent causing an issue to the battery when I connect the device to the wall wart supply?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 5 years ago +8
    Sean, I typically place a schottky diode inline with each potential power source. In this case, there are three potential sources of input to the voltage regulator (AP2127). V+ (D1G$3) is the charger input…
  • Andrew J
    Andrew J over 5 years ago +6
    Sean, I don’t know the set up you have, but if it is currently powered by a battery and you can modify it to add a diode AND you want to power it with a wall wart which implies you need to alter it to…
  • milosrasic98
    milosrasic98 over 5 years ago +5
    As genebren already said, using Schottky diodes is the way to go because of their low drop voltage. This principle is also used for power switching on some of the Arduino boards. I made a circuit similar…
Parents
  • milosrasic98
    milosrasic98 over 5 years ago

    As genebren already said, using Schottky diodes is the way to go because of their low drop voltage. This principle is also used for power switching on some of the Arduino boards. I made a circuit similar to this recently and it worked great for lower power devices, but struggled on something more power hungry like the Raspberry (due to the drop on the 5V rail and the 7805 not being able to handle such current).

    image

     

    Milos

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • milosrasic98
    milosrasic98 over 5 years ago

    As genebren already said, using Schottky diodes is the way to go because of their low drop voltage. This principle is also used for power switching on some of the Arduino boards. I made a circuit similar to this recently and it worked great for lower power devices, but struggled on something more power hungry like the Raspberry (due to the drop on the 5V rail and the 7805 not being able to handle such current).

    image

     

    Milos

    • Cancel
    • Vote Up +5 Vote Down