Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Hi guys Iam looking for a varistor with 4 pin connections. The characterisitcs are in the table below.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 70 subscribers
  • Views 674 views
  • Users 0 members are here
Related

Hi guys Iam looking for a varistor with 4 pin connections. The characterisitcs are in the table below.

e14 Contributor
e14 Contributor over 15 years ago
Disc Size (mm)25⁰C25⁰C85⁰C
AC (Volts)DC (Volts)Energy (10x1000µs)Max. PowerMax Current (8x20 µs)Tension varistance under 1mATension Decretage MaxiCapacitance (1KHz)
JoulesWattsAmperesVoltsTol.VoltsAmperepF
14435513.00.6020006810%135105000


I would really appreciate if anyone could help me find the right part

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I have worked on the design of 3-pin varistors, but <generally> not 4-pin.

     

    1. I am aware of manufacturers using non-bonded thermal fuses (usually with heatshrink over them), thereby forming a 4-lead device. The purpose of this is to sense the condition of the MOV separately from actually disconnecting it under over-temp conditions. This is acceptable for instrumentation applications, but isn't very useful for power applications.
    2. Another reason may be to avoid extreme currents in the MOV-PCB interface (i.e. solder). Simply adding 2 more leads doesn't really help much, and a 14mm MOV isn't going to conduct enough current (within it's ratings) to warrant it.
    3. If your reason is other than this, I am interested. Otherwise, just use a 2-lead device instead.

     

    Regards,

     

    Jonathan Point

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    I have worked on the design of 3-pin varistors, but <generally> not 4-pin.

     

    1. I am aware of manufacturers using non-bonded thermal fuses (usually with heatshrink over them), thereby forming a 4-lead device. The purpose of this is to sense the condition of the MOV separately from actually disconnecting it under over-temp conditions. This is acceptable for instrumentation applications, but isn't very useful for power applications.
    2. Another reason may be to avoid extreme currents in the MOV-PCB interface (i.e. solder). Simply adding 2 more leads doesn't really help much, and a 14mm MOV isn't going to conduct enough current (within it's ratings) to warrant it.
    3. If your reason is other than this, I am interested. Otherwise, just use a 2-lead device instead.

     

    Regards,

     

    Jonathan Point