Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Hi guys Iam looking for a varistor with 4 pin connections. The characterisitcs are in the table below.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 70 subscribers
  • Views 669 views
  • Users 0 members are here
Related

Hi guys Iam looking for a varistor with 4 pin connections. The characterisitcs are in the table below.

e14 Contributor
e14 Contributor over 15 years ago
Disc Size (mm)25⁰C25⁰C85⁰C
AC (Volts)DC (Volts)Energy (10x1000µs)Max. PowerMax Current (8x20 µs)Tension varistance under 1mATension Decretage MaxiCapacitance (1KHz)
JoulesWattsAmperesVoltsTol.VoltsAmperepF
14435513.00.6020006810%135105000


I would really appreciate if anyone could help me find the right part

  • Sign in to reply
  • Cancel
  • hargreaves
    hargreaves over 15 years ago

    Hi Aman.

    With varistors it is always hard to get an exact match if you have precise requirements. Farnell has only 2 pin versions near to these values. I assume your varistor has 4 pins for mechanical reasons, but if you can get away with 2 pins, you could try Farnell codes 1004735 and 1057176-11057176-1.

    http://uk.farnell.com/epcos/b72214s0400k101/varistor-13-0j-40vac/dp/1004375

    http://uk.farnell.com/littelfuse/v68za10p/varistor-13-0j-40vac/dp/1057176

    You will see from the datasheets that these don't exactly match on the DC and AC voltages but depending on your circuit, may do nicely.

    BTW, the Epcos datasheet link is broken so try this,

    http://www.epcos.com/inf/70/db/var_08/SIOV_Leaded_StandarD.pdf

     

    Kevin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I have worked on the design of 3-pin varistors, but <generally> not 4-pin.

     

    1. I am aware of manufacturers using non-bonded thermal fuses (usually with heatshrink over them), thereby forming a 4-lead device. The purpose of this is to sense the condition of the MOV separately from actually disconnecting it under over-temp conditions. This is acceptable for instrumentation applications, but isn't very useful for power applications.
    2. Another reason may be to avoid extreme currents in the MOV-PCB interface (i.e. solder). Simply adding 2 more leads doesn't really help much, and a 14mm MOV isn't going to conduct enough current (within it's ratings) to warrant it.
    3. If your reason is other than this, I am interested. Otherwise, just use a 2-lead device instead.

     

    Regards,

     

    Jonathan Point