Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Why is this transistor required
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 71 subscribers
  • Views 2834 views
  • Users 0 members are here
  • relay
Related

Why is this transistor required

rishi2628
rishi2628 over 10 years ago

Why is the transistor Q3 required in this circuit of a optocoupler and a relay. Can't I directly attach the power pin of the relay to the opto coupler pin 3 and ground the other pin of the relay. I tried it and it works. Just want to know why is it not implemented and why is the transistor required.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 10 years ago in reply to rishi2628 +1
    Ah yes, I see what you mean. Possibly the switching current for the relay coil is higher than the optocoupler can safely provide, so the transistor is there to do the job instead.
Parents
  • spannerspencer
    0 spannerspencer over 10 years ago

    Looks like it's probably switching the relay it's connected to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rishi2628
    0 rishi2628 over 10 years ago in reply to spannerspencer

    Yes Sir but I want to know why cant we directly connect the relay to the Optocoupler. Is this circuit more reliable or something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 10 years ago in reply to rishi2628

    Ah yes, I see what you mean. Possibly the switching current for the relay coil is higher than the optocoupler can safely provide, so the transistor is there to do the job instead.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • spannerspencer
    0 spannerspencer over 10 years ago in reply to rishi2628

    Ah yes, I see what you mean. Possibly the switching current for the relay coil is higher than the optocoupler can safely provide, so the transistor is there to do the job instead.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to spannerspencer

    The simple answer is the opto coupler is only rated for 50mA while the relay is either 72 or 90mA.

     

     

    image

     

     

    Under some circumstance you may be able to drive it (although it may not pull in correctly), but these have issues being drivn by a Raspberry Pi.

    The 3v3, series resitor and LED n the input side combine to be just on the edge of triggering even with the transistor.

    The answer is to add a second 1K across the resistor (R5 in the schematic).

     

    Mark