Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum How to decide the Temperature range of an IC??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 73 subscribers
  • Views 7678 views
  • Users 0 members are here
Related

How to decide the Temperature range of an IC??

rishi2628
rishi2628 over 10 years ago

I am using a MAX3241E ic in a device that has to run 24x7 out in the open. I am facing a problem deciding the temperature range of the the IC. Since it is out in the open, the ic has to withstand the heat from the sun plus the heating effect due to losses and resistances, etc. I am living in Delhi, India and here the temperature easily reaches 35 degrees. This ic that I have choosen can bear a max temp of 70 degrees. Should I use this ic or should I go for a higher temperature one? Also please tell how should one decide the max temperature of any ic?

 

Datasheet of the IC: - http://www.mouser.com/ds/2/256/MAX3222E-MAX3246E-99333.pdf

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +2 suggested
    Hi Rishi, This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the…
  • D_Hersey
    D_Hersey over 10 years ago +1
    Hi, John, I trust that you are well. Thermo-electric cooler, also called a Peltier cooler. Very useful in chilling detectors in telescopes, for example
  • D_Hersey
    D_Hersey over 10 years ago +1
    On the topic of TECs, I would like to try to use them for crystal growing. I would pour a nearly boiling saturated solution of, say, copper sulphate, into a squarish glass container. I would have washed…
Parents
  • michaelkellett
    0 michaelkellett over 10 years ago

    There is no substitute for actual testing. A device left out in full sunlight can get extremely hot (>60C) the link discusses temperatures inside a car:

     

    HEAT EXPOSURE IN AN ENCLOSED AUTOMOBILE

     

    Your device may be better or worse - and then you must add the temperature rise caused by the operation of the electronics (which you can easily measure.).

    You should aim never to get closer than 10C away from the maximum junction temperature for the chip you are using (to give yourself a margin for error).

     

    You would be unwise to use a 0-70C rated part in this application and you need some testing to be sure that -40 - +85 is OK.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago

    There is no substitute for actual testing. A device left out in full sunlight can get extremely hot (>60C) the link discusses temperatures inside a car:

     

    HEAT EXPOSURE IN AN ENCLOSED AUTOMOBILE

     

    Your device may be better or worse - and then you must add the temperature rise caused by the operation of the electronics (which you can easily measure.).

    You should aim never to get closer than 10C away from the maximum junction temperature for the chip you are using (to give yourself a margin for error).

     

    You would be unwise to use a 0-70C rated part in this application and you need some testing to be sure that -40 - +85 is OK.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer