Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum How to decide the Temperature range of an IC??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 73 subscribers
  • Views 7698 views
  • Users 0 members are here
Related

How to decide the Temperature range of an IC??

rishi2628
rishi2628 over 10 years ago

I am using a MAX3241E ic in a device that has to run 24x7 out in the open. I am facing a problem deciding the temperature range of the the IC. Since it is out in the open, the ic has to withstand the heat from the sun plus the heating effect due to losses and resistances, etc. I am living in Delhi, India and here the temperature easily reaches 35 degrees. This ic that I have choosen can bear a max temp of 70 degrees. Should I use this ic or should I go for a higher temperature one? Also please tell how should one decide the max temperature of any ic?

 

Datasheet of the IC: - http://www.mouser.com/ds/2/256/MAX3222E-MAX3246E-99333.pdf

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +2 suggested
    Hi Rishi, This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the…
  • D_Hersey
    D_Hersey over 10 years ago +1
    Hi, John, I trust that you are well. Thermo-electric cooler, also called a Peltier cooler. Very useful in chilling detectors in telescopes, for example
  • D_Hersey
    D_Hersey over 10 years ago +1
    On the topic of TECs, I would like to try to use them for crystal growing. I would pour a nearly boiling saturated solution of, say, copper sulphate, into a squarish glass container. I would have washed…
  • jw0752
    0 jw0752 over 10 years ago

    Hi Rishi,

     

    This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the rain. If it is protected and the case is in the sun light I would expect ambient temps in the enclosure to rise to as much as 50 degrees C. This should still be acceptable for the operation of the chip but be sure to factor this temperature into your design as other components may drift from nominal values at this temperature. If self heating of the IC is an issue it will likely be covered in the data sheet with specific directions for heat sinking the component. I could find nothing about heat sinking on this IC.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rishi2628
    0 rishi2628 over 10 years ago in reply to jw0752

    will this ic work for an ambient temperature of 45 degrees??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 10 years ago in reply to rishi2628

    All IC's operating temperatures are documented in their data sheets however there are three general temperature specifications that almost all ICs use:

     

    Commercial  0 deg. C to 70 deg. C

    Industrial  -40 deg. C to 85 deg. C

    Military to -55 deg. C to 125 deg. C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago

    There is no substitute for actual testing. A device left out in full sunlight can get extremely hot (>60C) the link discusses temperatures inside a car:

     

    HEAT EXPOSURE IN AN ENCLOSED AUTOMOBILE

     

    Your device may be better or worse - and then you must add the temperature rise caused by the operation of the electronics (which you can easily measure.).

    You should aim never to get closer than 10C away from the maximum junction temperature for the chip you are using (to give yourself a margin for error).

     

    You would be unwise to use a 0-70C rated part in this application and you need some testing to be sure that -40 - +85 is OK.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    If you have power freely available, you could maybe use a TEC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to D_Hersey

    Hi Don,

     

    I have over 500 entries in my list of electronic acronyms and initialisms list but I do not know what TEC stands for.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    Hi, John, I trust that you are well.

     

    Thermo-electric cooler, also called a Peltier cooler.  Very useful in chilling detectors in telescopes, for example

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to jw0752

    Someone with all the answers image

     

    But I think he means Thermo Electric Cooler -

     

    @ Don, kind of overkill for an RS232 driver  - TI (and others) offer 125C parts.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago

    Hey, I definitely said 'maybe.'  All semis are on their way south.  The endpoint is when the dopants get all mixed up due to entropy.  Every ten degrees warmer halves the lifetime of your solid-state device.  Funny, I've got some thermionic devices from the '30s that still work fine.  TECs are like three bux nowadays on AMAZON, though you would need to power the cooler and find a way to drain the heat away from the hot side.  Just trying to be comprehensive.  If I were all that practical-minded, I doubt I'd be bothering with this whatsoever.  If you have a natural temperature differential available you could use other TECs to power it. . .

     

    John, you are not the only person I PO with my reliance on TLAs and FLEAs, etc.  Down here in the big city I am not the only one with this OTT trope.  It excludes the hoi polloi, and speeds communication, I suppose.  Why is being annoying so much fun?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    I suggest putting this in a fair sized box with cotton balls as insulation like http://www.homeadvisor.com/article.show.Cotton-Insulation-is-Safe-Green-and-Effective.15108.html . This will mitigate the temps if you are concerned.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>