Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Does any one know what this (automotive thing) is ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 68 subscribers
  • Views 1908 views
  • Users 0 members are here
Related

Does any one know what this (automotive thing) is ?

michaelkellett
michaelkellett over 2 years ago

image

A friend (who mends agricultural machinery) has asked me.

MKI

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 2 years ago +2
    back to back schottkey diode used for voltage suppression https://www.electronicshub.org/types-of-diodes/ 12. Transient Voltage Suppression Diode In semiconductor devices, transients will occur due…
  • michaelkellett
    michaelkellett over 2 years ago in reply to shabaz +2
    Hello, It's wired across the battery supply between the alternator and the battery. The symbol is for a 14.5 V bidirectional transient suppressor (what I call a "transorb"). It makes sense. If…
  • colporteur
    colporteur over 2 years ago in reply to robogary +1
    Wow great reference link.
Parents
  • robogary
    robogary over 2 years ago

    back to back schottkey diode used for voltage suppression 

    https://www.electronicshub.org/types-of-diodes/

    12. Transient Voltage Suppression Diode
    In semiconductor devices, transients will occur due to the sudden change in the state voltage. They will damage the device’s output response. To overcome this problem, Voltage Suppression Diodes are used. The operation of voltage suppression diode is similar to Zener diode operation.

    The operation of these diodes is normal as p-n junction diodes but at the time of transient voltage its operation changes. In normal condition, the impedance of the diode is high. When any transient voltage occurs in the circuit, the diode enters in to the avalanche breakdown region in which a low impedance is provided.

    It is very spontaneously because the avalanche breakdown duration ranges in Pico seconds. Transient voltage suppression diode will clamp the voltage to the fixed levels, mostly its clamping voltage is in minimum range.

    These are having applications in the telecommunication fields, medical, microprocessors and signal processing. It responds to over voltages faster than Varistors or gas discharge tubes.

    The symbol for Transient voltage suppression diode is as shown below.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 2 years ago

    back to back schottkey diode used for voltage suppression 

    https://www.electronicshub.org/types-of-diodes/

    12. Transient Voltage Suppression Diode
    In semiconductor devices, transients will occur due to the sudden change in the state voltage. They will damage the device’s output response. To overcome this problem, Voltage Suppression Diodes are used. The operation of voltage suppression diode is similar to Zener diode operation.

    The operation of these diodes is normal as p-n junction diodes but at the time of transient voltage its operation changes. In normal condition, the impedance of the diode is high. When any transient voltage occurs in the circuit, the diode enters in to the avalanche breakdown region in which a low impedance is provided.

    It is very spontaneously because the avalanche breakdown duration ranges in Pico seconds. Transient voltage suppression diode will clamp the voltage to the fixed levels, mostly its clamping voltage is in minimum range.

    These are having applications in the telecommunication fields, medical, microprocessors and signal processing. It responds to over voltages faster than Varistors or gas discharge tubes.

    The symbol for Transient voltage suppression diode is as shown below.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 2 years ago in reply to robogary

    Wow great reference link.