Code Exchange
  • Technologies
  • More
Code Exchange
Blog modern C++ for loop, but you still want an index
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 5 Nov 2025 9:08 PM Date Created
  • Views 1681 views
  • Likes 8 likes
  • Comments 7 comments
  • Modern C++
  • c++26
Related
Recommended

modern C++ for loop, but you still want an index

Jan Cumps
Jan Cumps
5 Nov 2025

C++ has a range loop. A for loop that will run over all elements in the range you give it:

std::vector<int> v = {0, 1, 2, 3, 4, 5};
// ...

    for (auto i : v)
        std::cout << i << ' ';
    std::cout << '\n';

You don't have to check for container size. The for loop will give you the next item in i, contained in v, at each loop execution. start to end.
At runtime, this loop is as performant as the traditional C loop. You don't need to index the item in the range yourself, and it's overflow safe.

But there are times where you use the old school index for something else. Maybe to print rows:

int myNumbers[] = {25, 50, 75, 100};

int length = sizeof(myNumbers) / sizeof(myNumbers[0]);
int i;

for (i = 0; i < length; i++) {
  printf("%d %d\n", i, myNumbers[i]);
}

The range for loop doesn't have an index. But if you need one, it's not hard to create one. The new construct has an initialiser clause you can use. The advantage of that initialiser is, that the variable you declare there, is not visible outside the loop. No scope leakage:

std::vector<int> v = {0, 1, 2, 3, 4, 5};

    for (size_t inx = 0; auto i : v)
        std::cout << inx++ << ": " << i << ' ';
    std::cout << '\n';

Just a little code snippet that gives you all of the range for loop, and gives you that counter if you need it.
Thank you for reading.

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps 11 months ago

    The example in this blog is trivial. But range for loops are intuitive, even for more complex containers.

        for (auto &h: handlers) {
            pio_irq_manager_t::register_handler(h.pio, h.sm, &h, true);
        }

    The container in the example above is an STL array (called handlers) of Raspberry Pico stepper motor objects. The loop visits each of the objects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps 11 months ago

    The example in this blog is trivial. But range for loops are intuitive, even for more complex containers.

        for (auto &h: handlers) {
            pio_irq_manager_t::register_handler(h.pio, h.sm, &h, true);
        }

    The container in the example above is an STL array (called handlers) of Raspberry Pico stepper motor objects. The loop visits each of the objects.