Code Exchange
  • Technologies
  • More
Code Exchange
Blog Raspberry Pi Workout Timer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 17 Dec 2012 4:20 AM Date Created
  • Views 3673 views
  • Likes 2 likes
  • Comments 2 comments
  • raspbpi
  • python
  • code_exchange
  • Code Exchange
  • programming
  • raspberry_pi
  • rpi
  • pygame
Related
Recommended

Raspberry Pi Workout Timer

oneleggedredcow
oneleggedredcow
17 Dec 2012

So, I enjoy working out and have turned half of my garage into a home gym.  One thing that I don’t have and would like in my gym is a big stopwatch for doing a cross fit work out, so I looked around to see what was on amazon and was shocked at how expensive they were.  I mean $150 for a stopwatch with a large display is a bit excessive. So, I decided that I would build one using a raspberry pi, an old computer monitor that I had laying around, and some python code.

 

At the end of writing my last blog post, I got the idea about writing a maze game using pygame on the raspberry pi.  After doing a little more research, it looked like a great way to quickly write a graphics program, so I decided to give it a shot.  Since, I don’t have much experience with python, I decided to start small and just draw a rectangle on the screen.  Here’s the code to make that happen:

 

import pygame

import os

import time

 

red = pygame.Color(255, 0, 0)

 

def main():

    # Initialize the screen

    pygame.init()

    screen = pygame.display.set_mode((750, 350))

    pygame.display.set_caption('Timer')

 

    # Draw a rectangle

    pygame.draw.rect(screen, red, pygame.Rect(10,10, 50, 50))

    pygame.display.flip()

 

    # Exit when a key is pressed or the X is clicked

    while(1):

        for event in pygame.event.get():

            if event.type == pygame.KEYUP or event.type == pygame.QUIT:

                return

 

        time.sleep(0.1)

 

if __name__ == '__main__': main()


That creates a window with a red rectangle in it that looks like this:

image

After I got a rectangle on the screen, I decided to draw out the 7 segments of a typical clock display. The code to put in the place of the draw rectangle section looks something like this:

 

# Draw a seven segment led

led_height = 10

led_width = 75

 

offset = 4 * led_height / 3

 

# Top Center

pygame.draw.rect(screen, red, pygame.Rect(offset, 0, led_width, led_height))

# Top Left

pygame.draw.rect(screen, red, pygame.Rect(0, offset, led_height, led_width))

# Top Right

pygame.draw.rect(screen, red, pygame.Rect(2*offset + led_width - led_height, offset, led_height, led_width))

# Middle Center

pygame.draw.rect(screen, red, pygame.Rect(offset, 2*offset + led_width - led_height, led_width, led_height))

# Bottom Left

pygame.draw.rect(screen, red, pygame.Rect(0, 3*offset + led_width - led_height, led_height, led_width))

# Bottom Right

pygame.draw.rect(screen, red, pygame.Rect(2*offset + led_width - led_height, 3*offset + led_width - led_height, led_height,led_width))

# Bottom Center

pygame.draw.rect(screen, red, pygame.Rect(offset, 4*offset + 2*led_width - 2*led_height, led_width, led_height))

 

pygame.display.flip()


That creates a window with a seven segment LED that looks like this:

image

The last part of the puzzle is to take in a number and then determine which segments to light up.  To do this I used a pretty sneaky trick (well at least I think it is sneaky), I created a hash table where the key was the numbers 0-9 and the value was a bit mask that contained which segments should be on for that particular number.  So, the hash table looks like this:

 

digit_hash = {}

digit_hash[0] = int('1110111', 2)

digit_hash[1] = int('0100100', 2)

digit_hash[2] = int('1011101', 2)

digit_hash[3] = int('1101101', 2)

digit_hash[4] = int('0101110', 2)

digit_hash[5] = int('1101011', 2)

digit_hash[6] = int('1111011', 2)

digit_hash[7] = int('0100101', 2)

digit_hash[8] = int('1111111', 2)

digit_hash[9] = int('0101111', 2)


And the least significant bit is the top center LED segment, and the next bit is the top left LED segment, and so on, in the order that the segments were given in the previous code sample.  Now, all I can light up the LED segment based on whether or not the corresponding bit is set. Something like this:

 

mask = digit_hash[digit]

 

# Top Center

if(mask & int('0000001', 2)):

    pygame.draw.rect(canvas, color, pygame.Rect(offset, 0, led_width, led_height))

# Top Left

if(mask & int('0000010', 2)):

    pygame.draw.rect(canvas, color, pygame.Rect(0, offset, led_height, led_width))

 

And so on for the rest of the LED segments.

 

That’s all of the tricky parts of the code, the rest is just combining the pieces and updating the time every second.  The complete code is in the attached zip file.

 

Finally, here’s a video of the code running on my raspberry pi:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
WorkoutTimerCode.zip
  • Sign in to reply
Parents
  • darrell.little
    darrell.little over 9 years ago

    I know this is over 5 years old, but has anyone got the Timer.py to work?  The RedRectangle.py and SevenSegmentLed.py work as a demo, but not the actual Timer program.  Just curious.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sandeepnd
    sandeepnd over 9 years ago in reply to darrell.little

    There is a line that checks to see if the OS is NT. modify that line to say os.name!="NT". That should work. The author might have tried it on his windows PC while finally posting this. But pretty nice code! Just tried it out now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sandeepnd
    sandeepnd over 9 years ago in reply to darrell.little

    There is a line that checks to see if the OS is NT. modify that line to say os.name!="NT". That should work. The author might have tried it on his windows PC while finally posting this. But pretty nice code! Just tried it out now.