Code Exchange
  • Technologies
  • More
Code Exchange
Forum Python case
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 51 subscribers
  • Views 726 views
  • Users 0 members are here
  • python
  • Code Exchange
Related

Python case

markvenn
markvenn over 11 years ago

Greetings

Question for you. Does python suffer from a lack of switch / case statement in your opinions. I say yes, if / elif is OK but seems very inelegant to me.

Your opinions please.

Mark

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago +1
    @ Mark Venn I do not believe so and here is why. If I had many cases to test, I can use the dictionary list and simply use that in place of a case. The IF condition would be the key with the result being…
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    I don't personally think that Python suffers from an absence of the Switch-Case statements. The if-elif method is very similar, and though you have to repeatedly state the variable being assessed, you don't need to include break statements.

     

    The if-elseif approach (while not so elegant) can also be applied to many other languages as well, so from an educational point of view it may be more universal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 11 years ago

    I don't personally think that Python suffers from an absence of the Switch-Case statements. The if-elif method is very similar, and though you have to repeatedly state the variable being assessed, you don't need to include break statements.

     

    The if-elseif approach (while not so elegant) can also be applied to many other languages as well, so from an educational point of view it may be more universal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • markvenn
    markvenn over 11 years ago in reply to gadget.iom

    Paul

    Your comment about being if / elif being used in others is a point well made! I just like the use of switch cases in other languages. But of you are going from python onto another such as c++ then you already have a structure that works. But of course going from c++ to python you may, as I have, be used to using cases. Just one of those things I suppose image