Code Exchange
  • Technologies
  • More
Code Exchange
Forum If-Else construct in C language-hello world
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 51 subscribers
  • Views 2519 views
  • Users 0 members are here
  • loop
  • Code Exchange
  • world
  • hello
  • if-else
Related

If-Else construct in C language-hello world

dr.akshay_1980@yahoo.com
dr.akshay_1980@yahoo.com over 11 years ago

Hi,

       I want to display hello world after compiling the below code, How can this be possible?

 

main()

{

    if(?)

     {

        printf("hello");

     }

  else

    {

      printf( "world");

    }

}

 

Is this possible by any means? what should be in place of question mark above

  • Sign in to reply
  • Cancel

Top Replies

  • coolbox
    coolbox over 11 years ago in reply to dr.akshay_1980@yahoo.com +2 suggested
    Yes,It is Possible.You Know This question is similar to : Write a Hello world C program without using a semicolon(;) This is Full code: #include<stdio.h> #include<conio.h> int DemoFunction( void ) { printf…
  • dr.akshay_1980@yahoo.com
    dr.akshay_1980@yahoo.com over 11 years ago in reply to coolbox +1
    Yes great buddy,indeed I thought for this, but i was confused that calling the function in the the parameter and the zero(0) which is a return type, will it be returned to the stack or act as if condition…
  • shabaz
    shabaz over 11 years ago in reply to dr.akshay_1980@yahoo.com +1
    You're still only traversing one path of the fork of course. Which means that the other path is still never exercised, i.e. unused code - not great coding because effectively it can all be collapsed to…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    I don't imagine the compiler not objecting to the prior code 'cause void is not a type that can be true or false.  G_d I hate these stupid code puzzles, they never seem to illuminate much!  You could put a static variable in the fn, something like Virgin = 0.  When the function executes the last line is Virgin =1.  Virgin can be used as an index for a string table.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    I don't imagine the compiler not objecting to the prior code 'cause void is not a type that can be true or false.  G_d I hate these stupid code puzzles, they never seem to illuminate much!  You could put a static variable in the fn, something like Virgin = 0.  When the function executes the last line is Virgin =1.  Virgin can be used as an index for a string table.