Code Exchange
  • Technologies
  • More
Code Exchange
Forum multiple pre increment/post increment in expression of C language
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 35 replies
  • Answers 3 answers
  • Subscribers 53 subscribers
  • Views 19451 views
  • Users 0 members are here
  • increment
  • c
  • in
  • Code Exchange
  • post
  • single
  • precedency
  • operator
  • left
  • value
  • pre
  • expression
  • right
  • turbo
Related

multiple pre increment/post increment in expression of C language

dr.akshay_1980@yahoo.com
dr.akshay_1980@yahoo.com over 11 years ago

I would like to know the explanation for the following expression evaluation in C under windows TURBO c..

void main()

{

     int i=4;

    int x;

    x= ++i + ++i + ++i;   // i becomes 5 then 6 added becomes 11 and then incremented to 12 so 11+12=23   

    printf("%d",x);

    getch();

}

when the above was executed value of x comes out to be 21

 

Slightly eliminating the x variable in the above

 

void main()

{

    int i=4;

    printf("%d", ++i + ++i + ++i);   //accordingly at this step  5+6+7=18

    getch();

}

when the above is executed the answer comes out to be 18


Can anyone provide a decent explanation step by step and why two answers are different???


Thanks in advance.

Akshay


  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to dr.akshay_1980@yahoo.com +3
    If anyone asked you that (kind of) question at an interview (unless, perhaps, the job was to revise the C standard specification) you should explain that the only reasonable approach to such code was to…
  • gadget.iom
    gadget.iom over 11 years ago in reply to dr.akshay_1980@yahoo.com +2
    Ahhh... Complete code usually helps As for the problem... You have fallen victim to undefined behaviour as a result of each compilers interpretation of ambiguous code.
  • shabaz
    shabaz over 11 years ago in reply to dr.akshay_1980@yahoo.com +1
    Oh. I now get this is purely an academic question (and a very esoteric one not in my area of interest, sorry!) In real life people wouldn't write that code.. perhaps it is tested nowadays and therefore…
Parents
  • james.flynn
    0 james.flynn over 7 years ago

    Very interesting discussion but overall doesn't yield much useful information, mostly just fun to read about all the contributors opinions and self-reflective expertise.  I've been writing embedded code since the 80's in FORTRAN IV, FORTRAN77, PASCAL, MODULA-2, C, C++, and Assembly for way to many architectures and I still wouldn't consider myself an expert (I did have to write a Modula2 compiler during my masters project capstone).  But all that being what it is, the code presented here is kind of an Obfuscated code project rather than what you would see in a commercially supported/maintained project.  You can find other eccentric coding examples at  https://en.wikipedia.org/wiki/International_Obfuscated_C_Code_Contest.  More to the point of this original question, you can step through the statement using the 'C Operator Precedence' rules and determine the answer a compliant compiler would generate yourself.  That would cover the expression evaluation itself but not the language semantics/adherence. A 24 year old compiler, you would have to dig out the operator precedence rules that applied for that compiler.

     

    Just for the fun of it though, I did put this code into a GCC compiler:

     

    arm-oe-linux-gnueabi-gcc (GCC) 5.3.0

    Copyright (C) 2015 Free Software Foundation, Inc.

    This is free software; see the source for copying conditions.  There is NO

    warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

     

    To see what it said, it doesn't generate a syntax error but it does generate a warning:

     

    warning: operation on 'i' may be undefined [-Wsequence-point]

         x= ++i + ++i + ++i;   // i becomes 5 then 6 added becomes 11 and then incremented to 12 so 11+12=23  

                           ^

    warning: operation on 'i' may be undefined [-Wsequence-point]

     

     

    This warning is tell you the code has undefined semantics because of violations of sequence point rules in the C and C++ standards, so it isn't a syntax error but it is telling you that you may spend a long time debugging a problem that you could easily avoid.

     

    But hey, if you are trying to win the Obfuscated Code Coding contest maybe that is what you want...

     

    /Jim

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to james.flynn

    james.flynn  wrote:

     

    you can step through the statement using the 'C Operator Precedence' rules and determine the answer a compliant compiler would generate yourself. 

    This really isn't right.

    A compliant compiler is one which is compliant with a specified standard.

    ISO/IEC 9899 ("C99"|) and as far as I know all subsequent ISO C standards specify things like:

    i = ++i + 1;

    a[i++] = i;

     

    as undefined.

     

    This means that a compiler may make any result it likes and still be compliant.

    MK

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 7 years ago in reply to michaelkellett

    No, not really if your code is not compliant. 1 it probably not run. I know folk love to talk about it but. And even if it does run there is no guaranty the answer will be correct.

    BTW the two examples you show maybe compliant. As in the first one if i started as 1 answer should be 3

    in #2 you increment i after the store OK. but things like

    i = i++ + i++ are illegal and not compliant as most if not all parsers (2 or 3 pass optimizing) will get very confused. (this is where we all got on this stupid train, and as for me its time to get off and do something more important.) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • james.flynn
    0 james.flynn over 7 years ago in reply to phoenixcomm

    At this point the discussion really is a dead horse.  I compiled the code with GCC v5.x--which is a Compliant compiler (https://gcc.gnu.org/onlinedocs/gcc/Standards.html )--so your assertion that is it illegal and not compliant is flat out wrong.

     

    Rather than beating the horse, what I really want to highlight that people come to web-sites like element14 for primarily 2 reasons: (1) to get an answer to a question [I doubt they are going to come here to determine if their compiler is compliant] and (2) to find solutions to problems.  I responded to this thread because it is promulgating incorrect information about the compliance/legality of a correctly (though idiotic) C expression, then attempted to validate that information by incorrectly citing BNF notation.  The entire premises of the argument is invalidated by simply compiling the code segment and seeing that it does compile (though with a warning) and run.

     

    IMO, it is wrong to disseminate incorrect information as fact when it is really opinion.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • james.flynn
    0 james.flynn over 7 years ago in reply to phoenixcomm

    At this point the discussion really is a dead horse.  I compiled the code with GCC v5.x--which is a Compliant compiler (https://gcc.gnu.org/onlinedocs/gcc/Standards.html )--so your assertion that is it illegal and not compliant is flat out wrong.

     

    Rather than beating the horse, what I really want to highlight that people come to web-sites like element14 for primarily 2 reasons: (1) to get an answer to a question [I doubt they are going to come here to determine if their compiler is compliant] and (2) to find solutions to problems.  I responded to this thread because it is promulgating incorrect information about the compliance/legality of a correctly (though idiotic) C expression, then attempted to validate that information by incorrectly citing BNF notation.  The entire premises of the argument is invalidated by simply compiling the code segment and seeing that it does compile (though with a warning) and run.

     

    IMO, it is wrong to disseminate incorrect information as fact when it is really opinion.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer