Code Exchange
  • Technologies
  • More
Code Exchange
Forum Redundant parathensis in C
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 4 answers
  • Subscribers 54 subscribers
  • Views 3790 views
  • Users 0 members are here
  • Code Exchange
  • redundant
  • conditional tricky writing style
  • if else construct
  • paranthesis
Related

Redundant parathensis in C

dr.akshay_1980@yahoo.com
dr.akshay_1980@yahoo.com over 10 years ago

Hi,

Out of curiosity and experimenting with ANSI C constructs ,I would like to know any means by which we can ignore the empty braces for the conditional statements in C programming??? Does C allow us to do this.

 

Refer below the sample C code for discussion

 

 

int main()

{

     if()             /// there should no error while writing this, empty parathensis..

{

     printf("your if  is without parameters...");

}

else

{

    printf("if block ignored....");

}

return 0;

}

 

 

How to implement the above code in C successfully without any errors(compile time/Run time)????? By any means I want to implement above style.

 

 

Thanks in advance....

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to clem57 +2
    It looks like another interview/college homework type question (they do ask odd questions sometimes). Much like this one: If-Else construct in C language-hello world As you say, nothing for any real practical…
  • amgalbu
    amgalbu over 10 years ago +1 suggested
    According to c grammar, you need to type a boolean expression. So there is no way to create an if without condition
  • amgalbu
    amgalbu over 10 years ago in reply to D_Hersey +1
    @akshay dharma is asking if it is possibile to uae empty braces after a if keyword. That's noto possibile imho. Btw true and false are c++ keywords, and are not allowed in ANSI c (aka c90)
Parents
  • clem57
    0 clem57 over 10 years ago

    What sense would you expect to ask a question with no facts? C is just logic! A null condition has no context,

    But look at Go and a for loop can have ( ) and acts as a forever loop if you like because the language defines it..

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dr.akshay_1980@yahoo.com
    0 dr.akshay_1980@yahoo.com over 10 years ago in reply to clem57

    Hi Clem, I do agree with you, but after all C logic can be bypassed as we people have developed the C. In this case my intention is that you people should come out with OUT OF BOX solution for this , being an embedded developer I generally come across situations where I have to convert the C++/JAVA code into C(for lower end systems that don't support OOPS), I was just fiddling with if else construct....

     

    The approach from my end is to befool the compiler anyhow and lets bypass the conditional check for if using pragma directives or assert macros... i was looking ahead in this direction...

     

    Can we come out for its solution...???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dr.akshay_1980@yahoo.com
    0 dr.akshay_1980@yahoo.com over 10 years ago in reply to clem57

    Hi Clem, I do agree with you, but after all C logic can be bypassed as we people have developed the C. In this case my intention is that you people should come out with OUT OF BOX solution for this , being an embedded developer I generally come across situations where I have to convert the C++/JAVA code into C(for lower end systems that don't support OOPS), I was just fiddling with if else construct....

     

    The approach from my end is to befool the compiler anyhow and lets bypass the conditional check for if using pragma directives or assert macros... i was looking ahead in this direction...

     

    Can we come out for its solution...???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • amgalbu
    0 amgalbu over 10 years ago in reply to dr.akshay_1980@yahoo.com

    Can you point out a practical case?

    Empty braces could be always evaluated ad either true or false (depending on the semantica you want to adopt) so you can simply remove the if()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dr.akshay_1980@yahoo.com

    A nil boolean expression has no cognitive meaning and is therefore correctly diagnosed as missing by `gcc`.  I suggest that you either code if(1) or #define TRUE 1 and use if(TRUE).

     

    Don't fight something that isn't going to change because there is no point to do so.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago in reply to e14 Contributor

    https://en.wikipedia.org/wiki/Three-valued_logic

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • amgalbu
    0 amgalbu over 10 years ago in reply to D_Hersey

    That's really interesting. Can't think of a practical usage but an interesting answer to explain the meanung of "if ()"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to D_Hersey

    Don, I do not know why you were pointing out 3-valued logic.  In any case, the C if statement is clearly based on 2-valued logic.