Code Exchange
  • Technologies
  • More
Code Exchange
Forum Code for small diy clock kits.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 36 replies
  • Answers 18 answers
  • Subscribers 51 subscribers
  • Views 11341 views
  • Users 0 members are here
  • mod
  • clock
  • at89
  • Code Exchange
  • attiny 2313
  • diy
  • assembly_language
Related

Code for small diy clock kits.

fbtjbt
fbtjbt over 8 years ago

I've been looking for a project that would be suitable for young Boy Scouts, and have decided that one of these DIY clock kits would be something that even the youngest could put together.

imageimage

Most of the kits appear to come with an AT89C2051 (they all seem to come with the same pcb as well), so I've also searched out code that the older scouts could program additional AT89C2051s with. I'll reach out to the local university to see if they've got a programmer that we can use, but the boys won't have access to one after we're done making these. I think having a couple extra chips to swap around with different programs would be cool to them.

 

The clock comes with a standard clock program, but I'm still looking for a simple countdown timer and a simple stopwatch. By "simple" I mean something that I can show the scouts, and explain commented snippets of the code.

The code that I've found has been on forums where the members haven't been active for years, so I can't ask them followup questions.

 

If anyone could help me out with simplified code for two projects, I would greatly appreciate it. I can reassign pins in the code if the boards end up being pinned slightly different than what is pictured (you never know with these things).

 

Countdown Timer:

- button1 == cancel timer / cancel buzzer

- button2 == add time to countdown

- button1 held >2sec == enter/exit setup mode.

- button1 in setup mode == toggle buzzer duration between: 60sec / 300sec / 600sec / 9999sec

- button2 in setup mode == toggle button2 "value" between: 30sec / 60sec / 180sec / 240sec / 300sec

Timer counts down in seconds from 9999 - 0 (in base10)

Digits blink at 500ms intervals while <=10sec

Button2 push adds value to current countdown at any time

Buzzer sounds at 500ms interval.

 

Stopwatch:

- button1 == clear

- button2 == start/pause

- button1 + button2 == switches between hh:mm / mm:ss / ss:ms ("Hr:  " / " :S " / " S:  ")

Time counts up (in base 60)

Time stops at 99:59 (i.e. 99hr:59min / 99min:59sec / 99sec:59ms)

 

I think there are some good learning opportunities between the two programs. Showing them the code and having them customize values in their code (like the available "values" for button1&2) will help them feel ownership in the project.

 

 

TheCustomGeek shared some code for one of his projects, and is what I used as the base for my attempts to make the Countdown Timer and Stopwatch described above. Here's a link Multiplexing for a 7 year old | The Custom Geek

I've attached the code, too, mainly so that the multiplexing can be similar in both projects (easier to explain to the scouts). Using a better method is fine too.  I've removed this, and attached the assembly code that I had initially started with -prior to finding TheCustomGeek's project. We do have access to a C compiler and linker for the 8051s (AT89C2051 included), though.

 

I'm still muddling through this on my own, but I'm hoping that one (or more) of you would be able to put together some code much faster/better/cleaner than I.

Attachments:
Countdown Timer.a51.txt.zip
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago in reply to shabaz +4 suggested
    The atTiny2313A is a supported product of Atmel/Microchip in current production. It's a way better part than the 8051 based one. Atmel Studio 7 supports it and gives you a free C compiler and debugger…
  • michaelkellett
    michaelkellett over 8 years ago in reply to fbtjbt +4 suggested
    I had some free Paypal money (from "Have a beer" promotion on Embedded related") so I just ordered 2 of these: https://www.ebay.co.uk/itm/282484911382?ViewItem=&item=282484911382 I'll try re-hearting one…
  • shabaz
    shabaz over 8 years ago in reply to fbtjbt +3 suggested
    That's assembler code, which is likely what you'll need to do for the AT89C2051, unless you can find a C compiler and linker (I have no idea if that is practical for that chip, and it will require some…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi,

     

    The attached code is for an Arduino, which contains a different microcontroller compared to AT89C2051. The code isn't compatible.

    You could rewrite the code for AT89C2051, but you'd almost have to start from scratch, since even the LED display is different, yours appears to have 12 pins, and the one that the Arduino code is for has 16 pins, so yours is multiplexed differently, and that would need to be deciphered too. So, a non-trivial exercise to do this, but possible.

    The AT89C2051 is a really ancient chip, so although you'll likely find information on the Internet on how to program it and perhaps some example programs to get you started, personally I don't have any example source code for this microcontroller - I think I maybe briefly used it >10 years ago. Personally I wouldn't advise it, because you'll need to source a programmer and compiler, and most of this is really ancient as mentioned. Better to just have a construction project with it using the pre-programmed chip supplied with the kit perhaps, and have a different project if you want to demonstrate different code.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to shabaz

    Dangit. I had started this project using code from one of those other groups that I mentioned, but then started looking for other code after a while. TheCustomGeek code was more 'legible' to me, so that's when I pivoted. Here is what I was working with before (see attached txt).

    Attachments:
    1856.Countdown Timer.a51.txt.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to gadget.iom

    I guess it depends on what you want to learn/teach.

     

    Lots of kids will be happy to attempt soldering the board together.

     

    Only a few will want to get into why it works - I always think that the ones who will stick with programming are the ones who get cheesed off when teachers, to use Shabaz's example, refuse to explain what 'sbit' means.

     

    To me the Arduino IDE is obfuscation not simplification (but that's just me image)

     

    For the OP, the good news is that he can use the atTiny and has a nice choice of options.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    I haven't ordered one yet, but here is the one I had planned on getting (just purchased):

    c51 4 bits digital 7-segment led electronic clock DIY kit set

     

    I just read up on the Atmel Studio 7 that you mentioned, and I think it's an excellent option!

    Downloading now...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to gadget.iom

    I haven't experimented with Arduino yet, but I see it everywhere.

    I've been able to explain C code fairly easily to my younger nephews, but I'm up for learning something new if it will be something these boys will use later on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to gadget.iom

    The Digispark Pro is using the ATtiny167 and this includes a bootloader.

     

    I'm not sure how compatible the two are, but in terms of the ease of use then Arduino with all it's limits and benefits might be a better option.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    I'm definitely interested in the help, that would be awesome!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to fbtjbt

    I had some free Paypal money (from "Have a beer" promotion on Embedded related") so I just ordered 2 of these:

     

    https://www.ebay.co.uk/itm/282484911382?ViewItem=&item=282484911382

     

    I'll try re-hearting one with an atTiny.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    I have received mine, and have started tinkering. How is yours going?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to fbtjbt

    I have two - I built one the other day and it does run. The instructions for operating it are so utterly dreadful that I can't understand them at all - I managed to set it by random fiddling.

     

    I forgot to order Atmel processors but I did that just now: 1841620 from Farnell (ATtiny4313)

     

    I'll write some code for re-purposing the board as a timer - and post it.

     

    How are you getting on ?

     

    image

     

    If anyone can translate into English it would be nice image

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    This guy shows how to set up the original clock. https://www.youtube.com/watch?v=q421PYti3Ic

     

    Ive been messing with code, but i think I need a different programmer for the ATtiny4313... so I've been searching YouTube for How-to vids and checking out their equipment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    I ordered a different programmer that I saw in a video on youtube. It should be here this weekend/monday. I've modified code for a "multiplexing" clock to (hopefully) work with the pinout of the DIY Clock, so I can try it out once the programmer gets here.

    As long as it works, I can start messing with code for the two projects above.

    How goes the Countdown Timer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    I ordered a different programmer that I saw in a video on youtube. It should be here this weekend/monday. I've modified code for a "multiplexing" clock to (hopefully) work with the pinout of the DIY Clock, so I can try it out once the programmer gets here.

    As long as it works, I can start messing with code for the two projects above.

    How goes the Countdown Timer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to fbtjbt

    My own playing has not gone well - lack of time so zero progress since Feb25th image

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fbtjbt
    0 fbtjbt over 8 years ago in reply to michaelkellett

    The rest of my kit came in, and everything is assembled, so my first attempt is to get the display working with a simple program.

    It turns out that the schematic associated with the clock is incorrect. I've updated the schematic below with the display pin numbers to match the PCB layout.

    I haven't been able to verify that the segment order is correct, nor if the digit order is correct, because I'm still trying to wrap my head around how it works using sip resistors.

     

    Would you turn OFF the segments by setting the segment pins LOW (and digit pins HIGH) to pull the 5v away from the display?

    Then set the digit pin LOW to select the digit, and the segment pin HIGH to divert the 5v back to the segment?

     

     

    image

     

    EDIT: I've confirmed a few of the display pinouts (above), so I'd imagine that the rest are correct also.

     

    I've gotten to the point where I can blink the display ONCE (without control over duration) then the display becomes unresponsive.

    - Setting the digit pins to HIGH, and the segment pins to LOW disables the display.

    - Setting pin0 (digit pin 12) to LOW, and pin10 (segment pin 5 'g') to HIGH gives me a short "-"blink.

    - Setting pins 0, 1, 4 & 8 (digit pins 12, 9, 8 & 6) to LOW, and pin10 (segment pin 5 'g') to HIGH gives me a short "----"blink.

     

    I still don't fully understand how to drive the display when using pull-up resistors on the segment pins.

    Am I right in that HIGH=SOURCE and LOW=SINK?

    Or do you need to use LOW to SINK (divert power), then "FLOAT" the segment pins to allow the LED to pull power through the 1K resistor array?