Code Exchange
  • Technologies
  • More
Code Exchange
Forum How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 55 subscribers
  • Views 3624 views
  • Users 0 members are here
  • 32bit
  • raspbpi
  • raspcontrol
  • Code Exchange
  • programming
  • embedded
  • raspberry_pi_rev_2
  • arm
  • arduino
  • atmel
Related

How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?

shahbhaumik
shahbhaumik over 13 years ago

There are various option when it comes to connect RPI with external embedded boards. Currently many geeks are trying to interface various peripherals with RPI with the I/O header given. I feel there are following option one can go with.

 

1) Use I/O header.

Which i feel is good for prototyping but as we move do something that looks good this option is not what I feel is best, I hate all the wires that comes out of RPI and then loose connection and what not to take care of...

 

2) Use of USB port.

RPI is computer and you it can communicate to co-processor using its USB ports.I think this is very neat way to do things. For example if you are making a robot which has a microcontroller that has UART it can easily communicate with RPI above that you can reflash you microcontroller as per your application using RPI. I know there are no instruction or related work out there like this but soon i will be posting instruction to do this on my blog as well on code exchange.

 

 

Would like to now community views on same.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago +1
    Thus far I've been using the Adafruit Pi Cobbler Adafruit Pi Cobbler to interface the header with a breadboard and programming in Python using libraries like RPi.GPIO . I've really enjoyed Adafruit's tutorials…
  • morgaine
    morgaine over 13 years ago in reply to fustini +1
    Since you've already dealt with 1) Use I/O header , and 2) Use of USB port , I think I'll add the missing alternative, 3) Use of Ethernet . Some people consider USB a fixture and a sacred cow, but I've…
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    On the issue of Ethernet complexity, I can't help you further since you refuse to use the engineering concept of dividing a communications stack into layers so that properties of single layers can be discused…
Parents
  • johnbeetem
    0 johnbeetem over 13 years ago

    Like many others, I've used the GPIO header for LEDs.  Very quick and easy at the device register level, except for having to sudo unless you want to write a device driver.  If you don't want a cable, it's easy to make a PCB sandwich.

     

    USB is attractive, and I intend to come up the learning curve on USB software one of these months.  RasPi has known USB issues with lost packets in some cases, so you must make sure your application can handle lost packets, for example by using a high-level protocol like TCP that retransmits lost packets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 13 years ago

    Like many others, I've used the GPIO header for LEDs.  Very quick and easy at the device register level, except for having to sudo unless you want to write a device driver.  If you don't want a cable, it's easy to make a PCB sandwich.

     

    USB is attractive, and I intend to come up the learning curve on USB software one of these months.  RasPi has known USB issues with lost packets in some cases, so you must make sure your application can handle lost packets, for example by using a high-level protocol like TCP that retransmits lost packets.