Code Exchange
  • Technologies
  • More
Code Exchange
Forum Raspberry Pi Python code
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 49 subscribers
  • Views 513 views
  • Users 0 members are here
  • Code Exchange
  • pyhton
  • c++
Related

Raspberry Pi Python code

e14 Contributor
e14 Contributor over 13 years ago

hi everyone i need some code to control 6 relays via the gpio pins

ill give you the c code i have but i want it in python pls can you help me

 

 

 

#include <stdio.h>

#include <fcntl.h>

#include <sys/mman.h>

 

 

#define IOBASE   0x20000000

 

 

#define GPIO_BASE (IOBASE + 0x200000)

 

 

#define GPFSEL0    *(gpio.addr + 0)

#define GPFSEL1    *(gpio.addr + 1)

#define GPFSEL2    *(gpio.addr + 2)

#define GPFSEL3    *(gpio.addr + 3)

#define GPFSEL4    *(gpio.addr + 4)

#define GPFSEL5    *(gpio.addr + 5)

// Reserved @ word offset 6

#define GPSET0    *(gpio.addr + 7)

#define GPSET1    *(gpio.addr + 8)

// Reserved @ word offset 9

#define GPCLR0    *(gpio.addr + 10)

#define GPCLR1    *(gpio.addr + 11)

// Reserved @ word offset 12

#define GPLEV0    *(gpio.addr + 13)

#define GPLEV1    *(gpio.addr + 14)

 

 

#define BIT_17 (1 << 17)

 

 

#define PAGESIZE 4096

#define BLOCK_SIZE 4096

 

 

struct bcm2835_peripheral {

    unsigned long addr_p;

    int mem_fd;

    void *map;

    volatile unsigned int *addr;

};

 

 

struct bcm2835_peripheral gpio = {GPIO_BASE};

 

 

// Some forward declarations...

int map_peripheral(struct bcm2835_peripheral *p);

void unmap_peripheral(struct bcm2835_peripheral *p);

 

 

int gpio_state = -1;

 

 

////////////////

//  main()

////////////////

int main(int argc, char *argv[]) {

 

 

    if(argc == 2) {

        if(!strcmp(argv[1], "on"))

            gpio_state = 1;

        if(!strcmp(argv[1], "off"))

            gpio_state = 0;

    }

 

 

    if(map_peripheral(&gpio) == -1) {

        printf("Failed to map the physical GPIO registers into the virtual memory space.\n");

        return -1;

    }

 

 

    /* Set GPIO 17 as an output pin */

    GPFSEL1 &= ~(7 << 21); // Mask out bits 23-21 of GPFSEL1 (i.e. force to zero)

    GPFSEL1 |= (1 << 21);  // Set bits 23-21 of GPFSEL1 to binary '001'

 

 

    if(gpio_state == 0)

        GPCLR0 = BIT_17;

    else if(gpio_state == 1)

        GPSET0 = BIT_17;

 

 

    usleep(1);    // Delay to allow any change in state to be reflected in the LEVn, register bit.

 

 

    printf("GPIO 17 is %s\n", (GPLEV0 & BIT_17) ? "high" : "low");

 

 

    unmap_peripheral(&gpio);

 

 

    // Done!

}

 

 

// Exposes the physical address defined in the passed structure using mmap on /dev/mem

int map_peripheral(struct bcm2835_peripheral *p)

{

   // Open /dev/mem

   if ((p->mem_fd = open("/dev/mem", O_RDWR|O_SYNC) ) < 0) {

      printf("Failed to open /dev/mem, try checking permissions.\n");

      return -1;

   }

 

 

   p->map = mmap(

      NULL,

      BLOCK_SIZE,

      PROT_READ|PROT_WRITE,

      MAP_SHARED,

      p->mem_fd,  // File descriptor to physical memory virtual file '/dev/mem'

      p->addr_p      // Address in physical map that we want this memory block to expose

   );

 

 

   if (p->map == MAP_FAILED) {

        perror("mmap");

        return -1;

   }

 

 

   p->addr = (volatile unsigned int *)p->map;

 

 

   return 0;

}

 

 

void unmap_peripheral(struct bcm2835_peripheral *p) {

 

 

    munmap(p->map, BLOCK_SIZE);

    close(p->mem_fd);

}

  • Sign in to reply
  • Cancel
  • callum311
    0 callum311 over 12 years ago

    you should be able to use that as long as you have the arduino repository if you are on raspberry pi you will need an arduino board and install the software

     

    sudo apt-get install arduino

     

    or even have a look on you tube but just remember on the standard gpio pins it is all output not input