Code Exchange
  • Technologies
  • More
Code Exchange
Forum Beaglebone & C
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 51 subscribers
  • Views 2210 views
  • Users 0 members are here
  • c
  • compilers
  • embedded
Related

Beaglebone & C

e14 Contributor
e14 Contributor over 12 years ago

I've been playing with I/O ports in Javascript, that works fine, but basically I'm a C programmer.  I want to do the same, read a sensor and turn things on & off with the beaglebone using C.  The only information I've found so far is a wiki about embedded C that references a header file, iohw.h that makes it all possible, but which doesn't exist within the C compiler in the Angstrom or Debian distributions.  Shall I assume that what I want to do cannot be done in C on the beaglebone?  A standard ansi C manual has nothing on the topic for obvious reasons, and if there's any documentation for the beaglebone's C compiler it has escaped my searches so far.  Can this be done, and if so, what is the function to write a bit to gpio44 or read a bit from gpio46?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mconners +2
    Michael Conners wrote: Realize that is one of the things you give up when going from bare metal to working with an operating system. The OS becomes the gatekeeper between you and the underlying hardware…
  • mconners
    mconners over 12 years ago in reply to e14 Contributor +1
    There is nothing stopping you from getting to the specific architecture of the chip as far as the compiler goes. You can still get there, that's how they wrote the OS in the first place. I'm just saying…
  • mconners
    mconners over 12 years ago in reply to mconners +1
    Another good resource http ://derekmolloy.ie/beaglebone/beaglebone-gpio-programming-on-arm-embedded-linux/ Mike
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    I've accessed GPIOs on a BeagleBoard using mmap().  Here's an old Google Groups thread on the topic: https://groups.google.com/forum/#!topic/beagleboard/_29qqEOv2VA

     

    I suspect the Bone is similar, with different addresses.  You will probably have to "sudo" to be able to mmap() the GPIOs directly.  The thread has some other methods that may be easier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    Thanks.  I'll give that a try. I thought about writing direct to the registers, but the chip data sheet only gives the offsets to the registers, I'm still looking for the base address.  With the microcontrollers I'm used to working with if you want to do something to PORTB you just call it PORTB or PORTB,4 to play with bit 4. there's no need to plow through a 4700 page chip manual to find an address you can attach to a symbolic name.  It doesn't look like any of the names for ports are in the C compiler, unless they're in a header file I haven't found yet.  I'll admit I'm a bit rusty, my last serious exposure to unix was System 5 Rev. 4 on Unisys 6000-50's handling 911 call centers.  Yeah, that long ago. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to e14 Contributor

    No, C wouldn't know about the device registers for any particular SoC.  There may be header files somewhere, but I don't know where.  A lot of GNU/Linux programmers use a device driver on SBCs like Raspberry Pi and Beagles.  Personally, I prefer mmap() and accessing the registers, but maybe I'm still stuck in the PDP-11 days :-)

     

    Raspberry Pi GPIO is quite well developed and supported, and maybe some of this applies to Beagle: RasPi Hardware Wiki

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to e14 Contributor

    No, C wouldn't know about the device registers for any particular SoC.  There may be header files somewhere, but I don't know where.  A lot of GNU/Linux programmers use a device driver on SBCs like Raspberry Pi and Beagles.  Personally, I prefer mmap() and accessing the registers, but maybe I'm still stuck in the PDP-11 days :-)

     

    Raspberry Pi GPIO is quite well developed and supported, and maybe some of this applies to Beagle: RasPi Hardware Wiki