Code Exchange
  • Technologies
  • More
Code Exchange
Forum OS Development
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 50 subscribers
  • Views 2274 views
  • Users 0 members are here
  • Code Exchange
  • assembly
Related

OS Development

nick123
nick123 over 11 years ago

     I've been studying assembly language for a long long long time, and I want to try OS Development. I've heard of MikeOS it was entirely written in real mode assembly. I looked over the code of MikeOS and now I feel very discouraged. It is a lot of complicated code just for a simple os.

 

MikeOS - simple x86 assembly language operating system

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    Most OS are not written in assembler but in C or other high level language. To write even a small scheduler type OS in assembler is an odd thing to do since it will make it take longer and it won't be…
  • johnbeetem
    johnbeetem over 11 years ago in reply to nick123 +1
    Nick Gallagher wrote: Why is C portable and not assembly? An assembly language program only runs on one computer architecture, i.e., one instruction set. You can't run ARM assembly language on x86…
  • clem57
    clem57 over 11 years ago in reply to nick123 +1
    Yes if they produce a .COM module and assembly inline OK if you are careful.
Parents
  • johnbeetem
    0 johnbeetem over 11 years ago

    C was originally created as a system programming language so that you could write operating system kernels and utilities using portable high-level syntax.  C was designed to be easy to compile into efficient assembly language, specifically PDP-11.  Like many people, I think of C as a portable assembly language that uses high-level notations.

     

    As an amusing historical note, I once used a Unix system where the man page for the assembler had the following text:

    Assembly language is dead.  Necrophilia will be punished.

    That said, you'll write better C programs if you've mastered assembly language first.  You'll also find it easier to debug C programs since the C run-time model is machine language, i.e., no seat belts to protect your program from itself.

     

    JMO/YMMV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nick123
    0 nick123 over 11 years ago in reply to johnbeetem

    Why  is C portable and not assembly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to nick123

    Nick Gallagher wrote:

     

    Why  is C portable and not assembly?

    An assembly language program only runs on one computer architecture, i.e., one instruction set.  You can't run ARM assembly language on x86, or vice-versa, because the instructions and processor registers for one assembly language aren't the same as another.  (Well, you can use an emulator if you don't need high performance.)

     

    Unless it accesses implementation-specific device registers, a well-written [*] C program can run on any computer architecture for which you can get a C compiler.  So you can run the same C program on ARM and x86, except for the parts that access device registers.  If those are in device drivers, your well-written application programs are completely portable.

     

    [*]  There are some nuances that make C programs non-portable, such as writing code that depends on whether your architecture is big-endian or little-endian.  This is not an issue between x86 and ARM, because both are usually little-endian.  It is an issue porting C programs between x86/ARM and 68000/PowerPC.  There are other nuances as well, which is why software development groups need a few "grown-ups" around who have mastered assembly language so they know what things can go wrong and how to fix them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nick123
    0 nick123 over 11 years ago in reply to johnbeetem

    So, can C be compiled into flat binary like assembly? Also, is C anything like assembly. Can I put bits of assembly code in C?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to nick123

    Yes if they produce a .COM module and assembly inline OK if you are careful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to nick123

    Yes if they produce a .COM module and assembly inline OK if you are careful.