Code Exchange
  • Technologies
  • More
Code Exchange
Forum Can anyone tell me what code this is?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 52 subscribers
  • Views 5266 views
  • Users 0 members are here
  • Code Exchange
Related

Can anyone tell me what code this is?

clem57
clem57 over 11 years ago

This is a quiz of sorts. I wish to know

  1. what microprocessor uses these instructions
  2. who makes it
  3. what does it do

 

0000 90      GHI 0  
0001 B6      PHI 6
0002 F829    LDI DOIT 
0004 A6      PLO 6
0005 E0      SEX 0  
0006 6400    OUT 4,00  
0009 3F09    BN4 * 
000B 6C      INP 4  
000C 64      OUT 4  
000D 370D    B4 *  
000F F860    LDI #60  
0011 A6      PLO 6  
0012 E0      SEX 0  
0013 6401    OUT 4,01
0015 3F15    BN4 *
0017 E6      SEX 6  
0018 6C      INP 4  
0019 64      OUT 4  
001A 371A    B4 *
001C E0      SEX 0  
001D 6402    OUT 4,02
001F E6      SEX 6
0020 3F20 LOOP: BN4 * 
0022 6C      INP 4  
0023 64      OUT 4  
0024 3724    B4 * 
0026 26      DEC 6  
0027 26      DEC 6
0028 46      LDA 6  
0029 C4 DOIT: NOP  
002A C4      NOP  
002B 26      DEC 6   
002C 56      STR 6 
002D 64      OUT 4  
002E 7A      REQ  
002F CA0020  LBNZ LOOP  
0032 7B      SEQ  
0033 3020    BR LOOP 

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago +2 verified
    There's only one microprocessor I know of that has a SEX instruction. It was the first CMOS microprocessor and was produced by the company that pioneered CMOS. The company originally called it COS/MOS…
  • michaelkellett
    michaelkellett over 11 years ago +2 suggested
    Much too easy - just Google the first 5 lines of code. I considered using one a long time ago but we never did - Motorola brought out a CMOS 6805 just in time. MK.
  • gdstew
    gdstew over 11 years ago in reply to johnbeetem +1
    Without looking I do at least know which one the COS/MOS processor is, having never used it I did not recognize the code. The Motorola 6809 processor also has a sex (sign extend) instruction and it has…
Parents
  • johnbeetem
    0 johnbeetem over 11 years ago

    There's only one microprocessor I know of that has a SEX instruction.  It was the first CMOS microprocessor and was produced by the company that pioneered CMOS.  The company originally called it COS/MOS: COmplementary-Symmetry Metal-Oxide Semiconductor.

     

    To avoid spoiling the game for others, I won't name the company or processor.  But I found it quickly at Wikipedia, and the page has your assembly language listing image

     

    I can't believe I still remember that chip.  It's not like I ever used it.  IIRC I looked at the instruction set and found it pretty ugly.  I think its chief advantage was that COS/MOS could be powered from 3V to 15V, so the "SEX machine" was a good fit for industrial applications where you needed really wide noise margins.  COS/MOS was also really low power, drawing next to nothing at low frequencies.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago

    There's only one microprocessor I know of that has a SEX instruction.  It was the first CMOS microprocessor and was produced by the company that pioneered CMOS.  The company originally called it COS/MOS: COmplementary-Symmetry Metal-Oxide Semiconductor.

     

    To avoid spoiling the game for others, I won't name the company or processor.  But I found it quickly at Wikipedia, and the page has your assembly language listing image

     

    I can't believe I still remember that chip.  It's not like I ever used it.  IIRC I looked at the instruction set and found it pretty ugly.  I think its chief advantage was that COS/MOS could be powered from 3V to 15V, so the "SEX machine" was a good fit for industrial applications where you needed really wide noise margins.  COS/MOS was also really low power, drawing next to nothing at low frequencies.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • gdstew
    0 gdstew over 11 years ago in reply to johnbeetem

    Without looking I do at least know which one the COS/MOS processor is, having never used it I did not recognize the code.

     

    The Motorola 6809 processor also has a sex (sign extend) instruction and it has a bra (branch always) instruction too.