Code Exchange
  • Technologies
  • More
Code Exchange
Forum How would / could I send a 0x10?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 49 subscribers
  • Views 877 views
  • Users 0 members are here
  • Code Exchange
  • c++
Related

How would / could I send a 0x10?

thesea
thesea over 7 years ago

Hello,

The problem I met is the above display would be something like ON / OFF or SLEEPIN / SLEEPOUT.

The used controller ILI9341 should be able to do that. There is no SPI or I2C used but 8 data lines.

The following commands are defined in registers.

 

………...
#define ILI9341_SOFTRESET          0x01
#define ILI9341_SLEEPIN            0x10
#define ILI9341_SLEEPOUT           0x11
#define ILI9341_NORMALDISP         0x13
#define ILI9341_INVERTOFF          0x20
#define ILI9341_INVERTON           0x21
#define ILI9341_GAMMASET           0x26
#define ILI9341_DISPLAYOFF         0x28
#define ILI9341_DISPLAYON          0x29
.................

 

So how would / could I send a 0x10, for example?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +1
    It depends on what you're using in terms of the connection. It can be run in 16-bit parallel, 8-bit parallel, or 3/4-wire serial as per Page 26 of the datasheet: https://cdn-shop.adafruit.com/datasheets…
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    It depends on what you're using in terms of the connection. It can be run in 16-bit parallel, 8-bit parallel, or 3/4-wire serial as per Page 26 of the datasheet: https://cdn-shop.adafruit.com/datasheets/ILI9341.pdf

     

    Assuming you have identified which mode you're using (see mode pins IM0-IM3), I'll assume a basic 8-bit parallel one, you will need to set the data lines to the register to match the command address and toggle the WRX line with CSX asserted (e.g. Page 31), then repeat with the value you want written to the register.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 7 years ago

    It depends on what you're using in terms of the connection. It can be run in 16-bit parallel, 8-bit parallel, or 3/4-wire serial as per Page 26 of the datasheet: https://cdn-shop.adafruit.com/datasheets/ILI9341.pdf

     

    Assuming you have identified which mode you're using (see mode pins IM0-IM3), I'll assume a basic 8-bit parallel one, you will need to set the data lines to the register to match the command address and toggle the WRX line with CSX asserted (e.g. Page 31), then repeat with the value you want written to the register.

     

    - Gough