Code Exchange
  • Technologies
  • More
Code Exchange
Documents Rescaling positive value
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: jpnbino
  • Date Created: 23 Aug 2018 10:05 PM Date Created
  • Last Updated Last Updated: 6 Oct 2021 9:42 PM
  • Views 718 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Rescaling positive value

Edit: I know its boring to take someone else's code and set up an environment. For that, I've made the code available and ready to run in https://www.jdoodle.com/embed/v0/FeZ

 

Hey Folks, many times we need to translate values to different ranges so I wrote this piece of code. I hope you enjoy and give feedback and ideas to improve:

 

 

/**
  @Description
    This function performs a conversion from one scale X to scale Y. The relation between those scales is considered linear. Then, based on the parameters a known value x in scale X is converted to a value y in scale Y.
  @Preconditions
    None
  @Param
    x  - is the value to be converted to scale y
     xa - is the minimum scale X value.
     xb - is the maximum scale X value.
     ya - is the minimum scale Y value.
     yb - is the maximum scale Y value.
  @Returns
    The value converted from scale X to scale Y.
  @Comment
    This function uses the round half up method as an integer rounding method
  @Example
    <code>
     #define MIN_X 20
     #define MAX_X 50

     #define MIN_Y 1000
     #define MAX_Y 2000

     uint16_t y;
     uint16_t x = 30;

     y = Rescale_Value( x, MIN_X, MAX_X, MIN_Y, MAX_Y );

    </code>
*/

uint16_t Rescale_Value (uint16_t x , uint16_t xa, uint16_t xb, uint16_t ya, uint16_t yb )
{
/**
Algorithm:
1 - Find a linear equation;
2 - Calculate the equation considering rounding;

Explanation:
- A equation of the line correlates two different range of values. The equation
is given by the following formula,

y = ((yb - ya)*(x - xa))/(xb - xa)) + ya;

where,
(xa,ya) and (xb,yb) -> are known points in the line.

OBS: to complete understand solution search equation of the line theory.
Considerations:
y will be written as a/b + ya
where,
a = (yb - ya)*(x - xa)
b = (xb - xa)
*/
//test input condition
    if(x < xa)
    {
        x = xa;
    }
    else if ( x > xb)
    {
        x = xb;
    }
  
uint16_t y;

//multiplication of two 16bits gives a 32bits integer
uint32_t a;
uint16_t b;


a = (yb - ya)*(x - xa);
b = (xb - xa);

/**
In the matter of integers, calculation rounding must be considered.
Then, y is calculated using the round half up method
So, a/b is aproximated as (a/b + 1/2), but as calculation is performed by integers
1/2 = 0 (zero), then (a/b + 1/2) is rewritten as((a + b/2)/b).
*/
y = ((a + b/2)/b) + ya;

    return y ; 
}